EmberCommandState Struct Reference
For use when declaring a separate command streams. The fields are not accessed directly by the application. More...
#include <
command-interpreter2.h
>
Data Fields |
|
| uint8_t | state |
| uint8_t | buffer [ EMBER_COMMAND_BUFFER_LENGTH ] |
| uint8_t | tokenIndices [ MAX_TOKEN_COUNT +1] |
| uint8_t | tokenCount |
| uint16_t | index |
| uint8_t | error |
| uint8_t | hexHighNibble |
| uint8_t | argOffset |
| uint8_t | previousCharacter |
| uint8_t | defaultBase |
| EmberCommandEntry * | currentCommand |
For use when declaring a separate command streams. The fields are not accessed directly by the application.
Definition at line
407
of file
command-interpreter2.h
.
Field Documentation
◆ argOffset
| uint8_t EmberCommandState::argOffset |
Definition at line
433
of file
command-interpreter2.h
.
◆ buffer
| uint8_t EmberCommandState::buffer[ EMBER_COMMAND_BUFFER_LENGTH ] |
Definition at line
414
of file
command-interpreter2.h
.
◆ currentCommand
| EmberCommandEntry * EmberCommandState::currentCommand |
Definition at line
443
of file
command-interpreter2.h
.
◆ defaultBase
| uint8_t EmberCommandState::defaultBase |
Definition at line
440
of file
command-interpreter2.h
.
◆ error
| uint8_t EmberCommandState::error |
Definition at line
427
of file
command-interpreter2.h
.
◆ hexHighNibble
| uint8_t EmberCommandState::hexHighNibble |
Definition at line
430
of file
command-interpreter2.h
.
◆ index
| uint16_t EmberCommandState::index |
Definition at line
424
of file
command-interpreter2.h
.
◆ previousCharacter
| uint8_t EmberCommandState::previousCharacter |
Definition at line
437
of file
command-interpreter2.h
.
◆ state
| uint8_t EmberCommandState::state |
Definition at line
409
of file
command-interpreter2.h
.
◆ tokenCount
| uint8_t EmberCommandState::tokenCount |
Definition at line
421
of file
command-interpreter2.h
.
◆ tokenIndices
| uint8_t EmberCommandState::tokenIndices[ MAX_TOKEN_COUNT +1] |
Definition at line
418
of file
command-interpreter2.h
.
The documentation for this struct was generated from the following file:
-
command-interpreter2.h