Command Interpreter Plugin
Processes commands coming from the serial port. More...
Data Structures |
|
| struct | EmberCommandEntry |
|
Command entry for a command table.
More...
|
|
| struct | EmberCommandState |
|
For use when declaring a separate command streams. The fields are not accessed directly by the application.
More...
|
|
Macros |
|
| #define | MAX_TOKEN_COUNT ( EMBER_MAX_COMMAND_ARGUMENTS + 1) |
| #define | emberCommandEntryAction (name, command, arguments, description) { name, command, arguments, description } |
| #define | emberCommandEntrySubMenu (name, nestedCommands, description) { name, NULL , (PGM_P)nestedCommands, description } |
| #define | emberCommandEntryTerminator () { NULL , NULL , NULL , NULL } |
| #define | emberCommand emberCommandEntryAction |
| #define | emberNestedCommand emberCommandEntrySubMenu |
| #define | emberProcessCommandInput (port) emberProcessCommandString ( NULL , port) |
|
Process the input coming in on the given serial port.
More...
|
|
Typedefs |
|
| typedef void(* | CommandAction ) (void) |
| typedef void | EmberCommandErrorHandler ( EmberCommandStatus status, EmberCommandEntry *command) |
|
Type of error handlers; the command argument is currently always NULL.
More...
|
|
Functions |
|
| void | emberCommandErrorHandler ( EmberCommandStatus status, EmberCommandEntry *command) |
| void | emberPrintCommandUsage ( EmberCommandEntry *entry) |
| void | emberPrintCommandUsageNotes (void) |
| void | emberPrintCommandTable (void) |
| void | emberCommandClearBuffer (void) |
| void | emberCommandReaderInit (void) |
|
Initialize the command interpreter.
More...
|
|
| bool | emberProcessCommandString (const uint8_t *input, uint16_t sizeOrPort) |
|
Process the given string as a command.
More...
|
|
| uint8_t | emberHexToInt (uint8_t ch) |
|
Return the value of a hexadecimal digit ch (0 - 15). Returns a value > 15 if ch is not a hexadecimal digit.
More...
|
|
| bool | emberStringToIpAddress (const uint8_t *string, uint8_t stringLength, uint8_t *target) |
|
Parse textual representations of IPv6 addresses as described in
http://www.ietf.org/rfc/rfc4291.txt
.
More...
|
|
| bool | emberStringToIpPrefix (const uint8_t *string, uint8_t stringLength, uint8_t *target) |
|
Parse textual representations of IPv6 prefixes as described in
http://www.ietf.org/rfc/rfc4291.txt
.
More...
|
|
| void | emberInitializeCommandState ( EmberCommandState *state) |
|
Must be called to initialize a command state before passing it to
emberRunCommandInterpreter()
.
More...
|
|
| bool | emberRunCommandInterpreter (bool commandIsBinary, EmberCommandState *state, EmberCommandEntry *commands, EmberCommandErrorHandler *errorHandler, const uint8_t *input, uint16_t sizeOrPort) |
|
For use when additional different command streams are used.
More...
|
|
| void | emberCommandReaderSetDefaultBase (uint8_t base) |
Variables |
|
| EmberCommandEntry | emberCommandTable [] |
Command Table Settings |
|
| #define | EMBER_MAX_COMMAND_ARGUMENTS 20 |
| #define | EMBER_COMMAND_BUFFER_LENGTH 125 |
| #define | EMBER_CUSTOM_COMMAND_BUFFER_LENGTH ( EMBER_COMMAND_BUFFER_LENGTH - 3) |
| #define | EMBER_COMMAND_INTEPRETER_HAS_DESCRIPTION_FIELD |
Functions to Retrieve Arguments |
|
|
Use the following functions that process commands to retrieve arguments from the command interpreter. These functions pull out unsigned integers, signed integers, strings, and hexadecimal strings. Index 0 is the first command argument. |
|
| uint8_t | emberCommandArgumentCount (void) |
| uint32_t | emberUnsignedCommandArgument (uint8_t argNum) |
| int32_t | emberSignedCommandArgument (uint8_t argNum) |
| uint8_t * | emberStringCommandArgument (int8_t argNum, uint8_t *length) |
| const char * | emberCommandName (void) |
| uint8_t | emberGetStringArgument (int8_t argNum, uint8_t *destination, uint8_t maxLength, bool leftPad) |
| bool | emberGetIpArgument (uint8_t index, uint8_t *target) |
| bool | emberGetIpPrefixArgument (uint8_t index, uint8_t *target) |
| void | emberGetExtendedPanIdArgument (int8_t index, uint8_t *extendedPanId) |
| #define | emberCopyKeyArgument (index, keyDataPointer) |
| #define | emberCopyEui64Argument (index, eui64) ( emberGetStringArgument ((index), (eui64), EUI64_SIZE , TRUE )) |
| #define | emberGetKeyArgument (index, keyDataPointer) |
| #define | emberGetEui64Argument (index, eui64) emberGetExtendedPanIdArgument (index, (eui64)->bytes) |
Detailed Description
Processes commands coming from the serial port.
Interpret serial port commands. See command-interpreter2.c for source code.
See the following application usage example followed by a brief explanation.
-
Applications specify the commands that can be interpreted by defining the emberCommandTable array of type
EmberCommandEntry
. The table includes the following information for each command:
- The full command name.
- The application's function name that implements the command.
- An EmberCommandEntry::argumentTypes string specifies the number and types of arguments the command accepts.
- A description string explains the command.
- A default error handler emberCommandErrorHandler() is provided to deal with the incorrect command input. Applications may override it.
- The application calls emberCommandReaderInit() to initialize and emberProcessCommandInput() in its main loop.
- Within the application's command functions, use emberXXXCommandArgument() functions to retrieve command arguments.
The command interpreter does extensive processing and validation of the command input before calling the function that implements the command. It checks that the number, type, syntax, and range of all arguments is correct. It performs any conversions necessary, for example, converting integers and strings input in hexadecimal notation into the corresponding bytes so that no additional parsing is necessary within command functions. If an error occurs in the command input, emberCommandErrorHandler() is called instead of a command function.
The command interpreter allows inexact matches of command names. The input command may be either shorter or longer than the actual command. However, if more than one inexact match is found and there is no exact match, an error of type EMBER_CMD_ERR_NO_SUCH_COMMAND is generated. To disable this feature, define EMBER_REQUIRE_EXACT_COMMAND_NAME in the application configuration header.
Macro Definition Documentation
◆ EMBER_COMMAND_BUFFER_LENGTH
| #define EMBER_COMMAND_BUFFER_LENGTH 125 |
The maximum number of arguments a command can have. A nested command counts as an argument.
Definition at line
117
of file
command-interpreter2.h
.
◆ EMBER_COMMAND_INTEPRETER_HAS_DESCRIPTION_FIELD
| #define EMBER_COMMAND_INTEPRETER_HAS_DESCRIPTION_FIELD |
Indicate whether or not the command entry structure includes descriptions for the commands. This consumes additional CONST space, which is expensive on the XAP. By default, descriptions are not included.
Definition at line
130
of file
command-interpreter2.h
.
◆ EMBER_CUSTOM_COMMAND_BUFFER_LENGTH
| #define EMBER_CUSTOM_COMMAND_BUFFER_LENGTH ( EMBER_COMMAND_BUFFER_LENGTH - 3) |
The maximum message size for custom commands reserves three bytes for the length (1 bytes) and the custom command identifier (2 bytes).
Definition at line
123
of file
command-interpreter2.h
.
◆ EMBER_MAX_COMMAND_ARGUMENTS
| #define EMBER_MAX_COMMAND_ARGUMENTS 20 |
The maximum number of arguments a command can have. A nested command counts as an argument.
Definition at line
113
of file
command-interpreter2.h
.
◆ emberCommand
| #define emberCommand emberCommandEntryAction |
Definition at line
224
of file
command-interpreter2.h
.
◆ emberCommandEntryAction
| #define emberCommandEntryAction | ( |
name,
|
|
command,
|
|||
arguments,
|
|||
description
|
|||
| ) | { name, command, arguments, description } |
Definition at line
215
of file
command-interpreter2.h
.
◆ emberCommandEntrySubMenu
| #define emberCommandEntrySubMenu | ( |
name,
|
|
nestedCommands,
|
|||
description
|
|||
| ) | { name, NULL , (PGM_P)nestedCommands, description } |
Definition at line
217
of file
command-interpreter2.h
.
◆ emberCommandEntryTerminator
Definition at line
219
of file
command-interpreter2.h
.
◆ emberCopyEui64Argument
| #define emberCopyEui64Argument | ( |
index,
|
|
eui64
|
|||
| ) | ( emberGetStringArgument ((index), (eui64), EUI64_SIZE , TRUE )) |
A convenience macro for copying eui64 arguments to an EmberEUI64.
Definition at line
301
of file
command-interpreter2.h
.
◆ emberCopyKeyArgument
| #define emberCopyKeyArgument | ( |
index,
|
|
keyDataPointer
|
|||
| ) |
ember-types.h:48
A convenience macro for copying security key arguments to an EmberKeyData pointer.
Definition at line
294
of file
command-interpreter2.h
.
◆ emberGetEui64Argument
| #define emberGetEui64Argument | ( |
index,
|
|
eui64
|
|||
| ) | emberGetExtendedPanIdArgument (index, (eui64)->bytes) |
Copy the EUI64 argument to the given EmberEui64 destination reversing the bytes. EUI64's are stored little endian so reversing the bytes means they are big endian in the input command string.
Definition at line
348
of file
command-interpreter2.h
.
◆ emberGetKeyArgument
| #define emberGetKeyArgument | ( |
index,
|
|
keyDataPointer
|
|||
| ) |
ember-types.h:48
A convenience macro for copying security key arguments to an EmberKeyData pointer.
Definition at line
338
of file
command-interpreter2.h
.
◆ emberNestedCommand
| #define emberNestedCommand emberCommandEntrySubMenu |
Definition at line
225
of file
command-interpreter2.h
.
◆ emberProcessCommandInput
| #define emberProcessCommandInput | ( |
port
|
) | emberProcessCommandString ( NULL , port) |
Process the input coming in on the given serial port.
- Returns
-
true if an end of line character was read. If the application uses a command line prompt, this indicates it is time to print the prompt.
void emberProcessCommandInput (uint8_t port);
Definition at line
382
of file
command-interpreter2.h
.
◆ MAX_TOKEN_COUNT
| #define MAX_TOKEN_COUNT ( EMBER_MAX_COMMAND_ARGUMENTS + 1) |
Definition at line
136
of file
command-interpreter2.h
.
Typedef Documentation
◆ CommandAction
| typedef void(* CommandAction) (void) |
Definition at line
138
of file
command-interpreter2.h
.
◆ EmberCommandErrorHandler
| typedef void EmberCommandErrorHandler( EmberCommandStatus status, EmberCommandEntry *command) |
Type of error handlers; the command argument is currently always NULL.
Definition at line
455
of file
command-interpreter2.h
.
Enumeration Type Documentation
◆ EmberCommandStatus
| enum EmberCommandStatus |
Command error states.
If you change this list, also change the strings that describe these errors in the array emberCommandErrorNames[] in command-interpreter2-error.c.
Definition at line
236
of file
command-interpreter2.h
.
Function Documentation
◆ emberCommandArgumentCount()
| uint8_t emberCommandArgumentCount | ( | void |
|
) |
Returns the number of arguments for the current command.
◆ emberCommandClearBuffer()
| void emberCommandClearBuffer | ( | void |
|
) |
◆ emberCommandErrorHandler()
| void emberCommandErrorHandler | ( | EmberCommandStatus |
status,
|
| EmberCommandEntry * |
command
|
||
| ) |
◆ emberCommandName()
| const char* emberCommandName | ( | void |
|
) |
A convenience macro for copying security key arguments to an EmberKeyData pointer.
◆ emberCommandReaderInit()
| void emberCommandReaderInit | ( | void |
|
) |
Initialize the command interpreter.
◆ emberCommandReaderSetDefaultBase()
| void emberCommandReaderSetDefaultBase | ( | uint8_t |
base
|
) |
◆ emberGetExtendedPanIdArgument()
| void emberGetExtendedPanIdArgument | ( | int8_t |
index,
|
| uint8_t * |
extendedPanId
|
||
| ) |
Copy the extended PAN ID argument to the given destination, reversing the bytes. Extended PAN IDs are stored little endian so reversing the bytes means they are big endian in the input command string.
◆ emberGetIpArgument()
| bool emberGetIpArgument | ( | uint8_t |
index,
|
| uint8_t * |
target
|
||
| ) |
Parse and return, via target, an IP address at the provided index. Returns true if an IP address was successfully parsed Returns false otherwise.
◆ emberGetIpPrefixArgument()
| bool emberGetIpPrefixArgument | ( | uint8_t |
index,
|
| uint8_t * |
target
|
||
| ) |
Parse and return, via target, an IP prefix at the provided index. Returns true if an IP prefix was successfully parsed. Returns false otherwise.
◆ emberGetStringArgument()
| uint8_t emberGetStringArgument | ( | int8_t |
argNum,
|
| uint8_t * |
destination,
|
||
| uint8_t |
maxLength,
|
||
| bool |
leftPad
|
||
| ) |
Copy the string argument to the given destination up to maxLength. If the argument length is not zero but less than maxLength and leftPad is true, leading zeroes are prepended to bring the total length of the target up to maxLength. If the argument is longer than the maxLength, it is truncated to maxLength. Returns the minimum of the argument length and maxLength. ASCII strings are null terminated but the null terminator is not included in the returned length.
This function is commonly used for reading in hexadecimal strings, such as EUI64 or key data and left padding them with zeros. See emberGetKeyArgument and emberGetEui64Argument for convenience macros for this purpose.
◆ emberHexToInt()
| uint8_t emberHexToInt | ( | uint8_t |
ch
|
) |
Return the value of a hexadecimal digit ch (0 - 15). Returns a value > 15 if ch is not a hexadecimal digit.
◆ emberInitializeCommandState()
| void emberInitializeCommandState | ( | EmberCommandState * |
state
|
) |
Must be called to initialize a command state before passing it to emberRunCommandInterpreter() .
◆ emberPrintCommandTable()
| void emberPrintCommandTable | ( | void |
|
) |
◆ emberPrintCommandUsage()
| void emberPrintCommandUsage | ( | EmberCommandEntry * |
entry
|
) |
◆ emberPrintCommandUsageNotes()
| void emberPrintCommandUsageNotes | ( | void |
|
) |
◆ emberProcessCommandString()
| bool emberProcessCommandString | ( | const uint8_t * |
input,
|
| uint16_t |
sizeOrPort
|
||
| ) |
Process the given string as a command.
◆ emberRunCommandInterpreter()
| bool emberRunCommandInterpreter | ( | bool |
commandIsBinary,
|
| EmberCommandState * |
state,
|
||
| EmberCommandEntry * |
commands,
|
||
| EmberCommandErrorHandler * |
errorHandler,
|
||
| const uint8_t * |
input,
|
||
| uint16_t |
sizeOrPort
|
||
| ) |
For use when additional different command streams are used.
◆ emberSignedCommandArgument()
| int32_t emberSignedCommandArgument | ( | uint8_t |
argNum
|
) |
Retrieve signed integer arguments.
◆ emberStringCommandArgument()
| uint8_t* emberStringCommandArgument | ( | int8_t |
argNum,
|
| uint8_t * |
length
|
||
| ) |
Retrieve quoted string or hexadecimal string arguments. Hexadecimal strings are already converted into binary. ASCII strings are null terminated. The null terminator is not included in the returned length argument. To retrieve the name of the command itself, use an argNum of -1. For example, to retrieve the first character of the command, uint8_t firstChar = emberStringCommandArgument(-1, NULL)[0]. If the command is nested, an index of -2, -3, and so on retrieves the higher level command names. Note that [-1] only returns the text entered. If an abbreviated command name is entered, only the text entered will be returned with [-1].
◆ emberStringToIpAddress()
| bool emberStringToIpAddress | ( | const uint8_t * |
string,
|
| uint8_t |
stringLength,
|
||
| uint8_t * |
target
|
||
| ) |
Parse textual representations of IPv6 addresses as described in http://www.ietf.org/rfc/rfc4291.txt .
◆ emberStringToIpPrefix()
| bool emberStringToIpPrefix | ( | const uint8_t * |
string,
|
| uint8_t |
stringLength,
|
||
| uint8_t * |
target
|
||
| ) |
Parse textual representations of IPv6 prefixes as described in http://www.ietf.org/rfc/rfc4291.txt .
◆ emberUnsignedCommandArgument()
| uint32_t emberUnsignedCommandArgument | ( | uint8_t |
argNum
|
) |
Retrieves unsigned integer arguments.
Variable Documentation
◆ emberCommandTable
| EmberCommandEntry emberCommandTable[] |