Compiler and Platform specific definitions and typedefs for the IAR ARM C compiler. More...

Macros

#define HAL_HAS_INT64
Denotes that this platform supports 64-bit data-types. More...
#define _HAL_USE_COMMON_PGM_
Use the Master Program Memory Declarations from platform-common.h . More...
#define PLATCOMMONOKTOINCLUDE
Include platform-common.h last to pick up defaults and common definitions. More...
#define MAIN_FUNCTION_PARAMETERS void
The kind of arguments the main function takes. More...
#define MAIN_FUNCTION_ARGUMENTS

Functions

void _executeBarrierInstructions (void)

Master Variable Types

LEGACY_PHY_BUILD

These are a set of typedefs to make the size of all variable declarations explicitly known.

typedef bool boolean
A typedef to make the size of the variable explicitly known. More...
typedef unsigned char int8u
A typedef to make the size of the variable explicitly known. More...
typedef signed char int8s
A typedef to make the size of the variable explicitly known. More...
typedef unsigned short int16u
A typedef to make the size of the variable explicitly known. More...
typedef signed short int16s
A typedef to make the size of the variable explicitly known. More...
typedef unsigned int int32u
A typedef to make the size of the variable explicitly known. More...
typedef signed int int32s
A typedef to make the size of the variable explicitly known. More...
typedef unsigned long long int64u
A typedef to make the size of the variable explicitly known. More...
typedef signed long long int64s
A typedef to make the size of the variable explicitly known. More...
typedef unsigned int PointerType
A typedef to make the size of the variable explicitly known. More...

Miscellaneous Macros

void halInternalAssertFailed (const char *filename, int linenumber)
A prototype definition for use by the assert macro. (see hal/micro/micro.h ) More...
void halInternalResetWatchDog (void)
Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful. More...
#define BIGENDIAN_CPU false
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian. More...
#define NTOHS (val) (__REV16(val))
Define intrinsics for NTOHL and NTOHS to save code space by making endian.c compile to nothing. More...
#define NTOHL (val) (__REV(val))
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian. More...
#define NO_STRIPPING __root
A friendlier name for the compiler's intrinsic for not stripping. More...
#define EEPROM errorerror
A friendlier name for the compiler's intrinsic for eeprom reference. More...
#define __SOURCEFILE__ __FILE__
The SOURCEFILE macro is used by asserts to list the filename if it isn't otherwise defined, set it to the compiler intrinsic which specifies the whole filename and path of the sourcefile. More...
#define assert (condition)
A custom implementation of the C language assert macro. This macro implements the conditional evaluation and calls the function halInternalAssertFailed() . (see hal/micro/micro.h ) More...
#define halResetWatchdog () halInternalResetWatchDog ()
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian. More...
#define UNUSED
Declare a variable as unused to avoid a warning. Has no effect in IAR builds. More...
#define SIGNED_ENUM
Some platforms need to cast enum values that have the high bit set. More...
#define STACK_FILL_VALUE 0xCDCDCDCDU
Define the magic value that is interpreted by IAR C-SPY's Stack View. More...
#define RAMFUNC __ramfunc
Define a generic RAM function identifier to a compiler specific one. More...
#define NO_OPERATION () __NOP()
Define a generic no operation identifier to a compiler specific one. More...
#define SET_REG_FIELD (reg, field, value)
A convenience macro that makes it easy to change the field of a register to any unsigned value. More...
#define SET_CMSIS_REG (reg, mask, value)
A convenience macro that makes it easy to change a register using the provided mask(s) and value(s). Example: SET_CMSIS_REG(GPIO->P[1].CFGH, (_GPIO_P_CFGH_Px5_MASK | _GPIO_P_CFGH_Px6_MASK), (GPIO_P_CFGH_Px5_OUT | GPIO_P_CFGH_Px6_OUT));. More...
#define SET_CMSIS_REG_FIELD (reg, field, value)
A convenience macro that makes it easy to change the field of a register, as defined in CMSIS Device headers, to any unsigned value. Example using EM35xx: SET_CMSIS_REG_FIELD(GPIO->P[0].CFGL, GPIO_P_CFGL_Px0, _GPIO_P_CFGL_Px0_OUT);. More...
#define simulatedTimePasses ()
Stub for code not running in simulation. More...
#define simulatedTimePassesMs (x)
Stub for code not running in simulation. More...
#define simulatedSerialTimePasses ()
Stub for code not running in simulation. More...
#define _HAL_USE_COMMON_DIVMOD_
Use the Divide and Modulus Operations from platform-common.h . More...
#define VAR_AT_SEGMENT (__variableDeclaration, __segmentName) __variableDeclaration @ __segmentName
Provide a portable way to specify the segment where a variable lives. More...
#define STRINGIZE (X) #X
Convinience macro for turning a token into a string. More...
#define ALIGNMENT (X) _Pragma( STRINGIZE (data_alignment = X))
Provide a portable way to align data. More...
#define WEAK (__symbol) __weak __symbol
Provide a portable way to specify a symbol as weak. More...
#define NO_INIT (__symbol) __no_init __symbol
Provide a portable way to specify a non initialized symbol. More...
#define STATIC_ASSERT (__condition, __errorstr) static_assert(__condition, __errorstr)
Provide a portable way to specify a compile time assert. More...

Portable segment names

#define __NO_INIT__ ".noinitlegacy"
Portable segment names. More...
#define __DEBUG_CHANNEL__ "DEBUG_CHANNEL"
Portable segment names. More...
#define __INTVEC__ ".intvec"
Portable segment names. More...
#define __CSTACK__ "CSTACK"
Portable segment names. More...
#define __RESETINFO__ "RESETINFO"
Portable segment names. More...
#define __DATA_INIT__ ".data_init"
Portable segment names. More...
#define __DATA__ ".data"
Portable segment names. More...
#define __BSS__ ".bss"
Portable segment names. More...
#define __CONST__ ".rodata"
Portable segment names. More...
#define __TEXT__ ".text"
Portable segment names. More...
#define __TEXTRW_INIT__ ".textrw_init"
Portable segment names. More...
#define __TEXTRW__ ".textrw"
Portable segment names. More...
#define __AAT__ "AAT"
Portable segment names. More...
#define __BAT__ "BAT"
Portable segment names. More...
#define __BAT_INIT__ "BAT"
Portable segment names. More...
#define __FAT__ "FAT"
Portable segment names. More...
#define __RAT__ "RAT"
Portable segment names. More...
#define __SIMEE__ "SIMEE"
Portable segment names. More...
#define __PSSTORE__ "PSSTORE"
Portable segment names. More...
#define __LONGTOKEN__ "LONGTOKEN"
Portable segment names. More...
#define __EMHEAP__ "EMHEAP"
Portable segment names. More...
#define __GUARD_REGION__ "GUARD_REGION"
Portable segment names. More...
#define __DLIB_PERTHREAD_INIT__ "__DLIB_PERTHREAD_init"
Portable segment names. More...
#define __DLIB_PERTHREAD_INITIALIZED_DATA__ "DLIB_PERTHREAD_INITIALIZED_DATA"
Portable segment names. More...
#define __DLIB_PERTHREAD_ZERO_DATA__ "DLIB_PERTHREAD_ZERO_DATA"
Portable segment names. More...
#define __INTERNAL_STORAGE__ "INTERNAL_STORAGE"
Portable segment names. More...
#define __LOCKBITS_IN_MAINFLASH__ "LOCKBITS_IN_MAINFLASH"
Portable segment names. More...
#define __UNRETAINED_RAM__ "UNRETAINED_RAM"
Portable segment names. More...
#define _NO_INIT_SEGMENT_BEGIN __segment_begin( __NO_INIT__ )
Portable segment names. More...
#define _DEBUG_CHANNEL_SEGMENT_BEGIN __segment_begin( __DEBUG_CHANNEL__ )
Portable segment names. More...
#define _INTVEC_SEGMENT_BEGIN __segment_begin( __INTVEC__ )
Portable segment names. More...
#define _CSTACK_SEGMENT_BEGIN __segment_begin( __CSTACK__ )
Portable segment names. More...
#define _RESETINFO_SEGMENT_BEGIN __segment_begin( __RESETINFO__ )
Portable segment names. More...
#define _DATA_INIT_SEGMENT_BEGIN __segment_begin( __DATA_INIT__ )
Portable segment names. More...
#define _DATA_SEGMENT_BEGIN __segment_begin( __DATA__ )
Portable segment names. More...
#define _BSS_SEGMENT_BEGIN __segment_begin( __BSS__ )
Portable segment names. More...
#define _CONST_SEGMENT_BEGIN __segment_begin( __CONST__ )
Portable segment names. More...
#define _TEXT_SEGMENT_BEGIN __segment_begin( __TEXT__ )
Portable segment names. More...
#define _TEXTRW_INIT_SEGMENT_BEGIN __segment_begin( __TEXTRW_INIT__ )
Portable segment names. More...
#define _TEXTRW_SEGMENT_BEGIN __segment_begin( __TEXTRW__ )
Portable segment names. More...
#define _AAT_SEGMENT_BEGIN __segment_begin( __AAT__ )
Portable segment names. More...
#define _BAT_SEGMENT_BEGIN __segment_begin( __BAT__ )
Portable segment names. More...
#define _BAT_INIT_SEGMENT_BEGIN __segment_begin( __BAT_INIT__ )
Portable segment names. More...
#define _FAT_SEGMENT_BEGIN __segment_begin( __FAT__ )
Portable segment names. More...
#define _RAT_SEGMENT_BEGIN __segment_begin( __RAT__ )
Portable segment names. More...
#define _SIMEE_SEGMENT_BEGIN __segment_begin( __SIMEE__ )
Portable segment names. More...
#define _PSSTORE_SEGMENT_BEGIN __segment_begin( __PSSTORE__ )
Portable segment names. More...
#define _LONGTOKEN_SEGMENT_BEGIN __segment_begin( __LONGTOKEN__ )
Portable segment names. More...
#define _EMHEAP_SEGMENT_BEGIN __segment_begin( __EMHEAP__ )
Portable segment names. More...
#define _GUARD_REGION_SEGMENT_BEGIN __segment_begin( __GUARD_REGION__ )
Portable segment names. More...
#define _DLIB_PERTHREAD_INIT_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_INIT__ )
Portable segment names. More...
#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_INITIALIZED_DATA__ )
Portable segment names. More...
#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_ZERO_DATA__ )
Portable segment names. More...
#define _INTERNAL_STORAGE_SEGMENT_BEGIN __segment_begin( __INTERNAL_STORAGE__ )
Portable segment names. More...
#define _LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN __segment_begin( __LOCKBITS_IN_MAINFLASH__ )
Portable segment names. More...
#define _UNRETAINED_RAM_SEGMENT_BEGIN __segment_begin( __UNRETAINED_RAM__ )
Portable segment names. More...
#define _NO_INIT_SEGMENT_END __segment_end( __NO_INIT__ )
Portable segment names. More...
#define _DEBUG_CHANNEL_SEGMENT_END __segment_end( __DEBUG_CHANNEL__ )
Portable segment names. More...
#define _INTVEC_SEGMENT_END __segment_end( __INTVEC__ )
Portable segment names. More...
#define _CSTACK_SEGMENT_END __segment_end( __CSTACK__ )
Portable segment names. More...
#define _RESETINFO_SEGMENT_END __segment_end( __RESETINFO__ )
Portable segment names. More...
#define _DATA_INIT_SEGMENT_END __segment_end( __DATA_INIT__ )
Portable segment names. More...
#define _DATA_SEGMENT_END __segment_end( __DATA__ )
Portable segment names. More...
#define _BSS_SEGMENT_END __segment_end( __BSS__ )
Portable segment names. More...
#define _CONST_SEGMENT_END __segment_end( __CONST__ )
Portable segment names. More...
#define _TEXT_SEGMENT_END __segment_end( __TEXT__ )
Portable segment names. More...
#define _TEXTRW_INIT_SEGMENT_END __segment_end( __TEXTRW_INIT__ )
Portable segment names. More...
#define _TEXTRW_SEGMENT_END __segment_end( __TEXTRW__ )
Portable segment names. More...
#define _AAT_SEGMENT_END __segment_end( __AAT__ )
Portable segment names. More...
#define _BAT_SEGMENT_END __segment_end( __BAT__ )
Portable segment names. More...
#define _BAT_INIT_SEGMENT_END __segment_end( __BAT_INIT__ )
Portable segment names. More...
#define _FAT_SEGMENT_END __segment_end( __FAT__ )
Portable segment names. More...
#define _RAT_SEGMENT_END __segment_end( __RAT__ )
Portable segment names. More...
#define _SIMEE_SEGMENT_END __segment_end( __SIMEE__ )
Portable segment names. More...
#define _PSSTORE_SEGMENT_END __segment_end( __PSSTORE__ )
Portable segment names. More...
#define _LONGTOKEN_SEGMENT_END __segment_end( __LONGTOKEN__ )
Portable segment names. More...
#define _EMHEAP_SEGMENT_END __segment_end( __EMHEAP__ )
Portable segment names. More...
#define _GUARD_REGION_SEGMENT_END __segment_end( __GUARD_REGION__ )
Portable segment names. More...
#define _DLIB_PERTHREAD_INIT_SEGMENT_END __segment_end( __DLIB_PERTHREAD_INIT__ )
Portable segment names. More...
#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END __segment_end( __DLIB_PERTHREAD_INITIALIZED_DATA__ )
Portable segment names. More...
#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END __segment_end( __DLIB_PERTHREAD_ZERO_DATA__ )
Portable segment names. More...
#define _INTERNAL_STORAGE_SEGMENT_END __segment_end( __INTERNAL_STORAGE__ )
Portable segment names. More...
#define _LOCKBITS_IN_MAINFLASH_SEGMENT_END __segment_end( __LOCKBITS_IN_MAINFLASH__ )
Portable segment names. More...
#define _UNRETAINED_RAM_SEGMENT_END __segment_end( __UNRETAINED_RAM__ )
Portable segment names. More...
#define _NO_INIT_SEGMENT_SIZE __segment_size( __NO_INIT__ )
Portable segment names. More...
#define _DEBUG_CHANNEL_SEGMENT_SIZE __segment_size( __DEBUG_CHANNEL__ )
Portable segment names. More...
#define _INTVEC_SEGMENT_SIZE __segment_size( __INTVEC__ )
Portable segment names. More...
#define _CSTACK_SEGMENT_SIZE __segment_size( __CSTACK__ )
Portable segment names. More...
#define _RESETINFO_SEGMENT_SIZE __segment_size( __RESETINFO__ )
Portable segment names. More...
#define _DATA_INIT_SEGMENT_SIZE __segment_size( __DATA_INIT__ )
Portable segment names. More...
#define _DATA_SEGMENT_SIZE __segment_size( __DATA__ )
Portable segment names. More...
#define _BSS_SEGMENT_SIZE __segment_size( __BSS__ )
Portable segment names. More...
#define _CONST_SEGMENT_SIZE __segment_size( __CONST__ )
Portable segment names. More...
#define _TEXT_SEGMENT_SIZE __segment_size( __TEXT__ )
Portable segment names. More...
#define _TEXTRW_INIT_SEGMENT_SIZE __segment_size( __TEXTRW_INIT__ )
Portable segment names. More...
#define _TEXTRW_SEGMENT_SIZE __segment_size( __TEXTRW__ )
Portable segment names. More...
#define _AAT_SEGMENT_SIZE __segment_size( __AAT__ )
Portable segment names. More...
#define _BAT_SEGMENT_SIZE __segment_size( __BAT__ )
Portable segment names. More...
#define _BAT_INIT_SEGMENT_SIZE __segment_size( __BAT_INIT__ )
Portable segment names. More...
#define _FAT_SEGMENT_SIZE __segment_size( __FAT__ )
Portable segment names. More...
#define _RAT_SEGMENT_SIZE __segment_size( __RAT__ )
Portable segment names. More...
#define _SIMEE_SEGMENT_SIZE __segment_size( __SIMEE__ )
Portable segment names. More...
#define _PSSTORE_SEGMENT_SIZE __segment_size( __PSSTORE__ )
Portable segment names. More...
#define _LONGTOKEN_SEGMENT_SIZE __segment_size( __LONGTOKEN__ )
Portable segment names. More...
#define _EMHEAP_SEGMENT_SIZE __segment_size( __EMHEAP__ )
Portable segment names. More...
#define _GUARD_REGION_SEGMENT_SIZE __segment_size( __GUARD_REGION__ )
Portable segment names. More...
#define _DLIB_PERTHREAD_INIT_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_INIT__ )
Portable segment names. More...
#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_INITIALIZED_DATA__ )
Portable segment names. More...
#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_ZERO_DATA__ )
Portable segment names. More...
#define _INTERNAL_STORAGE_SEGMENT_SIZE __segment_size( __INTERNAL_STORAGE__ )
Portable segment names. More...
#define _LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE __segment_size( __LOCKBITS_IN_MAINFLASH__ )
Portable segment names. More...
#define _UNRETAINED_RAM_SEGMENT_SIZE __segment_size( __UNRETAINED_RAM__ )
Portable segment names. More...

External Declarations

If the line below is uncommented we will use Ember memory APIs, otherwise, we will use the C Standard library (memset,memcpy,memmove) APIs.

These are routines that are defined in certain header files that we don't want to include, e.g. stdlib.h

int abs (int I)
Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I. More...

Detailed Description

Compiler and Platform specific definitions and typedefs for the IAR ARM C compiler.

Note
iar.h should be included first in all source files by setting the preprocessor macro PLATFORM_HEADER to point to it. iar.h automatically includes platform-common.h .

See iar.h and platform-common.h for source code.

Macro Definition Documentation

◆ __AAT__

#define __AAT__ "AAT"

Portable segment names.

Definition at line 355 of file iar.h .

◆ __BAT__

#define __BAT__ "BAT"

Portable segment names.

Definition at line 356 of file iar.h .

◆ __BAT_INIT__

#define __BAT_INIT__ "BAT"

Portable segment names.

Definition at line 357 of file iar.h .

◆ __BSS__

#define __BSS__ ".bss"

Portable segment names.

Definition at line 350 of file iar.h .

◆ __CONST__

#define __CONST__ ".rodata"

Portable segment names.

Definition at line 351 of file iar.h .

◆ __CSTACK__

#define __CSTACK__ "CSTACK"

Portable segment names.

Definition at line 346 of file iar.h .

◆ __DATA__

#define __DATA__ ".data"

Portable segment names.

Definition at line 349 of file iar.h .

◆ __DATA_INIT__

#define __DATA_INIT__ ".data_init"

Portable segment names.

Definition at line 348 of file iar.h .

◆ __DEBUG_CHANNEL__

#define __DEBUG_CHANNEL__ "DEBUG_CHANNEL"

Portable segment names.

Definition at line 344 of file iar.h .

◆ __DLIB_PERTHREAD_INIT__

#define __DLIB_PERTHREAD_INIT__ "__DLIB_PERTHREAD_init"

Portable segment names.

Definition at line 365 of file iar.h .

◆ __DLIB_PERTHREAD_INITIALIZED_DATA__

#define __DLIB_PERTHREAD_INITIALIZED_DATA__ "DLIB_PERTHREAD_INITIALIZED_DATA"

Portable segment names.

Definition at line 366 of file iar.h .

◆ __DLIB_PERTHREAD_ZERO_DATA__

#define __DLIB_PERTHREAD_ZERO_DATA__ "DLIB_PERTHREAD_ZERO_DATA"

Portable segment names.

Definition at line 367 of file iar.h .

◆ __EMHEAP__

#define __EMHEAP__ "EMHEAP"

Portable segment names.

Definition at line 363 of file iar.h .

◆ __FAT__

#define __FAT__ "FAT"

Portable segment names.

Definition at line 358 of file iar.h .

◆ __GUARD_REGION__

#define __GUARD_REGION__ "GUARD_REGION"

Portable segment names.

Definition at line 364 of file iar.h .

◆ __INTERNAL_STORAGE__

#define __INTERNAL_STORAGE__ "INTERNAL_STORAGE"

Portable segment names.

Definition at line 368 of file iar.h .

◆ __INTVEC__

#define __INTVEC__ ".intvec"

Portable segment names.

Definition at line 345 of file iar.h .

◆ __LOCKBITS_IN_MAINFLASH__

#define __LOCKBITS_IN_MAINFLASH__ "LOCKBITS_IN_MAINFLASH"

Portable segment names.

Definition at line 369 of file iar.h .

◆ __LONGTOKEN__

#define __LONGTOKEN__ "LONGTOKEN"

Portable segment names.

Definition at line 362 of file iar.h .

◆ __NO_INIT__

#define __NO_INIT__ ".noinitlegacy"

Portable segment names.

Definition at line 341 of file iar.h .

◆ __PSSTORE__

#define __PSSTORE__ "PSSTORE"

Portable segment names.

Definition at line 361 of file iar.h .

◆ __RAT__

#define __RAT__ "RAT"

Portable segment names.

Definition at line 359 of file iar.h .

◆ __RESETINFO__

#define __RESETINFO__ "RESETINFO"

Portable segment names.

Definition at line 347 of file iar.h .

◆ __SIMEE__

#define __SIMEE__ "SIMEE"

Portable segment names.

Definition at line 360 of file iar.h .

◆ __SOURCEFILE__

#define __SOURCEFILE__ __FILE__

The SOURCEFILE macro is used by asserts to list the filename if it isn't otherwise defined, set it to the compiler intrinsic which specifies the whole filename and path of the sourcefile.

Definition at line 143 of file iar.h .

◆ __TEXT__

#define __TEXT__ ".text"

Portable segment names.

Definition at line 352 of file iar.h .

◆ __TEXTRW__

#define __TEXTRW__ ".textrw"

Portable segment names.

Definition at line 354 of file iar.h .

◆ __TEXTRW_INIT__

#define __TEXTRW_INIT__ ".textrw_init"

Portable segment names.

Definition at line 353 of file iar.h .

◆ __UNRETAINED_RAM__

#define __UNRETAINED_RAM__ "UNRETAINED_RAM"

Portable segment names.

Definition at line 370 of file iar.h .

◆ _AAT_SEGMENT_BEGIN

#define _AAT_SEGMENT_BEGIN __segment_begin( __AAT__ )

Portable segment names.

Definition at line 420 of file iar.h .

◆ _AAT_SEGMENT_END

#define _AAT_SEGMENT_END __segment_end( __AAT__ )

Portable segment names.

Definition at line 449 of file iar.h .

◆ _AAT_SEGMENT_SIZE

#define _AAT_SEGMENT_SIZE __segment_size( __AAT__ )

Portable segment names.

Definition at line 478 of file iar.h .

◆ _BAT_INIT_SEGMENT_BEGIN

#define _BAT_INIT_SEGMENT_BEGIN __segment_begin( __BAT_INIT__ )

Portable segment names.

Definition at line 422 of file iar.h .

◆ _BAT_INIT_SEGMENT_END

#define _BAT_INIT_SEGMENT_END __segment_end( __BAT_INIT__ )

Portable segment names.

Definition at line 451 of file iar.h .

◆ _BAT_INIT_SEGMENT_SIZE

#define _BAT_INIT_SEGMENT_SIZE __segment_size( __BAT_INIT__ )

Portable segment names.

Definition at line 480 of file iar.h .

◆ _BAT_SEGMENT_BEGIN

#define _BAT_SEGMENT_BEGIN __segment_begin( __BAT__ )

Portable segment names.

Definition at line 421 of file iar.h .

◆ _BAT_SEGMENT_END

#define _BAT_SEGMENT_END __segment_end( __BAT__ )

Portable segment names.

Definition at line 450 of file iar.h .

◆ _BAT_SEGMENT_SIZE

#define _BAT_SEGMENT_SIZE __segment_size( __BAT__ )

Portable segment names.

Definition at line 479 of file iar.h .

◆ _BSS_SEGMENT_BEGIN

#define _BSS_SEGMENT_BEGIN __segment_begin( __BSS__ )

Portable segment names.

Definition at line 415 of file iar.h .

◆ _BSS_SEGMENT_END

#define _BSS_SEGMENT_END __segment_end( __BSS__ )

Portable segment names.

Definition at line 444 of file iar.h .

◆ _BSS_SEGMENT_SIZE

#define _BSS_SEGMENT_SIZE __segment_size( __BSS__ )

Portable segment names.

Definition at line 473 of file iar.h .

◆ _CONST_SEGMENT_BEGIN

#define _CONST_SEGMENT_BEGIN __segment_begin( __CONST__ )

Portable segment names.

Definition at line 416 of file iar.h .

◆ _CONST_SEGMENT_END

#define _CONST_SEGMENT_END __segment_end( __CONST__ )

Portable segment names.

Definition at line 445 of file iar.h .

◆ _CONST_SEGMENT_SIZE

#define _CONST_SEGMENT_SIZE __segment_size( __CONST__ )

Portable segment names.

Definition at line 474 of file iar.h .

◆ _CSTACK_SEGMENT_BEGIN

#define _CSTACK_SEGMENT_BEGIN __segment_begin( __CSTACK__ )

Portable segment names.

Definition at line 411 of file iar.h .

◆ _CSTACK_SEGMENT_END

#define _CSTACK_SEGMENT_END __segment_end( __CSTACK__ )

Portable segment names.

Definition at line 440 of file iar.h .

◆ _CSTACK_SEGMENT_SIZE

#define _CSTACK_SEGMENT_SIZE __segment_size( __CSTACK__ )

Portable segment names.

Definition at line 469 of file iar.h .

◆ _DATA_INIT_SEGMENT_BEGIN

#define _DATA_INIT_SEGMENT_BEGIN __segment_begin( __DATA_INIT__ )

Portable segment names.

Definition at line 413 of file iar.h .

◆ _DATA_INIT_SEGMENT_END

#define _DATA_INIT_SEGMENT_END __segment_end( __DATA_INIT__ )

Portable segment names.

Definition at line 442 of file iar.h .

◆ _DATA_INIT_SEGMENT_SIZE

#define _DATA_INIT_SEGMENT_SIZE __segment_size( __DATA_INIT__ )

Portable segment names.

Definition at line 471 of file iar.h .

◆ _DATA_SEGMENT_BEGIN

#define _DATA_SEGMENT_BEGIN __segment_begin( __DATA__ )

Portable segment names.

Definition at line 414 of file iar.h .

◆ _DATA_SEGMENT_END

#define _DATA_SEGMENT_END __segment_end( __DATA__ )

Portable segment names.

Definition at line 443 of file iar.h .

◆ _DATA_SEGMENT_SIZE

#define _DATA_SEGMENT_SIZE __segment_size( __DATA__ )

Portable segment names.

Definition at line 472 of file iar.h .

◆ _DEBUG_CHANNEL_SEGMENT_BEGIN

#define _DEBUG_CHANNEL_SEGMENT_BEGIN __segment_begin( __DEBUG_CHANNEL__ )

Portable segment names.

Definition at line 409 of file iar.h .

◆ _DEBUG_CHANNEL_SEGMENT_END

#define _DEBUG_CHANNEL_SEGMENT_END __segment_end( __DEBUG_CHANNEL__ )

Portable segment names.

Definition at line 438 of file iar.h .

◆ _DEBUG_CHANNEL_SEGMENT_SIZE

#define _DEBUG_CHANNEL_SEGMENT_SIZE __segment_size( __DEBUG_CHANNEL__ )

Portable segment names.

Definition at line 467 of file iar.h .

◆ _DLIB_PERTHREAD_INIT_SEGMENT_BEGIN

#define _DLIB_PERTHREAD_INIT_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_INIT__ )

Portable segment names.

Definition at line 430 of file iar.h .

◆ _DLIB_PERTHREAD_INIT_SEGMENT_END

#define _DLIB_PERTHREAD_INIT_SEGMENT_END __segment_end( __DLIB_PERTHREAD_INIT__ )

Portable segment names.

Definition at line 459 of file iar.h .

◆ _DLIB_PERTHREAD_INIT_SEGMENT_SIZE

#define _DLIB_PERTHREAD_INIT_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_INIT__ )

Portable segment names.

Definition at line 488 of file iar.h .

◆ _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN

#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_INITIALIZED_DATA__ )

Portable segment names.

Definition at line 431 of file iar.h .

◆ _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END

#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END __segment_end( __DLIB_PERTHREAD_INITIALIZED_DATA__ )

Portable segment names.

Definition at line 460 of file iar.h .

◆ _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE

#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_INITIALIZED_DATA__ )

Portable segment names.

Definition at line 489 of file iar.h .

◆ _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN

#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_ZERO_DATA__ )

Portable segment names.

Definition at line 432 of file iar.h .

◆ _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END

#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END __segment_end( __DLIB_PERTHREAD_ZERO_DATA__ )

Portable segment names.

Definition at line 461 of file iar.h .

◆ _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE

#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_ZERO_DATA__ )

Portable segment names.

Definition at line 490 of file iar.h .

◆ _EMHEAP_SEGMENT_BEGIN

#define _EMHEAP_SEGMENT_BEGIN __segment_begin( __EMHEAP__ )

Portable segment names.

Definition at line 428 of file iar.h .

◆ _EMHEAP_SEGMENT_END

#define _EMHEAP_SEGMENT_END __segment_end( __EMHEAP__ )

Portable segment names.

Definition at line 457 of file iar.h .

◆ _EMHEAP_SEGMENT_SIZE

#define _EMHEAP_SEGMENT_SIZE __segment_size( __EMHEAP__ )

Portable segment names.

Definition at line 486 of file iar.h .

◆ _FAT_SEGMENT_BEGIN

#define _FAT_SEGMENT_BEGIN __segment_begin( __FAT__ )

Portable segment names.

Definition at line 423 of file iar.h .

◆ _FAT_SEGMENT_END

#define _FAT_SEGMENT_END __segment_end( __FAT__ )

Portable segment names.

Definition at line 452 of file iar.h .

◆ _FAT_SEGMENT_SIZE

#define _FAT_SEGMENT_SIZE __segment_size( __FAT__ )

Portable segment names.

Definition at line 481 of file iar.h .

◆ _GUARD_REGION_SEGMENT_BEGIN

#define _GUARD_REGION_SEGMENT_BEGIN __segment_begin( __GUARD_REGION__ )

Portable segment names.

Definition at line 429 of file iar.h .

◆ _GUARD_REGION_SEGMENT_END

#define _GUARD_REGION_SEGMENT_END __segment_end( __GUARD_REGION__ )

Portable segment names.

Definition at line 458 of file iar.h .

◆ _GUARD_REGION_SEGMENT_SIZE

#define _GUARD_REGION_SEGMENT_SIZE __segment_size( __GUARD_REGION__ )

Portable segment names.

Definition at line 487 of file iar.h .

◆ _HAL_USE_COMMON_DIVMOD_

#define _HAL_USE_COMMON_DIVMOD_

Use the Divide and Modulus Operations from platform-common.h .

Definition at line 283 of file iar.h .

◆ _HAL_USE_COMMON_PGM_

#define _HAL_USE_COMMON_PGM_

Use the Master Program Memory Declarations from platform-common.h .

Definition at line 102 of file iar.h .

◆ _INTERNAL_STORAGE_SEGMENT_BEGIN

#define _INTERNAL_STORAGE_SEGMENT_BEGIN __segment_begin( __INTERNAL_STORAGE__ )

Portable segment names.

Definition at line 433 of file iar.h .

◆ _INTERNAL_STORAGE_SEGMENT_END

#define _INTERNAL_STORAGE_SEGMENT_END __segment_end( __INTERNAL_STORAGE__ )

Portable segment names.

Definition at line 462 of file iar.h .

◆ _INTERNAL_STORAGE_SEGMENT_SIZE

#define _INTERNAL_STORAGE_SEGMENT_SIZE __segment_size( __INTERNAL_STORAGE__ )

Portable segment names.

Definition at line 491 of file iar.h .

◆ _INTVEC_SEGMENT_BEGIN

#define _INTVEC_SEGMENT_BEGIN __segment_begin( __INTVEC__ )

Portable segment names.

Definition at line 410 of file iar.h .

◆ _INTVEC_SEGMENT_END

#define _INTVEC_SEGMENT_END __segment_end( __INTVEC__ )

Portable segment names.

Definition at line 439 of file iar.h .

◆ _INTVEC_SEGMENT_SIZE

#define _INTVEC_SEGMENT_SIZE __segment_size( __INTVEC__ )

Portable segment names.

Definition at line 468 of file iar.h .

◆ _LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN

#define _LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN __segment_begin( __LOCKBITS_IN_MAINFLASH__ )

Portable segment names.

Definition at line 434 of file iar.h .

◆ _LOCKBITS_IN_MAINFLASH_SEGMENT_END

#define _LOCKBITS_IN_MAINFLASH_SEGMENT_END __segment_end( __LOCKBITS_IN_MAINFLASH__ )

Portable segment names.

Definition at line 463 of file iar.h .

◆ _LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE

#define _LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE __segment_size( __LOCKBITS_IN_MAINFLASH__ )

Portable segment names.

Definition at line 492 of file iar.h .

◆ _LONGTOKEN_SEGMENT_BEGIN

#define _LONGTOKEN_SEGMENT_BEGIN __segment_begin( __LONGTOKEN__ )

Portable segment names.

Definition at line 427 of file iar.h .

◆ _LONGTOKEN_SEGMENT_END

#define _LONGTOKEN_SEGMENT_END __segment_end( __LONGTOKEN__ )

Portable segment names.

Definition at line 456 of file iar.h .

◆ _LONGTOKEN_SEGMENT_SIZE

#define _LONGTOKEN_SEGMENT_SIZE __segment_size( __LONGTOKEN__ )

Portable segment names.

Definition at line 485 of file iar.h .

◆ _NO_INIT_SEGMENT_BEGIN

#define _NO_INIT_SEGMENT_BEGIN __segment_begin( __NO_INIT__ )

Portable segment names.

Definition at line 408 of file iar.h .

◆ _NO_INIT_SEGMENT_END

#define _NO_INIT_SEGMENT_END __segment_end( __NO_INIT__ )

Portable segment names.

Definition at line 437 of file iar.h .

◆ _NO_INIT_SEGMENT_SIZE

#define _NO_INIT_SEGMENT_SIZE __segment_size( __NO_INIT__ )

Portable segment names.

Definition at line 466 of file iar.h .

◆ _PSSTORE_SEGMENT_BEGIN

#define _PSSTORE_SEGMENT_BEGIN __segment_begin( __PSSTORE__ )

Portable segment names.

Definition at line 426 of file iar.h .

◆ _PSSTORE_SEGMENT_END

#define _PSSTORE_SEGMENT_END __segment_end( __PSSTORE__ )

Portable segment names.

Definition at line 455 of file iar.h .

◆ _PSSTORE_SEGMENT_SIZE

#define _PSSTORE_SEGMENT_SIZE __segment_size( __PSSTORE__ )

Portable segment names.

Definition at line 484 of file iar.h .

◆ _RAT_SEGMENT_BEGIN

#define _RAT_SEGMENT_BEGIN __segment_begin( __RAT__ )

Portable segment names.

Definition at line 424 of file iar.h .

◆ _RAT_SEGMENT_END

#define _RAT_SEGMENT_END __segment_end( __RAT__ )

Portable segment names.

Definition at line 453 of file iar.h .

◆ _RAT_SEGMENT_SIZE

#define _RAT_SEGMENT_SIZE __segment_size( __RAT__ )

Portable segment names.

Definition at line 482 of file iar.h .

◆ _RESETINFO_SEGMENT_BEGIN

#define _RESETINFO_SEGMENT_BEGIN __segment_begin( __RESETINFO__ )

Portable segment names.

Definition at line 412 of file iar.h .

◆ _RESETINFO_SEGMENT_END

#define _RESETINFO_SEGMENT_END __segment_end( __RESETINFO__ )

Portable segment names.

Definition at line 441 of file iar.h .

◆ _RESETINFO_SEGMENT_SIZE

#define _RESETINFO_SEGMENT_SIZE __segment_size( __RESETINFO__ )

Portable segment names.

Definition at line 470 of file iar.h .

◆ _SIMEE_SEGMENT_BEGIN

#define _SIMEE_SEGMENT_BEGIN __segment_begin( __SIMEE__ )

Portable segment names.

Definition at line 425 of file iar.h .

◆ _SIMEE_SEGMENT_END

#define _SIMEE_SEGMENT_END __segment_end( __SIMEE__ )

Portable segment names.

Definition at line 454 of file iar.h .

◆ _SIMEE_SEGMENT_SIZE

#define _SIMEE_SEGMENT_SIZE __segment_size( __SIMEE__ )

Portable segment names.

Definition at line 483 of file iar.h .

◆ _TEXT_SEGMENT_BEGIN

#define _TEXT_SEGMENT_BEGIN __segment_begin( __TEXT__ )

Portable segment names.

Definition at line 417 of file iar.h .

◆ _TEXT_SEGMENT_END

#define _TEXT_SEGMENT_END __segment_end( __TEXT__ )

Portable segment names.

Definition at line 446 of file iar.h .

◆ _TEXT_SEGMENT_SIZE

#define _TEXT_SEGMENT_SIZE __segment_size( __TEXT__ )

Portable segment names.

Definition at line 475 of file iar.h .

◆ _TEXTRW_INIT_SEGMENT_BEGIN

#define _TEXTRW_INIT_SEGMENT_BEGIN __segment_begin( __TEXTRW_INIT__ )

Portable segment names.

Definition at line 418 of file iar.h .

◆ _TEXTRW_INIT_SEGMENT_END

#define _TEXTRW_INIT_SEGMENT_END __segment_end( __TEXTRW_INIT__ )

Portable segment names.

Definition at line 447 of file iar.h .

◆ _TEXTRW_INIT_SEGMENT_SIZE

#define _TEXTRW_INIT_SEGMENT_SIZE __segment_size( __TEXTRW_INIT__ )

Portable segment names.

Definition at line 476 of file iar.h .

◆ _TEXTRW_SEGMENT_BEGIN

#define _TEXTRW_SEGMENT_BEGIN __segment_begin( __TEXTRW__ )

Portable segment names.

Definition at line 419 of file iar.h .

◆ _TEXTRW_SEGMENT_END

#define _TEXTRW_SEGMENT_END __segment_end( __TEXTRW__ )

Portable segment names.

Definition at line 448 of file iar.h .

◆ _TEXTRW_SEGMENT_SIZE

#define _TEXTRW_SEGMENT_SIZE __segment_size( __TEXTRW__ )

Portable segment names.

Definition at line 477 of file iar.h .

◆ _UNRETAINED_RAM_SEGMENT_BEGIN

#define _UNRETAINED_RAM_SEGMENT_BEGIN __segment_begin( __UNRETAINED_RAM__ )

Portable segment names.

Definition at line 435 of file iar.h .

◆ _UNRETAINED_RAM_SEGMENT_END

#define _UNRETAINED_RAM_SEGMENT_END __segment_end( __UNRETAINED_RAM__ )

Portable segment names.

Definition at line 464 of file iar.h .

◆ _UNRETAINED_RAM_SEGMENT_SIZE

#define _UNRETAINED_RAM_SEGMENT_SIZE __segment_size( __UNRETAINED_RAM__ )

Portable segment names.

Definition at line 493 of file iar.h .

◆ ALIGNMENT

#define ALIGNMENT ( X ) _Pragma( STRINGIZE (data_alignment = X))

Provide a portable way to align data.

Definition at line 300 of file iar.h .

◆ assert

#define assert ( condition )

A custom implementation of the C language assert macro. This macro implements the conditional evaluation and calls the function halInternalAssertFailed() . (see hal/micro/micro.h )

Definition at line 160 of file iar.h .

◆ BIGENDIAN_CPU

#define BIGENDIAN_CPU false

A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.

Definition at line 115 of file iar.h .

◆ EEPROM

#define EEPROM errorerror

A friendlier name for the compiler's intrinsic for eeprom reference.

Definition at line 134 of file iar.h .

◆ HAL_HAS_INT64

#define HAL_HAS_INT64

Denotes that this platform supports 64-bit data-types.

Definition at line 97 of file iar.h .

◆ halResetWatchdog

#define halResetWatchdog ( ) halInternalResetWatchDog ()

A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.

Definition at line 191 of file iar.h .

◆ MAIN_FUNCTION_ARGUMENTS

#define MAIN_FUNCTION_ARGUMENTS

Definition at line 544 of file iar.h .

◆ MAIN_FUNCTION_PARAMETERS

#define MAIN_FUNCTION_PARAMETERS void

The kind of arguments the main function takes.

Definition at line 543 of file iar.h .

◆ NO_INIT

#define NO_INIT ( __symbol ) __no_init __symbol

Provide a portable way to specify a non initialized symbol.

Definition at line 312 of file iar.h .

◆ NO_OPERATION

#define NO_OPERATION ( ) __NOP()

Define a generic no operation identifier to a compiler specific one.

Definition at line 224 of file iar.h .

◆ NO_STRIPPING

#define NO_STRIPPING __root

A friendlier name for the compiler's intrinsic for not stripping.

Definition at line 128 of file iar.h .

◆ NTOHL

#define NTOHL ( val ) (__REV(val))

A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.

Definition at line 122 of file iar.h .

◆ NTOHS

#define NTOHS ( val ) (__REV16(val))

Define intrinsics for NTOHL and NTOHS to save code space by making endian.c compile to nothing.

Definition at line 121 of file iar.h .

◆ PLATCOMMONOKTOINCLUDE

#define PLATCOMMONOKTOINCLUDE

Include platform-common.h last to pick up defaults and common definitions.

Definition at line 536 of file iar.h .

◆ RAMFUNC

#define RAMFUNC __ramfunc

Define a generic RAM function identifier to a compiler specific one.

Definition at line 218 of file iar.h .

◆ SET_CMSIS_REG

#define SET_CMSIS_REG ( reg,
mask,
value
)
Value:
do { \
reg = (((reg) & (~mask)) | (value)); \
} while (0)

A convenience macro that makes it easy to change a register using the provided mask(s) and value(s). Example: SET_CMSIS_REG(GPIO->P[1].CFGH, (_GPIO_P_CFGH_Px5_MASK | _GPIO_P_CFGH_Px6_MASK), (GPIO_P_CFGH_Px5_OUT | GPIO_P_CFGH_Px6_OUT));.

Definition at line 247 of file iar.h .

◆ SET_CMSIS_REG_FIELD

#define SET_CMSIS_REG_FIELD ( reg,
field,
value
)
Value:
do { \
reg = ((reg & (~_##field##_MASK)) \
| ((value << _##field##_SHIFT) \
& (_##field##_MASK))); \
} while (0)

A convenience macro that makes it easy to change the field of a register, as defined in CMSIS Device headers, to any unsigned value. Example using EM35xx: SET_CMSIS_REG_FIELD(GPIO->P[0].CFGL, GPIO_P_CFGL_Px0, _GPIO_P_CFGL_Px0_OUT);.

Definition at line 258 of file iar.h .

◆ SET_REG_FIELD

#define SET_REG_FIELD ( reg,
field,
value
)
Value:
do { \
reg = ((reg & (~field##_MASK)) \
| ((((uint32_t) value) << field##_BIT) \
& (field##_MASK))); \
} while (0)

A convenience macro that makes it easy to change the field of a register to any unsigned value.

Definition at line 230 of file iar.h .

◆ SIGNED_ENUM

#define SIGNED_ENUM

Some platforms need to cast enum values that have the high bit set.

Definition at line 203 of file iar.h .

◆ simulatedSerialTimePasses

#define simulatedSerialTimePasses ( )

Stub for code not running in simulation.

Definition at line 278 of file iar.h .

◆ simulatedTimePasses

#define simulatedTimePasses ( )

Stub for code not running in simulation.

Definition at line 268 of file iar.h .

◆ simulatedTimePassesMs

#define simulatedTimePassesMs ( x )

Stub for code not running in simulation.

Definition at line 273 of file iar.h .

◆ STACK_FILL_VALUE

#define STACK_FILL_VALUE 0xCDCDCDCDU

Define the magic value that is interpreted by IAR C-SPY's Stack View.

Definition at line 208 of file iar.h .

◆ STATIC_ASSERT

#define STATIC_ASSERT ( __condition,
__errorstr
) static_assert(__condition, __errorstr)

Provide a portable way to specify a compile time assert.

Definition at line 318 of file iar.h .

◆ STRINGIZE

#define STRINGIZE ( X ) #X

Convinience macro for turning a token into a string.

Definition at line 295 of file iar.h .

◆ UNUSED

#define UNUSED

Declare a variable as unused to avoid a warning. Has no effect in IAR builds.

Definition at line 198 of file iar.h .

◆ VAR_AT_SEGMENT

#define VAR_AT_SEGMENT ( __variableDeclaration,
__segmentName
) __variableDeclaration @ __segmentName

Provide a portable way to specify the segment where a variable lives.

Definition at line 289 of file iar.h .

◆ WEAK

#define WEAK ( __symbol ) __weak __symbol

Provide a portable way to specify a symbol as weak.

Definition at line 306 of file iar.h .

Typedef Documentation

◆ boolean

typedef bool boolean

A typedef to make the size of the variable explicitly known.

Definition at line 82 of file iar.h .

◆ int16s

typedef signed short int16s

A typedef to make the size of the variable explicitly known.

Definition at line 86 of file iar.h .

◆ int16u

typedef unsigned short int16u

A typedef to make the size of the variable explicitly known.

Definition at line 85 of file iar.h .

◆ int32s

typedef signed int int32s

A typedef to make the size of the variable explicitly known.

Definition at line 88 of file iar.h .

◆ int32u

typedef unsigned int int32u

A typedef to make the size of the variable explicitly known.

Definition at line 87 of file iar.h .

◆ int64s

typedef signed long long int64s

A typedef to make the size of the variable explicitly known.

Definition at line 90 of file iar.h .

◆ int64u

typedef unsigned long long int64u

A typedef to make the size of the variable explicitly known.

Definition at line 89 of file iar.h .

◆ int8s

typedef signed char int8s

A typedef to make the size of the variable explicitly known.

Definition at line 84 of file iar.h .

◆ int8u

typedef unsigned char int8u

A typedef to make the size of the variable explicitly known.

Definition at line 83 of file iar.h .

◆ PointerType

typedef unsigned int PointerType

A typedef to make the size of the variable explicitly known.

Definition at line 91 of file iar.h .

Function Documentation

◆ _executeBarrierInstructions()

void _executeBarrierInstructions ( void )

◆ abs()

int abs ( int I )

Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I.

Parameters
I An integer.
Returns
A nonnegative integer.

◆ halInternalAssertFailed()

void halInternalAssertFailed ( const char * filename,
int linenumber
)

A prototype definition for use by the assert macro. (see hal/micro/micro.h )

◆ halInternalResetWatchDog()

void halInternalResetWatchDog ( void )

Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful.