EmberNetworkParameters Struct Reference

Hold network parameters. More...

#include < ember-types.h >

Data Fields

uint16_t panId
int16_t radioTxPower
uint16_t radioChannel

Hold network parameters.

For information about power settings and radio channels, see the technical specification for the RF communication module in your Developer Kit and the Radio Configurator Guide (AN971).

Definition at line 181 of file ember-types.h .

Field Documentation

◆ panId

uint16_t EmberNetworkParameters::panId

The network's PAN identifier.

Definition at line 183 of file ember-types.h .

◆ radioChannel

uint16_t EmberNetworkParameters::radioChannel

The radio channel. Be sure to specify a channel supported by the radio.

Definition at line 187 of file ember-types.h .

◆ radioTxPower

int16_t EmberNetworkParameters::radioTxPower

The transmit power setting, in deci-dBm.

Definition at line 185 of file ember-types.h .


The documentation for this struct was generated from the following file:
  • ember-types.h