Return-code definitions for Connect stack API functions. More...

Enumerations

enum EmberStatus {
EMBER_SUCCESS = 0x00,
EMBER_ERR_FATAL = 0x01,
EMBER_BAD_ARGUMENT = 0x02,
EMBER_EEPROM_MFG_STACK_VERSION_MISMATCH = 0x04,
EMBER_INVALID_CALL = 0x70,
EMBER_EEPROM_MFG_VERSION_MISMATCH = 0x06,
EMBER_EEPROM_STACK_VERSION_MISMATCH = 0x07,
EMBER_NO_BUFFERS = 0x18,
EMBER_SERIAL_INVALID_BAUD_RATE = 0x20,
EMBER_SERIAL_INVALID_PORT = 0x21,
EMBER_SERIAL_TX_OVERFLOW = 0x22,
EMBER_SERIAL_RX_OVERFLOW = 0x23,
EMBER_SERIAL_RX_FRAME_ERROR = 0x24,
EMBER_SERIAL_RX_PARITY_ERROR = 0x25,
EMBER_SERIAL_RX_EMPTY = 0x26,
EMBER_SERIAL_RX_OVERRUN_ERROR = 0x27,
EMBER_MAC_NO_DATA = 0x31,
EMBER_MAC_SYNC_TIMEOUT = 0x33,
EMBER_MAC_SYNC_WRONG_SEED = 0x34,
EMBER_MAC_SECURITY_FAILED = 0x35,
EMBER_MAC_UNKNOWN_DESTINATION = 0x37,
EMBER_MAC_SECURITY_NOT_SUPPORTED = 0x38,
EMBER_MAC_TRANSMIT_QUEUE_FULL = 0x39,
EMBER_MAC_ACK_HEADER_TYPE = 0x3B,
EMBER_MAC_SCANNING = 0x3D,
EMBER_MAC_BUSY = 0x3E,
EMBER_MAC_NO_ACK_RECEIVED = 0x40,
EMBER_MAC_INDIRECT_TIMEOUT = 0x41,
EMBER_MAC_INDIRECT_MESSAGE_PURGED = 0x42,
EMBER_SIM_EEPROM_ERASE_PAGE_GREEN = 0x43,
EMBER_SIM_EEPROM_ERASE_PAGE_RED = 0x44,
EMBER_SIM_EEPROM_FULL = 0x45,
EMBER_SIM_EEPROM_INIT_2_FAILED = 0x49,
EMBER_SIM_EEPROM_INIT_3_FAILED = 0x4A,
EMBER_SIM_EEPROM_REPAIRING = 0x4D,
EMBER_ERR_FLASH_WRITE_INHIBITED = 0x46,
EMBER_ERR_FLASH_VERIFY_FAILED = 0x47,
EMBER_ERR_FLASH_PROG_FAIL = 0x4B,
EMBER_MESSAGE_TOO_LONG = 0x74,
EMBER_ADC_CONVERSION_DONE = 0x80,
EMBER_ADC_CONVERSION_BUSY = 0x81,
EMBER_ADC_CONVERSION_DEFERRED = 0x82,
EMBER_ADC_NO_CONVERSION_PENDING = 0x84,
EMBER_SLEEP_INTERRUPTED = 0x85,
EMBER_PHY_TX_INCOMPLETE = 0x89,
EMBER_PHY_INVALID_CHANNEL = 0x8A,
EMBER_PHY_INVALID_POWER = 0x8B,
EMBER_PHY_TX_BUSY = 0x8C,
EMBER_PHY_TX_CCA_FAIL = 0x8D,
EMBER_PHY_CALIBRATING = 0x8E,
EMBER_PHY_ACK_RECEIVED = 0x8F,
EMBER_NETWORK_UP = 0x90,
EMBER_NETWORK_DOWN = 0x91,
EMBER_JOIN_SCAN_FAILED = 0x92,
EMBER_JOIN_FAILED = 0x94,
EMBER_JOIN_DENIED = 0x95,
EMBER_JOIN_TIMEOUT = 0x96,
EMBER_NO_VALID_BEACONS = 0xAB,
EMBER_SECURITY_DATA_INVALID = 0xBD,
EMBER_NOT_JOINED = 0x93,
EMBER_TABLE_FULL = 0xB4,
EMBER_LIBRARY_NOT_PRESENT = 0xB5,
EMBER_CHILD_NOT_FOUND = 0xB6,
EMBER_NVM3_ERR_OPENED_WITH_OTHER_PARAMETERS = 0xC1,
EMBER_NVM3_ERR_ALIGNMENT_INVALID = 0xC2,
EMBER_NVM3_ERR_SIZE_TOO_SMALL = 0xC3,
EMBER_NVM3_ERR_PAGE_SIZE_NOT_SUPPORTED = 0xC4,
EMBER_NVM3_ERR_TOKEN_INIT = 0xC5,
EMBER_NVM3_ERR_UPGRADE = 0xC6,
EMBER_NVM3_ERR_UNKNOWN = 0xC7,
EMBER_APPLICATION_ERROR_0 = 0xF0,
EMBER_APPLICATION_ERROR_1 = 0xF1,
EMBER_APPLICATION_ERROR_2 = 0xF2,
EMBER_APPLICATION_ERROR_3 = 0xF3,
EMBER_APPLICATION_ERROR_4 = 0xF4,
EMBER_APPLICATION_ERROR_5 = 0xF5,
EMBER_APPLICATION_ERROR_6 = 0xF6,
EMBER_APPLICATION_ERROR_7 = 0xF7,
EMBER_APPLICATION_ERROR_8 = 0xF8,
EMBER_APPLICATION_ERROR_9 = 0xF9,
EMBER_APPLICATION_ERROR_10 = 0xFA,
EMBER_APPLICATION_ERROR_11 = 0xFB,
EMBER_APPLICATION_ERROR_12 = 0xFC,
EMBER_APPLICATION_ERROR_13 = 0xFD,
EMBER_APPLICATION_ERROR_14 = 0xFE,
EMBER_APPLICATION_ERROR_15 = 0xFF
}

Detailed Description

Return-code definitions for Connect stack API functions.

Many Connect API functions return an EmberStatus value to indicate the success or failure of the call.

Return codes are one byte long.

This page documents the possible status codes and their meanings.

See error-def.h for source code.

See also error.h for information on how the values for the return codes are built up from these definitions. The file error-def.h is separated from error.h because utilities will use this file to parse the return codes.

Note
Do not include error-def.h directly. It is included by error.h inside an enum typedef, which is in turn included by ember.h.

Enumeration Type Documentation

◆ EmberStatus

Enumerator
EMBER_SUCCESS

The generic "no error" message.

EMBER_ERR_FATAL

The generic "fatal error" message.

EMBER_BAD_ARGUMENT

An invalid value was passed as an argument to a function.

EMBER_EEPROM_MFG_STACK_VERSION_MISMATCH

The manufacturing and stack token format in non-volatile memory is different than what the stack expects (returned at initialization).

EMBER_INVALID_CALL

The API call is not allowed given the current state of the stack.

EMBER_EEPROM_MFG_VERSION_MISMATCH

The manufacturing token format in non-volatile memory is different than what the stack expects (returned at initialization).

EMBER_EEPROM_STACK_VERSION_MISMATCH

The stack token format in non-volatile memory is different than what the stack expects (returned at initialization).

EMBER_NO_BUFFERS

There are no more buffers (either in the stack heap or the queue used by the associated module, such as indirect queue).

EMBER_SERIAL_INVALID_BAUD_RATE

Specified an invalid baud rate.

EMBER_SERIAL_INVALID_PORT

Specified an invalid serial port.

EMBER_SERIAL_TX_OVERFLOW

Tried to send too much data.

EMBER_SERIAL_RX_OVERFLOW

There was not enough space to store a received character and some characters were dropped.

EMBER_SERIAL_RX_FRAME_ERROR

Detected a UART framing error.

EMBER_SERIAL_RX_PARITY_ERROR

Detected a UART parity error.

EMBER_SERIAL_RX_EMPTY

There is no received data to process.

EMBER_SERIAL_RX_OVERRUN_ERROR

The receive interrupt was not handled in time and some characters were dropped.

EMBER_MAC_NO_DATA

No pending data exists for device doing a data poll.

EMBER_MAC_SYNC_TIMEOUT

The frequency hopping client failed the frequency hopping synchronization procedure. It timed out trying to reach the frequency hopping server.

EMBER_MAC_SYNC_WRONG_SEED

The frequency hopping client failed the frequency hopping synchronization procedure. The server is currently using a different seed.

EMBER_MAC_SECURITY_FAILED

MAC security operation failed.

EMBER_MAC_UNKNOWN_DESTINATION

Transmission failed: the destination node does not appear in the neighbor or child tables.

EMBER_MAC_SECURITY_NOT_SUPPORTED

Transmission failed: the local node does not support security or a secured transmission has been requested to a child that does not support security.

EMBER_MAC_TRANSMIT_QUEUE_FULL

The MAC transmit queue is full.

EMBER_MAC_ACK_HEADER_TYPE

MAC ACK header received.

EMBER_MAC_SCANNING

The MAC can't complete this task because it is scanning.

EMBER_MAC_BUSY

The requested operation cannot be completed because MAC is currently busy performing a high-priority task.

EMBER_MAC_NO_ACK_RECEIVED

Expected to receive an ACK following the transmission, but the MAC level ACK was never received.

EMBER_MAC_INDIRECT_TIMEOUT

Indirect data message timed out before polled.

EMBER_MAC_INDIRECT_MESSAGE_PURGED

Transmission failed: the indirect message was purged because the destination child has been removed or updated, or because emberPurgeIndirectMessages() was called.

EMBER_SIM_EEPROM_ERASE_PAGE_GREEN

The Simulated EEPROM is telling the application that there is at least one flash page to be erased. The GREEN status means the current page has not filled above the ::ERASE_CRITICAL_THRESHOLD.

The application should call the function halSimEepromErasePage() when it can to erase a page.

Warning
This status is generated in halSimEepromCallback() , and handled correctly in the default implementation.
EMBER_SIM_EEPROM_ERASE_PAGE_RED

The Simulated EEPROM is telling the application that there is at least one flash page to be erased. The RED status means the current page has filled above the ::ERASE_CRITICAL_THRESHOLD.

Because of the shrinking availability of write space, there is a danger of data loss. The application must call the function halSimEepromErasePage() as soon as possible to erase a page.

Warning
This status is generated in halSimEepromCallback() , and handled correctly in the default implementation.
EMBER_SIM_EEPROM_FULL

The Simulated EEPROM has run out of room to write any new data and the data trying to be set has been lost. This error code is the result of ignoring the EMBER_SIM_EEPROM_ERASE_PAGE_RED error code.

The application must call the function halSimEepromErasePage() to make room for any further calls to set a token.

Warning
This status is generated in halSimEepromCallback() , and handled correctly in the default implementation.
EMBER_SIM_EEPROM_INIT_2_FAILED

Attempt 2 to initialize the Simulated EEPROM has failed.

This failure means Attempt 1 failed, and the token system failed to properly reload default tokens and reset the Simulated EEPROM.

EMBER_SIM_EEPROM_INIT_3_FAILED

Attempt 3 to initialize the Simulated EEPROM has failed.

This failure means one or both of the tokens ::TOKEN_MFG_NVDATA_VERSION or ::TOKEN_STACK_NVDATA_VERSION were incorrect and the token system failed to properly reload default tokens and reset the Simulated EEPROM.

EMBER_SIM_EEPROM_REPAIRING

The Simulated EEPROM is repairing itself.

While there's nothing for an app to do when the SimEE is going to repair itself (SimEE has to be fully functional for the rest of the system to work), alert the application to the fact that repairing is occurring. There are debugging scenarios where an app might want to know that repairing is happening; such as monitoring frequency.

Note
Common situations will trigger an expected repair, such as using an erased chip or changing token definitions.
Warning
This status is generated in halSimEepromCallback() , and handled correctly in the default implementation.
EMBER_ERR_FLASH_WRITE_INHIBITED

A fatal error has occurred while trying to write data to the flash. The target memory attempting to be programmed is already programmed. The flash write routines were asked to flip a bit from a 0 to 1, which is physically impossible and the write was therefore inhibited. The data in the flash cannot be trusted after this error.

Warning
This status is generated in halSimEepromCallback() , and handled correctly in the default implementation.
EMBER_ERR_FLASH_VERIFY_FAILED

A fatal error has occurred while trying to write data to the flash and the write verification has failed. The data in the flash cannot be trusted after this error, and it is possible this error is the result of exceeding the life cycles of the flash.

Warning
This status is generated in halSimEepromCallback() , and handled correctly in the default implementation.
EMBER_ERR_FLASH_PROG_FAIL

A fatal error has occurred while trying to write data to the flash, possibly due to write protection or an invalid address. The data in the flash cannot be trusted after this error, and it is possible this error is the result of exceeding the life cycles of the flash.

EMBER_MESSAGE_TOO_LONG

The message to be transmitted is too big to fit into a single over-the-air packet.

EMBER_ADC_CONVERSION_DONE

Conversion is complete.

EMBER_ADC_CONVERSION_BUSY

Conversion cannot be done because a request is being processed.

EMBER_ADC_CONVERSION_DEFERRED

Conversion is deferred until the current request has been processed.

EMBER_ADC_NO_CONVERSION_PENDING

No results are pending.

EMBER_SLEEP_INTERRUPTED

Sleeping (for a duration) has been abnormally interrupted and exited prematurely.

EMBER_PHY_TX_INCOMPLETE

The transmit hardware did not finish transmitting a packet.

EMBER_PHY_INVALID_CHANNEL

An unsupported channel setting was specified.

EMBER_PHY_INVALID_POWER

An unsupported power setting was specified.

EMBER_PHY_TX_BUSY

The requested operation cannot be completed because the radio is currently busy, either transmitting a packet or performing calibration.

EMBER_PHY_TX_CCA_FAIL

The transmit attempt failed because all CCA attempts indicated that the channel was busy.

EMBER_PHY_CALIBRATING

The requested operation cannot be completed because the stack has triggered a radio calibration. Wait for about one second for it to complete.

EMBER_PHY_ACK_RECEIVED

The expected ACK was received after the last transmission.

EMBER_NETWORK_UP

The stack software has completed initialization required to be in a network and is ready to send and receive packets over the air.

See also
emberStackStatusHandler()
EMBER_NETWORK_DOWN

The network is not operating.

See also
emberStackStatusHandler()
EMBER_JOIN_SCAN_FAILED

The node failed to initiate the scanning process during the joining process.

See also
emberStackStatusHandler()
EMBER_JOIN_FAILED

An attempt to join a network failed.

See also
emberStackStatusHandler()
EMBER_JOIN_DENIED

An attempt to join a network was rejected.

See also
emberStackStatusHandler()
EMBER_JOIN_TIMEOUT

The node timed out waiting for a response during the joining process.

See also
emberStackStatusHandler()
EMBER_NO_VALID_BEACONS

An attempt to join or rejoin the network failed because no valid beacons was received by the joining node.

See also
emberStackStatusHandler()
EMBER_SECURITY_DATA_INVALID

The security data provided was not valid, or an integrity check failed.

EMBER_NOT_JOINED

The node has not joined a network. Returned by emberNetworkInit() if there was no connection data saved in tokens.

EMBER_TABLE_FULL

There are no empty entries left in the table.

EMBER_LIBRARY_NOT_PRESENT

The requested function cannot be executed because the library (plugin) that contains the necessary functionality is not present.

EMBER_CHILD_NOT_FOUND

The requested NodeId has not been found in the child list or grandchildren list (start network only).

EMBER_NVM3_ERR_OPENED_WITH_OTHER_PARAMETERS

NVM3 is telling the application that the initialization was aborted as the NVM3 instance was already opened with other parameters.

EMBER_NVM3_ERR_ALIGNMENT_INVALID

NVM3 is telling the application that the initialization was aborted as the NVM3 instance is not aligned properly in memory.

EMBER_NVM3_ERR_SIZE_TOO_SMALL

NVM3 is telling the application that the initialization was aborted as the size of the NVM3 instance is too small.

EMBER_NVM3_ERR_PAGE_SIZE_NOT_SUPPORTED

NVM3 is telling the application that the initialization was aborted as the NVM3 page size is not supported.

EMBER_NVM3_ERR_TOKEN_INIT

NVM3 is telling the application that there was an error initializing some of the tokens.

EMBER_NVM3_ERR_UPGRADE

NVM3 is telling the application there has been an error when attempting to upgrade SimEE tokens.

EMBER_NVM3_ERR_UNKNOWN

NVM3 is telling the application that there has been an unknown error.

EMBER_APPLICATION_ERROR_0

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_1

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_2

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_3

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_4

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_5

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_6

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_7

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_8

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_9

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_10

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_11

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_12

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_13

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_14

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_15

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

Definition at line 58 of file error-def.h .