For use when declaring a separate command streams. The fields are not accessed directly by the application. More...

#include < command-interpreter2.h >

Data Fields

uint8_t state
uint8_t buffer [ EMBER_COMMAND_BUFFER_LENGTH ]
uint8_t tokenIndices [ MAX_TOKEN_COUNT +1]
uint8_t tokenCount
uint16_t index
uint8_t error
uint8_t hexHighNibble
uint8_t argOffset
uint8_t previousCharacter
uint8_t defaultBase
EmberCommandEntry * currentCommand

For use when declaring a separate command streams. The fields are not accessed directly by the application.

Definition at line 415 of file command-interpreter2.h .

Field Documentation

argOffset

uint8_t EmberCommandState::argOffset

Definition at line 441 of file command-interpreter2.h .

buffer

uint8_t EmberCommandState::buffer[ EMBER_COMMAND_BUFFER_LENGTH ]

Definition at line 422 of file command-interpreter2.h .

currentCommand

EmberCommandEntry * EmberCommandState::currentCommand

Definition at line 451 of file command-interpreter2.h .

defaultBase

uint8_t EmberCommandState::defaultBase

Definition at line 448 of file command-interpreter2.h .

error

uint8_t EmberCommandState::error

Definition at line 435 of file command-interpreter2.h .

hexHighNibble

uint8_t EmberCommandState::hexHighNibble

Definition at line 438 of file command-interpreter2.h .

index

uint16_t EmberCommandState::index

Definition at line 432 of file command-interpreter2.h .

previousCharacter

uint8_t EmberCommandState::previousCharacter

Definition at line 445 of file command-interpreter2.h .

state

uint8_t EmberCommandState::state

Definition at line 417 of file command-interpreter2.h .

tokenCount

uint8_t EmberCommandState::tokenCount

Definition at line 429 of file command-interpreter2.h .

tokenIndices

uint8_t EmberCommandState::tokenIndices[ MAX_TOKEN_COUNT +1]

Definition at line 426 of file command-interpreter2.h .


The documentation for this struct was generated from the following file:
  • command-interpreter2.h