EmberMacAddress Struct Reference

A structure that stores an 802.15.4 address. More...

#include < ember-types.h >

Data Fields

union {
uint8_t longAddress [ EUI64_SIZE ]
Long (EUI-64) address. Valid if mode is EMBER_MAC_ADDRESS_MODE_LONG . More...
uint16_t shortAddress
Short address (node ID). Valid if mode is EMBER_MAC_ADDRESS_MODE_SHORT . More...
} addr
EmberMacAddressMode mode

A structure that stores an 802.15.4 address.

Definition at line 351 of file ember-types.h .

Field Documentation

◆ addr

union { ... } EmberMacAddress::addr

◆ longAddress

uint8_t EmberMacAddress::longAddress[ EUI64_SIZE ]

Long (EUI-64) address. Valid if mode is EMBER_MAC_ADDRESS_MODE_LONG .

Definition at line 357 of file ember-types.h .

◆ mode

EmberMacAddressMode EmberMacAddress::mode

Addressing mode

Definition at line 365 of file ember-types.h .

◆ shortAddress

uint16_t EmberMacAddress::shortAddress

Short address (node ID). Valid if mode is EMBER_MAC_ADDRESS_MODE_SHORT .

Definition at line 362 of file ember-types.h .


The documentation for this struct was generated from the following file:
  • ember-types.h