EmberEventData_S Struct Reference

Complete events with a control and a handler procedure. More...

#include < ember-types.h >

Data Fields

EmberEventControl * control
void(* handler )(void)

Complete events with a control and a handler procedure.

An application typically creates an array of events along with their handlers. The main loop passes the array to emberRunEvents() to call the handlers of any events whose time has arrived.

Definition at line 597 of file ember-types.h .

Field Documentation

◆ control

EmberEventControl * EmberEventData_S::control

The control structure for the event.

Definition at line 599 of file ember-types.h .

◆ handler

void(* EmberEventData_S::handler) (void)

The procedure to call when the event fires.

Definition at line 601 of file ember-types.h .


The documentation for this struct was generated from the following file:
  • ember-types.h