#include < micro-common.h >

Data Fields

uint32_t outgoingNwkFrameCounter
uint32_t incomingParentNwkFrameCounter
uint32_t outgoingLinkKeyFrameCounter
uint32_t incomingLinkKeyFrameCounter

Definition at line 222 of file micro-common.h .

Field Documentation

◆ incomingLinkKeyFrameCounter

uint32_t RTCCRamData::incomingLinkKeyFrameCounter

Definition at line 226 of file micro-common.h .

◆ incomingParentNwkFrameCounter

uint32_t RTCCRamData::incomingParentNwkFrameCounter

Definition at line 224 of file micro-common.h .

◆ outgoingLinkKeyFrameCounter

uint32_t RTCCRamData::outgoingLinkKeyFrameCounter

Definition at line 225 of file micro-common.h .

◆ outgoingNwkFrameCounter

uint32_t RTCCRamData::outgoingNwkFrameCounter

Definition at line 223 of file micro-common.h .


The documentation for this struct was generated from the following file:
  • micro-common.h