This API contains the HAL interfaces that applications must implement for the high-level serial code. More...

Enumerations

enum SerialBaudRate {
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0,
DEFINE_BAUD =(300) = 0
}
Assign numerical values for variables that hold Baud Rate parameters. More...
enum SerialParity {
DEFINE_PARITY =(NONE) = 0U,
DEFINE_PARITY =(NONE) = 0U,
DEFINE_PARITY =(NONE) = 0U
}
CORTEXM3_EFM32_MICRO. More...

Functions

void halHostFlushBuffers (void)
uint16_t halHostEnqueueTx (const uint8_t *data, uint16_t length)
void halHostFlushTx (void)
uint16_t serialCopyFromRx (const uint8_t *data, uint16_t length)
void emLoadSerialTx (void)

Serial Mode Definitions

These are numerical definitions for the possible serial modes so that code can test for the one being used. There may be additional modes defined in the micro-specific micro.h.

#define EMBER_SERIAL_UNUSED 0
A numerical definition for a possible serial mode the code can test for. More...
#define EMBER_SERIAL_FIFO 1
A numerical definition for a possible serial mode the code can test for. More...
#define EMBER_SERIAL_LOWLEVEL 2
A numerical definition for a possible serial mode the code can test for. More...

FIFO Utility Macros

These macros manipulate the FIFO queue data structures to add and remove data.

#define FIFO_ENQUEUE (queue, data, size)
Macro that enqueues a byte of data in a FIFO queue. More...
#define FIFO_DEQUEUE (queue, size)
Macro that de-queues a byte of data from a FIFO queue. More...

Serial HAL APIs

These functions must be implemented by the HAL in order for the serial code to operate. Only the higher-level serial code uses these functions, so they should not be called directly. The HAL should also implement the appropriate interrupt handlers to drain the TX queues and fill the RX FIFO queue.

EmberStatus halInternalUartInit (uint8_t port, SerialBaudRate rate, SerialParity parity, uint8_t stopBits)
Initializes the UART to the given settings (same parameters as ::emberSerialInit() ). More...
void halInternalPowerDownUart (void)
This function is typically called by halPowerDown() and it is responsible for performing all the work internal to the UART needed to stop the UART before a sleep cycle. More...
void halInternalPowerUpUart (void)
This function is typically called by halPowerUp() and it is responsible for performing all the work internal to the UART needed to restart the UART after a sleep cycle. More...
void halInternalStartUartTx (uint8_t port)
Called by serial code whenever anything is queued for transmission to start any interrupt-driven transmission. May be called when transmission is already in progess. More...
void halInternalStopUartTx (uint8_t port)
Called by serial code to stop any interrupt-driven serial transmission currently in progress. More...
EmberStatus halInternalForceWriteUartData (uint8_t port, uint8_t *data, uint8_t length)
Directly writes a byte to the UART for transmission, regardless of anything currently queued for transmission. Should wait for anything currently in the UART hardware registers to finish transmission first, and block until data is finished being sent. More...
EmberStatus halInternalForceReadUartByte (uint8_t port, uint8_t *dataByte)
Directly reads a byte from the UART for reception, regardless of anything currently queued for reception. Does not block if a data byte has not been received. More...
void halInternalWaitUartTxComplete (uint8_t port)
Blocks until the UART has finished transmitting any data in its hardware registers. More...
void halInternalRestartUart (void)
This function is typically called by ::halInternalPowerUpBoard() and it is responsible for performing all the work internal to the UART needed to restart the UART after a sleep cycle. (For example, resyncing the DMA hardware and the serial FIFO.) More...
bool halInternalUartFlowControlRxIsEnabled (uint8_t port)
Checks to see if the host is allowed to send serial data to the ncp - i.e., it is not being held off by nCTS or an XOFF. Returns true is the host is able to send. More...
bool halInternalUartXonRefreshDone (uint8_t port)
When Xon/Xoff flow control is used, returns true if the host is not being held off and XON refreshing is complete. More...
bool halInternalUartTxIsIdle (uint8_t port)
Returns true if the uart transmitter is idle, including the transmit shift register. More...
bool serialDropPacket (void)
Testing function implemented by the upper layer. Determines whether the next packet should be dropped. Returns true if the next packet should be dropped, false otherwise. More...
#define halInternalUartFlowControl (port) do {} while (false)
This function is used in FIFO mode when flow control is enabled. It is called from emberSerialReadByte(), and based on the number of bytes used in the uart receive queue, decides when to tell the host it may resume transmission. More...
#define halInternalUartRxPump (port) do {} while (false)
This function exists only in software UART (SOFTUART) mode on the EM3xx. This function is called by ::emberSerialReadByte(). It is responsible for maintaining synchronization between the emSerialRxQueue and the UART DMA. More...
#define halInternalUart1FlowControlRxIsEnabled () halInternalUartFlowControlRxIsEnabled (1)
This function is used in FIFO mode when flow control is enabled. It is called from emberSerialReadByte(), and based on the number of bytes used in the uart receive queue, decides when to tell the host it may resume transmission. More...
#define halInternalUart1XonRefreshDone () halInternalUartXonRefreshDone (1)
This function is used in FIFO mode when flow control is enabled. It is called from emberSerialReadByte(), and based on the number of bytes used in the uart receive queue, decides when to tell the host it may resume transmission. More...
#define halInternalUart1TxIsIdle () halInternalUartTxIsIdle (1)
This function is used in FIFO mode when flow control is enabled. It is called from emberSerialReadByte(), and based on the number of bytes used in the uart receive queue, decides when to tell the host it may resume transmission. More...

Virtual UART API

API used by the stack in debug builds to receive data arriving over the virtual UART.

void halStackReceiveVuartMessage (uint8_t *data, uint8_t length)
When using a debug build with virtual UART support, this API is called by the stack when virtual UART data has been received over the debug channel. More...

Detailed Description

This API contains the HAL interfaces that applications must implement for the high-level serial code.

This header describes the interface between the high-level serial APIs in serial/serial.h and the low level UART implementation.

Some functions in this file return an EmberStatus value. See error-def.h for definitions of all EmberStatus return values.

See hal/micro/serial.h for source code.

Macro Definition Documentation

◆ EMBER_SERIAL_FIFO

#define EMBER_SERIAL_FIFO 1

A numerical definition for a possible serial mode the code can test for.

Definition at line 96 of file serial.h .

◆ EMBER_SERIAL_LOWLEVEL

#define EMBER_SERIAL_LOWLEVEL 2

A numerical definition for a possible serial mode the code can test for.

Definition at line 97 of file serial.h .

◆ EMBER_SERIAL_UNUSED

#define EMBER_SERIAL_UNUSED 0

A numerical definition for a possible serial mode the code can test for.

Definition at line 95 of file serial.h .

◆ FIFO_DEQUEUE

#define FIFO_DEQUEUE ( queue,
size
)
Value:
(queue)->fifo[(queue)->tail]; \
(queue)->tail = (((queue)->tail + 1) % (size)); \
(queue)->used--

Macro that de-queues a byte of data from a FIFO queue.

Parameters
queue Pointer to the FIFO queue.
size Size used to control the wrap-around of the FIFO pointers.

Definition at line 291 of file serial.h .

◆ FIFO_ENQUEUE

#define FIFO_ENQUEUE ( queue,
data,
size
)
Value:
do { \
(queue)->fifo[(queue)->head] = (data); \
(queue)->head = (((queue)->head + 1) % (size)); \
(queue)->used++; \
} while (0)

Macro that enqueues a byte of data in a FIFO queue.

Parameters
queue Pointer to the FIFO queue.
data Data byte to be enqueued.
size Size used to control the wrap-around of the FIFO pointers.

Definition at line 276 of file serial.h .

◆ halInternalUart1FlowControlRxIsEnabled

#define halInternalUart1FlowControlRxIsEnabled ( ) halInternalUartFlowControlRxIsEnabled (1)

This function is used in FIFO mode when flow control is enabled. It is called from emberSerialReadByte(), and based on the number of bytes used in the uart receive queue, decides when to tell the host it may resume transmission.

Parameters
port Serial port number (0 or 1). (Does nothing for port 0)

Definition at line 520 of file serial.h .

◆ halInternalUart1TxIsIdle

#define halInternalUart1TxIsIdle ( ) halInternalUartTxIsIdle (1)

This function is used in FIFO mode when flow control is enabled. It is called from emberSerialReadByte(), and based on the number of bytes used in the uart receive queue, decides when to tell the host it may resume transmission.

Parameters
port Serial port number (0 or 1). (Does nothing for port 0)

Definition at line 545 of file serial.h .

◆ halInternalUart1XonRefreshDone

#define halInternalUart1XonRefreshDone ( ) halInternalUartXonRefreshDone (1)

This function is used in FIFO mode when flow control is enabled. It is called from emberSerialReadByte(), and based on the number of bytes used in the uart receive queue, decides when to tell the host it may resume transmission.

Parameters
port Serial port number (0 or 1). (Does nothing for port 0)

Definition at line 532 of file serial.h .

◆ halInternalUartFlowControl

#define halInternalUartFlowControl ( port ) do {} while (false)

This function is used in FIFO mode when flow control is enabled. It is called from emberSerialReadByte(), and based on the number of bytes used in the uart receive queue, decides when to tell the host it may resume transmission.

Parameters
port Serial port number (0 or 1). (Does nothing for port 0)

Definition at line 488 of file serial.h .

◆ halInternalUartRxPump

#define halInternalUartRxPump ( port ) do {} while (false)

This function exists only in software UART (SOFTUART) mode on the EM3xx. This function is called by ::emberSerialReadByte(). It is responsible for maintaining synchronization between the emSerialRxQueue and the UART DMA.

Parameters
port Serial port number (0 or 1).

Definition at line 502 of file serial.h .

Enumeration Type Documentation

◆ SerialBaudRate

Assign numerical values for variables that hold Baud Rate parameters.

Enumerator
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD
DEFINE_BAUD

Definition at line 304 of file serial.h .

◆ SerialParity

CORTEXM3_EFM32_MICRO.

Assign numerical values for the types of parity. Use for variables that hold Parity parameters.

Enumerator
DEFINE_PARITY
DEFINE_PARITY
DEFINE_PARITY

Definition at line 374 of file serial.h .

Function Documentation

◆ emLoadSerialTx()

void emLoadSerialTx ( void )

◆ halHostEnqueueTx()

uint16_t halHostEnqueueTx ( const uint8_t * data,
uint16_t length
)

◆ halHostFlushBuffers()

void halHostFlushBuffers ( void )

◆ halHostFlushTx()

void halHostFlushTx ( void )

◆ halInternalForceReadUartByte()

EmberStatus halInternalForceReadUartByte ( uint8_t port,
uint8_t * dataByte
)

Directly reads a byte from the UART for reception, regardless of anything currently queued for reception. Does not block if a data byte has not been received.

Parameters
port Serial port number (0 or 1).
dataByte The byte to receive data into.

◆ halInternalForceWriteUartData()

EmberStatus halInternalForceWriteUartData ( uint8_t port,
uint8_t * data,
uint8_t length
)

Directly writes a byte to the UART for transmission, regardless of anything currently queued for transmission. Should wait for anything currently in the UART hardware registers to finish transmission first, and block until data is finished being sent.

Parameters
port Serial port number (0 or 1).
data Pointer to the data to be transmitted.
length The length of data to be transmitted

◆ halInternalPowerDownUart()

void halInternalPowerDownUart ( void )

This function is typically called by halPowerDown() and it is responsible for performing all the work internal to the UART needed to stop the UART before a sleep cycle.

◆ halInternalPowerUpUart()

void halInternalPowerUpUart ( void )

This function is typically called by halPowerUp() and it is responsible for performing all the work internal to the UART needed to restart the UART after a sleep cycle.

◆ halInternalRestartUart()

void halInternalRestartUart ( void )

This function is typically called by ::halInternalPowerUpBoard() and it is responsible for performing all the work internal to the UART needed to restart the UART after a sleep cycle. (For example, resyncing the DMA hardware and the serial FIFO.)

◆ halInternalStartUartTx()

void halInternalStartUartTx ( uint8_t port )

Called by serial code whenever anything is queued for transmission to start any interrupt-driven transmission. May be called when transmission is already in progess.

Parameters
port Serial port number (0 or 1).

◆ halInternalStopUartTx()

void halInternalStopUartTx ( uint8_t port )

Called by serial code to stop any interrupt-driven serial transmission currently in progress.

Parameters
port Serial port number (0 or 1).

◆ halInternalUartFlowControlRxIsEnabled()

bool halInternalUartFlowControlRxIsEnabled ( uint8_t port )

Checks to see if the host is allowed to send serial data to the ncp - i.e., it is not being held off by nCTS or an XOFF. Returns true is the host is able to send.

◆ halInternalUartInit()

EmberStatus halInternalUartInit ( uint8_t port,
SerialBaudRate rate,
SerialParity parity,
uint8_t stopBits
)

Initializes the UART to the given settings (same parameters as ::emberSerialInit() ).

Parameters
port Serial port number (0 or 1).
rate Baud rate (see SerialBaudRate).
parity Parity value (see SerialParity).
stopBits Number of stop bits.
Returns
An error code if initialization failed (such as invalid baud rate), otherise EMBER_SUCCESS.

◆ halInternalUartTxIsIdle()

bool halInternalUartTxIsIdle ( uint8_t port )

Returns true if the uart transmitter is idle, including the transmit shift register.

◆ halInternalUartXonRefreshDone()

bool halInternalUartXonRefreshDone ( uint8_t port )

When Xon/Xoff flow control is used, returns true if the host is not being held off and XON refreshing is complete.

◆ halInternalWaitUartTxComplete()

void halInternalWaitUartTxComplete ( uint8_t port )

Blocks until the UART has finished transmitting any data in its hardware registers.

Parameters
port Serial port number (0 or 1).

◆ halStackReceiveVuartMessage()

void halStackReceiveVuartMessage ( uint8_t * data,
uint8_t length
)

When using a debug build with virtual UART support, this API is called by the stack when virtual UART data has been received over the debug channel.

Parameters
data Pointer to the the data received
length Length of the data received

◆ serialCopyFromRx()

uint16_t serialCopyFromRx ( const uint8_t * data,
uint16_t length
)

◆ serialDropPacket()

bool serialDropPacket ( void )

Testing function implemented by the upper layer. Determines whether the next packet should be dropped. Returns true if the next packet should be dropped, false otherwise.