Public Attributes#

void(*
uint8_t

Public Attribute Documentation#

pHandle#

void(* SCommandNetworkManagement::pHandle) (void)

Definition at line 1734 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

mode#

uint8_t SCommandNetworkManagement::mode

Definition at line 1737 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

nodeID#

node_id_t SCommandNetworkManagement::nodeID

Definition at line 1738 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h