Public Attribute Documentation#

FrameConfig#

STransmitFrameConfig SSendDataMultiEx::FrameConfig

Definition at line 1717 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SourceNodeId#

uint8_t SSendDataMultiEx::SourceNodeId

Definition at line 1718 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

GroupId#

uint8_t SSendDataMultiEx::GroupId

Definition at line 1719 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

eKeyType#

enum SECURITY_KEY SSendDataMultiEx::eKeyType

Definition at line 1720 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h