Controller API.

Public Attributes#

void(*

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.

Public Attribute Documentation#

Handle#

void(* SSetSucNodeId::Handle) (void)

Definition at line 1362 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SucNodeId#

node_id_t SSetSucNodeId::SucNodeId

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.


Definition at line 1365 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

bSucEnable#

bool SSetSucNodeId::bSucEnable

Definition at line 1366 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

bTxLowPower#

bool SSetSucNodeId::bTxLowPower

Definition at line 1367 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

Capabilities#

uint8_t SSetSucNodeId::Capabilities

Definition at line 1368 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h