Public Attributes#

uint32_t
uint32_t
uint8_t *

Public Attribute Documentation#

offset#

uint32_t SCommandNvmBackupRestore::offset

Definition at line 1516 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

length#

uint32_t SCommandNvmBackupRestore::length

Definition at line 1517 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

nvmData#

uint8_t* SCommandNvmBackupRestore::nvmData

Definition at line 1518 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h