Public Attributes#
uint8_t
Public Attribute Documentation#
NodeMask#
NODE_MASK_TYPE SReceiveMulti::NodeMask
Definition at line
2164
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
Payload#
UReceiveCmdPayload SReceiveMulti::Payload
Definition at line
2165
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
iCommandLength#
uint8_t SReceiveMulti::iCommandLength
Definition at line
2166
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
RxOptions#
RECEIVE_OPTIONS_TYPE SReceiveMulti::RxOptions
Definition at line
2167
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h