Public Attributes#
void(*
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
bool
Node to have its return routes deleted..
Public Attribute Documentation#
Handle#
void(* SDeleteReturnRoute::Handle) (void)
Definition at line
1414
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
DestNodeId#
node_id_t SDeleteReturnRoute::DestNodeId
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
Definition at line
1418
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
bDeleteSuc#
bool SDeleteReturnRoute::bDeleteSuc
Node to have its return routes deleted..
Definition at line
1419
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h