Public Attributes#

ZW_APPLICATION_TX_BUFFER
uint8_t

Public Attribute Documentation#

rxBuffer#

ZW_APPLICATION_TX_BUFFER UReceiveCmdPayload::rxBuffer

Definition at line 2080 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

padding#

uint8_t UReceiveCmdPayload::padding[ZW_MAX_PAYLOAD_SIZE]

Definition at line 2081 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h