VERSION - Version Defines

Description

Version API.

Macros specifying the EMLIB and CMSIS version.

Macros

#define _EMLIB_VERSION   5.10.0
 
#define _EMLIB_VERSION_MAJOR   5
 
#define _EMLIB_VERSION_MINOR   10
 
#define _EMLIB_VERSION_PATCH   0
 
#define _CMSIS_VERSION   5.3.0
 Version number of targeted CMSIS package.
 
#define _CMSIS_VERSION_MAJOR   5
 Major version of CMSIS.
 
#define _CMSIS_VERSION_MINOR   3
 Minor version of CMSIS.
 
#define _CMSIS_VERSION_PATCH   0
 Patch revision of CMSIS.
 

Macro Definition Documentation

◆ _EMLIB_VERSION

#define _EMLIB_VERSION   5.10.0

◆ _EMLIB_VERSION_MAJOR

#define _EMLIB_VERSION_MAJOR   5

This is the 32-bit MCU SDK version. A new version system for EMLIB will be provided in a later release.

◆ _EMLIB_VERSION_MINOR

#define _EMLIB_VERSION_MINOR   10

This is the 32-bit MCU SDK version. A new version system for EMLIB will be provided in a later release.

◆ _EMLIB_VERSION_PATCH

#define _EMLIB_VERSION_PATCH   0

This is the 32-bit MCU SDK version. A new version system for EMLIB will be provided in a later release.

◆ _CMSIS_VERSION

#define _CMSIS_VERSION   5.3.0

Version number of targeted CMSIS package.

◆ _CMSIS_VERSION_MAJOR

#define _CMSIS_VERSION_MAJOR   5

Major version of CMSIS.

◆ _CMSIS_VERSION_MINOR

#define _CMSIS_VERSION_MINOR   3

Minor version of CMSIS.

◆ _CMSIS_VERSION_PATCH

#define _CMSIS_VERSION_PATCH   0

Patch revision of CMSIS.