MSC_EccConfig_TypeDef Struct Reference

ECC configuration.

#include <em_msc.h>

Data Fields

bool enableEccBank [MSC_ECC_BANKS]
 Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device.
 
uint32_t dmaChannels [2]
 Array of 2 DMA channel numbers to use for ECC initialization.
 

ECC configuration.

Field Documentation

◆ enableEccBank

bool MSC_EccConfig_TypeDef::enableEccBank[MSC_ECC_BANKS]

Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device.

◆ dmaChannels

uint32_t MSC_EccConfig_TypeDef::dmaChannels[2]

Array of 2 DMA channel numbers to use for ECC initialization.