CMU_HFXOInit_TypeDef Struct Reference
HFXO initialization structure.
#include <em_cmu.h>
Data Fields |
|
| uint16_t | ctuneStartup |
|
Startup phase CTUNE (load capacitance) value.
|
|
| uint16_t | ctuneSteadyState |
|
Steady-state phase CTUNE (load capacitance) value.
|
|
| uint16_t | xoCoreBiasTrimStartup |
|
Startup XO core bias current trim.
|
|
| uint16_t | xoCoreBiasTrimSteadyState |
|
Steady-state XO core bias current trim.
|
|
| uint8_t | timeoutPeakDetect |
|
Timeout - peak detection.
|
|
| uint8_t | timeoutSteady |
|
Timeout - steady-state.
|
|
| uint8_t | timeoutStartup |
|
Timeout - startup.
|
|
| CMU_OscMode_TypeDef | mode |
|
Oscillator mode.
|
|
HFXO initialization structure.
Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
Field Documentation
◆ ctuneStartup
| uint16_t CMU_HFXOInit_TypeDef::ctuneStartup |
Startup phase CTUNE (load capacitance) value.
◆ ctuneSteadyState
| uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState |
Steady-state phase CTUNE (load capacitance) value.
◆ xoCoreBiasTrimStartup
| uint16_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup |
Startup XO core bias current trim.
◆ xoCoreBiasTrimSteadyState
| uint16_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState |
Steady-state XO core bias current trim.
◆ timeoutPeakDetect
| uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect |
Timeout - peak detection.
◆ timeoutSteady
| uint8_t CMU_HFXOInit_TypeDef::timeoutSteady |
Timeout - steady-state.
◆ timeoutStartup
| uint8_t CMU_HFXOInit_TypeDef::timeoutStartup |
Timeout - startup.
◆ mode
| CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode |
Oscillator mode.