QSPI_DelayConfig_TypeDef Struct Reference

QSPI Device Delay Configuration Structure.

#include <em_qspi.h>

Data Fields

uint8_t deassert
The minimal delay to keep the chip select line de-asserted between two transactions.
uint8_t deviceSwitch
Delay between one chip select being de-activated and the activation of another.
uint8_t lastBit
Delay between last bit and chip select de-assert.
uint8_t firstBit
Delay chip select assert and first bit in a transaction.

QSPI Device Delay Configuration Structure.

Field Documentation

◆ deassert

uint8_t QSPI_DelayConfig_TypeDef::deassert

The minimal delay to keep the chip select line de-asserted between two transactions.

◆ deviceSwitch

uint8_t QSPI_DelayConfig_TypeDef::deviceSwitch

Delay between one chip select being de-activated and the activation of another.

◆ lastBit

uint8_t QSPI_DelayConfig_TypeDef::lastBit

Delay between last bit and chip select de-assert.

◆ firstBit

uint8_t QSPI_DelayConfig_TypeDef::firstBit

Delay chip select assert and first bit in a transaction.