TIMER_InitDTI_TypeDef Struct Reference
TIMER Dead Time Insertion (DTI) initialization structure.
#include <em_timer.h>
Data Fields |
|
bool | enable |
Enable DTI or leave it disabled until
TIMER_EnableDTI()
is called.
|
|
bool | activeLowOut |
DTI Output Polarity.
|
|
bool | invertComplementaryOut |
DTI Complementary Output Invert.
|
|
bool | autoRestart |
Enable Automatic Start-up functionality (when debugger exits).
|
|
bool | enablePrsSource |
Enable/disable PRS as DTI input.
|
|
TIMER_PRSSEL_TypeDef | prsSel |
Select which PRS channel as DTI input.
|
|
TIMER_Prescale_TypeDef | prescale |
DTI prescaling factor, if HFPER / HFPERB clock used.
|
|
unsigned int | riseTime |
DTI Rise Time.
|
|
unsigned int | fallTime |
DTI Fall Time.
|
|
uint32_t | outputsEnableMask |
DTI outputs enable bit mask, consisting of one bit per DTI output signal, i.e., CC0, CC1, CC2, CDTI0, CDTI1, and CDTI2.
|
|
bool | enableFaultSourceCoreLockup |
Enable core lockup as a fault source.
|
|
bool | enableFaultSourceDebugger |
Enable debugger as a fault source.
|
|
bool | enableFaultSourcePrsSel0 |
Enable PRS fault source 0 (
faultSourcePrsSel0
).
|
|
TIMER_PRSSEL_TypeDef | faultSourcePrsSel0 |
Select which PRS signal to be PRS fault source 0.
|
|
bool | enableFaultSourcePrsSel1 |
Enable PRS fault source 1 (
faultSourcePrsSel1
).
|
|
TIMER_PRSSEL_TypeDef | faultSourcePrsSel1 |
Select which PRS signal to be PRS fault source 1.
|
|
TIMER_DtiFaultAction_TypeDef | faultAction |
Fault Action.
|
|
TIMER Dead Time Insertion (DTI) initialization structure.
Field Documentation
◆ enable
bool TIMER_InitDTI_TypeDef::enable |
Enable DTI or leave it disabled until TIMER_EnableDTI() is called.
◆ activeLowOut
bool TIMER_InitDTI_TypeDef::activeLowOut |
DTI Output Polarity.
◆ invertComplementaryOut
bool TIMER_InitDTI_TypeDef::invertComplementaryOut |
DTI Complementary Output Invert.
◆ autoRestart
bool TIMER_InitDTI_TypeDef::autoRestart |
Enable Automatic Start-up functionality (when debugger exits).
◆ enablePrsSource
bool TIMER_InitDTI_TypeDef::enablePrsSource |
Enable/disable PRS as DTI input.