LESENSE_AltExDesc_TypeDef Struct Reference
Alternate excitation descriptor structure.
#include <em_lesense.h>
Data Fields | |
bool | enablePin |
Configure alternate excitation pins. | |
LESENSE_AltExPinIdle_TypeDef | idleConf |
Configure idle phase setup of alternate excitation pins. | |
bool | alwaysEx |
Configure how to control external alternate excitation pins. | |
Alternate excitation descriptor structure.
Field Documentation
◆ enablePin
bool LESENSE_AltExDesc_TypeDef::enablePin |
Configure alternate excitation pins.
If set, the corresponding alternate excitation pin/signal is enabled.
◆ idleConf
LESENSE_AltExPinIdle_TypeDef LESENSE_AltExDesc_TypeDef::idleConf |
Configure idle phase setup of alternate excitation pins.
The idleConf parameter is not valid when altExMap==lesenseAltExMapACMP.
◆ alwaysEx
bool LESENSE_AltExDesc_TypeDef::alwaysEx |
Configure how to control external alternate excitation pins.
Only applies if altExMap has been set to lesenseAltExMapALTEX. If true, excitation happens on the corresponding alternate excitation pin during excitation periods of all the enabled channels. If false, excitation happens on the corresponding alternate excitation pin ONLY during excitation period of the corresponding channel. The alwaysEx parameter is not valid when altExMap==lesenseAltExMapACMP.