RTCC_Init_TypeDef Struct Reference
RTCC initialization structure.
#include <em_rtcc.h>
Data Fields | |
bool | enable |
Enable/disable counting when initialization is completed. | |
bool | debugRun |
Enable/disable timer counting during debug halt. | |
bool | precntWrapOnCCV0 |
Enable/disable pre-counter wrap on ch. | |
bool | cntWrapOnCCV1 |
Enable/disable counter wrap on ch. | |
RTCC_CntPresc_TypeDef | presc |
Counter prescaler. | |
RTCC_PrescMode_TypeDef | prescMode |
Prescaler mode. | |
bool | enaBackupModeSet |
Enable/disable storing RTCC counter value in RTCC_CCV2 upon backup mode entry. | |
bool | enaOSCFailDetect |
Enable/disable the check that sets OSCFFAIL interrupt flag if no LFCLK-RTCC ticks are detected within one ULFRCO cycles. | |
RTCC_CntMode_TypeDef | cntMode |
Select operational mode of the counter. | |
bool | disLeapYearCorr |
Disable leap year correction for calendar mode. | |
RTCC initialization structure.
Field Documentation
◆ enable
bool RTCC_Init_TypeDef::enable |
Enable/disable counting when initialization is completed.
◆ debugRun
bool RTCC_Init_TypeDef::debugRun |
Enable/disable timer counting during debug halt.
◆ precntWrapOnCCV0
bool RTCC_Init_TypeDef::precntWrapOnCCV0 |
Enable/disable pre-counter wrap on ch.
0 CCV value.
◆ cntWrapOnCCV1
bool RTCC_Init_TypeDef::cntWrapOnCCV1 |
Enable/disable counter wrap on ch.
1 CCV value.
◆ presc
RTCC_CntPresc_TypeDef RTCC_Init_TypeDef::presc |
Counter prescaler.
◆ prescMode
RTCC_PrescMode_TypeDef RTCC_Init_TypeDef::prescMode |
Prescaler mode.
◆ enaBackupModeSet
bool RTCC_Init_TypeDef::enaBackupModeSet |
Enable/disable storing RTCC counter value in RTCC_CCV2 upon backup mode entry.
◆ enaOSCFailDetect
bool RTCC_Init_TypeDef::enaOSCFailDetect |
Enable/disable the check that sets OSCFFAIL interrupt flag if no LFCLK-RTCC ticks are detected within one ULFRCO cycles.
◆ cntMode
RTCC_CntMode_TypeDef RTCC_Init_TypeDef::cntMode |
Select operational mode of the counter.
◆ disLeapYearCorr
bool RTCC_Init_TypeDef::disLeapYearCorr |
Disable leap year correction for calendar mode.
When this parameter is set to false, February has 29 days if (year % 4 == 0). If set to true, February always has 28 days.