ACMP_VAConfig_TypeDef Struct Reference

VA Configuration structure.

#include <em_acmp.h>

Data Fields

ACMP_VAInput_TypeDef input
 VA voltage input source.
 
uint32_t div0
 A divider for VA voltage input source when ACMP output is 0.
 
uint32_t div1
 A divider for VA voltage input source when ACMP output is 1.
 

VA Configuration structure.

This structure is used to configure the VA voltage input source and its dividers.

Field Documentation

◆ input

ACMP_VAInput_TypeDef ACMP_VAConfig_TypeDef::input

VA voltage input source.

◆ div0

uint32_t ACMP_VAConfig_TypeDef::div0

A divider for VA voltage input source when ACMP output is 0.

This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.

VA divided = VA input * (div0 + 1) / 64

◆ div1

uint32_t ACMP_VAConfig_TypeDef::div1

A divider for VA voltage input source when ACMP output is 1.

This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.

VA divided = VA input * (div1 + 1) / 64