ACMP_VBConfig_TypeDef Struct Reference

VB Configuration structure.

#include <em_acmp.h>

Data Fields

ACMP_VBInput_TypeDef input
VB Voltage input source.
uint32_t div0
A divider for VB voltage input source when ACMP output is 0.
uint32_t div1
A divider for VB voltage input source when ACMP output is 1.

VB Configuration structure.

This structure is used to configure the VB voltage input source and its dividers.

Field Documentation

input

ACMP_VBInput_TypeDef ACMP_VBConfig_TypeDef::input

VB Voltage input source.

div0

uint32_t ACMP_VBConfig_TypeDef::div0

A divider for VB voltage input source when ACMP output is 0.

This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.

VB divided = VB input * (div0 + 1) / 64

div1

uint32_t ACMP_VBConfig_TypeDef::div1

A divider for VB voltage input source when ACMP output is 1.

This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.

VB divided = VB input * (div1 + 1) / 64