CMU - Clock Management Unit
Description
Clock management unit (CMU) Peripheral API.
This module contains functions for the CMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The CMU module controls oscillators, clocks gates, clock multiplexers, pre-scalers, calibration modules and wait-states.
Data Structures |
|
| struct | CMU_LFXOInit_TypeDef |
|
LFXO initialization structure.
|
|
| struct | CMU_HFXOInit_TypeDef |
|
HFXO initialization structure.
|
|
| struct | CMU_DPLLInit_TypeDef |
|
DPLL initialization structure.
|
|
Functions |
|
| uint32_t | CMU_Calibrate (uint32_t cycles, CMU_Select_TypeDef ref) |
|
Calibrate an oscillator.
|
|
| void | CMU_CalibrateConfig (uint32_t downCycles, CMU_Select_TypeDef downSel, CMU_Select_TypeDef upSel) |
|
Configure clock calibration.
|
|
| uint32_t | CMU_CalibrateCountGet (void) |
|
Get calibration count value.
|
|
| void | CMU_ClkOutPinConfig (uint32_t clkNo, CMU_Select_TypeDef sel, CMU_ClkDiv_TypeDef clkDiv, GPIO_Port_TypeDef port, unsigned int pin) |
|
Direct a clock to a GPIO pin.
|
|
| CMU_ClkDiv_TypeDef | CMU_ClockDivGet ( CMU_Clock_TypeDef clock) |
|
Get clock divisor.
|
|
| void | CMU_ClockDivSet ( CMU_Clock_TypeDef clock, CMU_ClkDiv_TypeDef div) |
|
Set clock divisor.
|
|
| void | CMU_ClockEnable ( CMU_Clock_TypeDef clock, bool enable) |
|
Enable/disable a clock.
|
|
| uint32_t | CMU_ClockFreqGet ( CMU_Clock_TypeDef clock) |
|
Get clock frequency for a clock point.
|
|
| CMU_Select_TypeDef | CMU_ClockSelectGet ( CMU_Clock_TypeDef clock) |
|
Get currently selected reference clock used for a clock branch.
|
|
| void | CMU_ClockSelectSet ( CMU_Clock_TypeDef clock, CMU_Select_TypeDef ref) |
|
Select reference clock/oscillator used for a clock branch.
|
|
| uint16_t | CMU_LF_ClockPrecisionGet ( CMU_Clock_TypeDef clock) |
|
Gets the precision (in PPM) of the specified low frequency clock branch.
|
|
| CMU_HFRCODPLLFreq_TypeDef | CMU_HFRCODPLLBandGet (void) |
|
Get HFRCODPLL band in use.
|
|
| void | CMU_HFRCODPLLBandSet ( CMU_HFRCODPLLFreq_TypeDef freq) |
|
Set HFRCODPLL band and the tuning value based on the value in the calibration table made during production.
|
|
| bool | CMU_DPLLLock (const CMU_DPLLInit_TypeDef *init) |
|
Lock the DPLL to a given frequency.
|
|
| void | CMU_HFXOInit (const CMU_HFXOInit_TypeDef *hfxoInit) |
|
Initialize all HFXO control registers.
|
|
| void | CMU_HFXOCTuneDeltaSet (int32_t delta) |
|
Set the HFXO crystal tuning delta.
|
|
| int32_t | CMU_HFXOCTuneDeltaGet (void) |
|
Get the HFXO crystal tuning delta.
|
|
| void | CMU_LFXOInit (const CMU_LFXOInit_TypeDef *lfxoInit) |
|
Initialize LFXO control registers.
|
|
| void | CMU_LFXOPrecisionSet (uint16_t precision) |
|
Sets LFXO's crystal precision, in PPM.
|
|
| uint32_t | CMU_OscillatorTuningGet ( CMU_Osc_TypeDef osc) |
|
Get oscillator frequency tuning setting.
|
|
| void | CMU_OscillatorTuningSet ( CMU_Osc_TypeDef osc, uint32_t val) |
|
Set the oscillator frequency tuning control.
|
|
| void | CMU_UpdateWaitStates (uint32_t freq, int vscale) |
|
Configure wait state settings necessary to switch to a given core clock frequency at a certain voltage scale level.
|
|
| void | CMU_PCNTClockExternalSet (unsigned int instance, bool external) |
|
Select the PCNTn clock.
|
|
| void | CMU_CalibrateCont (bool enable) |
|
Configure continuous calibration mode.
|
|
| void | CMU_CalibrateStart (void) |
|
Start calibration.
|
|
| void | CMU_CalibrateStop (void) |
|
Stop calibration counters.
|
|
| void | CMU_DPLLUnlock (void) |
|
Unlock the DPLL.
|
|
| void | CMU_IntClear (uint32_t flags) |
|
Clear one or more pending CMU interrupt flags.
|
|
| void | CMU_IntDisable (uint32_t flags) |
|
Disable one or more CMU interrupt sources.
|
|
| void | CMU_IntEnable (uint32_t flags) |
|
Enable one or more CMU interrupt sources.
|
|
| uint32_t | CMU_IntGet (void) |
|
Get pending CMU interrupt sources.
|
|
| uint32_t | CMU_IntGetEnabled (void) |
|
Get enabled and pending CMU interrupt flags.
|
|
| void | CMU_IntSet (uint32_t flags) |
|
Set one or more pending CMU interrupt sources.
|
|
| void | CMU_Lock (void) |
|
Lock CMU register access in order to protect registers contents against unintended modification.
|
|
| void | CMU_OscillatorEnable ( CMU_Osc_TypeDef osc, bool enable, bool wait) |
|
Enable/disable oscillator.
|
|
| void | CMU_Unlock (void) |
|
Unlock CMU register access so that writing to registers is possible.
|
|
| void | CMU_WdogLock (void) |
|
Lock WDOG register access in order to protect registers contents against unintended modification.
|
|
| void | CMU_WdogUnlock (void) |
|
Unlock WDOG register access so that writing to registers is possible.
|
|
| uint32_t | CMU_PrescToLog2 (uint32_t presc) |
|
Convert prescaler dividend to a logarithmic value.
|
|
Macros |
|
| #define | CMU_HFRCODPLL_MIN cmuHFRCODPLLFreq_1M0Hz |
|
HFRCODPLL maximum frequency.
|
|
| #define | CMU_HFRCODPLL_MAX cmuHFRCODPLLFreq_80M0Hz |
|
HFRCODPLL minimum frequency.
|
|
| #define | CMU_LFXOINIT_DEFAULT |
|
Default LFXO initialization values for XTAL mode.
|
|
| #define | CMU_LFXOINIT_EXTERNAL_CLOCK |
|
Default LFXO initialization values for external clock mode.
|
|
| #define | CMU_LFXOINIT_EXTERNAL_SINE |
|
Default LFXO initialization values for external sine mode.
|
|
| #define | CMU_HFXOINIT_DEFAULT |
|
Default HFXO initialization values for XTAL mode.
|
|
| #define | CMU_HFXOINIT_EXTERNAL_SINE |
|
Default HFXO initialization values for external sine mode.
|
|
| #define | CMU_HFXOINIT_EXTERNAL_SINEPKDET |
|
Default HFXO initialization values for external sine mode with peak detector.
|
|
| #define | CMU_DPLL_LFXO_TO_40MHZ |
|
DPLL initialization values for 39,998,805 Hz using LFXO as reference clock, M=2 and N=3661.
|
|
| #define | CMU_DPLL_HFXO_TO_76_8MHZ |
|
DPLL initialization values for 76,800,000 Hz using HFXO as reference clock, M = 1919, N = 3839.
|
|
| #define | CMU_DPLL_HFXO_TO_80MHZ |
|
DPLL initialization values for 80,000,000 Hz using HFXO as reference clock, M = 1919, N = 3999.
|
|
| #define | CMU_DPLLINIT_DEFAULT |
|
Default configurations for DPLL initialization.
|
|
Typedefs |
|
| typedef uint32_t | CMU_ClkDiv_TypeDef |
|
Clock divider configuration.
|
|
Enumerations |
|
| enum |
CMU_HFRCODPLLFreq_TypeDef
{
cmuHFRCODPLLFreq_1M0Hz = 1000000U, cmuHFRCODPLLFreq_2M0Hz = 2000000U, cmuHFRCODPLLFreq_4M0Hz = 4000000U, cmuHFRCODPLLFreq_7M0Hz = 7000000U, cmuHFRCODPLLFreq_13M0Hz = 13000000U, cmuHFRCODPLLFreq_16M0Hz = 16000000U, cmuHFRCODPLLFreq_19M0Hz = 19000000U, cmuHFRCODPLLFreq_26M0Hz = 26000000U, cmuHFRCODPLLFreq_32M0Hz = 32000000U, cmuHFRCODPLLFreq_38M0Hz = 38000000U, cmuHFRCODPLLFreq_48M0Hz = 48000000U, cmuHFRCODPLLFreq_56M0Hz = 56000000U, cmuHFRCODPLLFreq_64M0Hz = 64000000U, cmuHFRCODPLLFreq_80M0Hz = 80000000U, cmuHFRCODPLLFreq_UserDefined = 0 } |
|
HFRCODPLL frequency bands.
|
|
| enum |
CMU_Clock_TypeDef
{
cmuClock_SYSCLK = (CMU_SYSCLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_SYSTICK = (CMU_SYSTICK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_HCLK = (CMU_HCLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_EXPCLK = (CMU_EXPCLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_PCLK = (CMU_PCLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_LSPCLK = (CMU_LSPCLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_TRACECLK = (CMU_TRACECLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_EM01GRPACLK = (CMU_EM01GRPACLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_EM01GRPBCLK = (CMU_EM01GRPBCLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_EUART0CLK = (CMU_EUART0CLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_IADCCLK = (CMU_IADCCLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_EM23GRPACLK = (CMU_EM23GRPACLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_WDOG0CLK = (CMU_WDOG0CLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_RTCCCLK = (CMU_RTCCCLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_EM4GRPACLK = (CMU_EM4GRPACLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_DPLLREFCLK = (CMU_DPLLREFCLK_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_CRYPTOAES , cmuClock_CRYPTOPK , cmuClock_CORE = (CMU_CORE_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_PDMREF = (CMU_PDMREF_BRANCH << CMU_CLK_BRANCH_POS), cmuClock_LDMA , cmuClock_LDMAXBAR , cmuClock_RADIOAES , cmuClock_GPCRC , cmuClock_TIMER0 , cmuClock_TIMER1 , cmuClock_TIMER2 , cmuClock_TIMER3 , cmuClock_TIMER4 , cmuClock_USART0 , cmuClock_USART1 , cmuClock_IADC0 , cmuClock_AMUXCP0 , cmuClock_LETIMER0 , cmuClock_WDOG0 , cmuClock_I2C0 , cmuClock_I2C1 , cmuClock_SYSCFG , cmuClock_DPLL0 , cmuClock_HFRCO0 , cmuClock_HFXO , cmuClock_FSRCO , cmuClock_LFRCO , cmuClock_LFXO , cmuClock_ULFRCO , cmuClock_EUART0 , cmuClock_PDM , cmuClock_GPIO , cmuClock_PRS , cmuClock_BURAM , cmuClock_BURTC , cmuClock_RTCC , cmuClock_DCDC , cmuClock_CRYPTOACC , cmuClock_SMU , cmuClock_ICACHE , cmuClock_MSC } |
|
Clock points in CMU clock-tree.
|
|
| enum |
CMU_Osc_TypeDef
{
cmuOsc_LFXO , cmuOsc_LFRCO , cmuOsc_FSRCO , cmuOsc_HFXO , cmuOsc_HFRCODPLL , cmuOsc_ULFRCO } |
|
Oscillator types.
|
|
| enum |
CMU_Select_TypeDef
{
cmuSelect_Error , cmuSelect_Disabled , cmuSelect_FSRCO , cmuSelect_HFXO , cmuSelect_HFXORT , cmuSelect_HFRCODPLL , cmuSelect_HFRCODPLLRT , cmuSelect_CLKIN0 , cmuSelect_LFXO , cmuSelect_LFRCO , cmuSelect_ULFRCO , cmuSelect_HCLK , cmuSelect_SYSCLK , cmuSelect_HCLKDIV1024 , cmuSelect_EM01GRPACLK , cmuSelect_EM23GRPACLK , cmuSelect_EXPCLK , cmuSelect_PRS , cmuSelect_TEMPOSC , cmuSelect_PFMOSC , cmuSelect_BIASOSC } |
|
Selectable clock sources.
|
|
| enum |
CMU_DPLLEdgeSel_TypeDef
{
cmuDPLLEdgeSel_Fall = 0, cmuDPLLEdgeSel_Rise = 1 } |
|
DPLL reference clock edge detect selector.
|
|
| enum |
CMU_DPLLLockMode_TypeDef
{
cmuDPLLLockMode_Freq = _DPLL_CFG_MODE_FLL, cmuDPLLLockMode_Phase = _DPLL_CFG_MODE_PLL } |
|
DPLL lock mode selector.
|
|
| enum |
CMU_LfxoOscMode_TypeDef
{
cmuLfxoOscMode_Crystal = _LFXO_CFG_MODE_XTAL, cmuLfxoOscMode_AcCoupledSine = _LFXO_CFG_MODE_BUFEXTCLK, cmuLfxoOscMode_External = _LFXO_CFG_MODE_DIGEXTCLK } |
|
LFXO oscillator modes.
|
|
| enum |
CMU_LfxoStartupDelay_TypeDef
{
cmuLfxoStartupDelay_2Cycles = _LFXO_CFG_TIMEOUT_CYCLES2, cmuLfxoStartupDelay_256Cycles = _LFXO_CFG_TIMEOUT_CYCLES256, cmuLfxoStartupDelay_1KCycles = _LFXO_CFG_TIMEOUT_CYCLES1K, cmuLfxoStartupDelay_2KCycles = _LFXO_CFG_TIMEOUT_CYCLES2K, cmuLfxoStartupDelay_4KCycles = _LFXO_CFG_TIMEOUT_CYCLES4K, cmuLfxoStartupDelay_8KCycles = _LFXO_CFG_TIMEOUT_CYCLES8K, cmuLfxoStartupDelay_16KCycles = _LFXO_CFG_TIMEOUT_CYCLES16K, cmuLfxoStartupDelay_32KCycles = _LFXO_CFG_TIMEOUT_CYCLES32K } |
|
LFXO start-up timeout delay.
|
|
| enum |
CMU_HfxoOscMode_TypeDef
{
cmuHfxoOscMode_Crystal = _HFXO_CFG_MODE_XTAL, cmuHfxoOscMode_ExternalSine = _HFXO_CFG_MODE_EXTCLK } |
|
HFXO oscillator modes.
|
|
| enum |
CMU_HfxoCbLsbTimeout_TypeDef
{
cmuHfxoCbLsbTimeout_8us = _HFXO_XTALCFG_TIMEOUTCBLSB_T8US, cmuHfxoCbLsbTimeout_20us = _HFXO_XTALCFG_TIMEOUTCBLSB_T20US, cmuHfxoCbLsbTimeout_41us = _HFXO_XTALCFG_TIMEOUTCBLSB_T41US, cmuHfxoCbLsbTimeout_62us = _HFXO_XTALCFG_TIMEOUTCBLSB_T62US, cmuHfxoCbLsbTimeout_83us = _HFXO_XTALCFG_TIMEOUTCBLSB_T83US, cmuHfxoCbLsbTimeout_104us = _HFXO_XTALCFG_TIMEOUTCBLSB_T104US, cmuHfxoCbLsbTimeout_125us = _HFXO_XTALCFG_TIMEOUTCBLSB_T125US, cmuHfxoCbLsbTimeout_166us = _HFXO_XTALCFG_TIMEOUTCBLSB_T166US, cmuHfxoCbLsbTimeout_208us = _HFXO_XTALCFG_TIMEOUTCBLSB_T208US, cmuHfxoCbLsbTimeout_250us = _HFXO_XTALCFG_TIMEOUTCBLSB_T250US, cmuHfxoCbLsbTimeout_333us = _HFXO_XTALCFG_TIMEOUTCBLSB_T333US, cmuHfxoCbLsbTimeout_416us = _HFXO_XTALCFG_TIMEOUTCBLSB_T416US, cmuHfxoCbLsbTimeout_833us = _HFXO_XTALCFG_TIMEOUTCBLSB_T833US, cmuHfxoCbLsbTimeout_1250us = _HFXO_XTALCFG_TIMEOUTCBLSB_T1250US, cmuHfxoCbLsbTimeout_2083us = _HFXO_XTALCFG_TIMEOUTCBLSB_T2083US, cmuHfxoCbLsbTimeout_3750us = _HFXO_XTALCFG_TIMEOUTCBLSB_T3750US } |
|
HFXO core bias LSB change timeout.
|
|
| enum |
CMU_HfxoSteadyStateTimeout_TypeDef
{
cmuHfxoSteadyStateTimeout_16us = _HFXO_XTALCFG_TIMEOUTSTEADY_T16US, cmuHfxoSteadyStateTimeout_41us = _HFXO_XTALCFG_TIMEOUTSTEADY_T41US, cmuHfxoSteadyStateTimeout_83us = _HFXO_XTALCFG_TIMEOUTSTEADY_T83US, cmuHfxoSteadyStateTimeout_125us = _HFXO_XTALCFG_TIMEOUTSTEADY_T125US, cmuHfxoSteadyStateTimeout_166us = _HFXO_XTALCFG_TIMEOUTSTEADY_T166US, cmuHfxoSteadyStateTimeout_208us = _HFXO_XTALCFG_TIMEOUTSTEADY_T208US, cmuHfxoSteadyStateTimeout_250us = _HFXO_XTALCFG_TIMEOUTSTEADY_T250US, cmuHfxoSteadyStateTimeout_333us = _HFXO_XTALCFG_TIMEOUTSTEADY_T333US, cmuHfxoSteadyStateTimeout_416us = _HFXO_XTALCFG_TIMEOUTSTEADY_T416US, cmuHfxoSteadyStateTimeout_500us = _HFXO_XTALCFG_TIMEOUTSTEADY_T500US, cmuHfxoSteadyStateTimeout_666us = _HFXO_XTALCFG_TIMEOUTSTEADY_T666US, cmuHfxoSteadyStateTimeout_833us = _HFXO_XTALCFG_TIMEOUTSTEADY_T833US, cmuHfxoSteadyStateTimeout_1666us = _HFXO_XTALCFG_TIMEOUTSTEADY_T1666US, cmuHfxoSteadyStateTimeout_2500us = _HFXO_XTALCFG_TIMEOUTSTEADY_T2500US, cmuHfxoSteadyStateTimeout_4166us = _HFXO_XTALCFG_TIMEOUTSTEADY_T4166US, cmuHfxoSteadyStateTimeout_7500us = _HFXO_XTALCFG_TIMEOUTSTEADY_T7500US } |
|
HFXO steady state timeout.
|
|
| enum |
CMU_HfxoCoreDegen_TypeDef
{
cmuHfxoCoreDegen_None = _HFXO_XTALCTRL_COREDGENANA_NONE, cmuHfxoCoreDegen_33 = _HFXO_XTALCTRL_COREDGENANA_DGEN33, cmuHfxoCoreDegen_50 = _HFXO_XTALCTRL_COREDGENANA_DGEN50, cmuHfxoCoreDegen_100 = _HFXO_XTALCTRL_COREDGENANA_DGEN100 } |
|
HFXO core degeneration control.
|
|
| enum |
CMU_HfxoCtuneFixCap_TypeDef
{
cmuHfxoCtuneFixCap_None = _HFXO_XTALCTRL_CTUNEFIXANA_NONE, cmuHfxoCtuneFixCap_Xi = _HFXO_XTALCTRL_CTUNEFIXANA_XI, cmuHfxoCtuneFixCap_Xo = _HFXO_XTALCTRL_CTUNEFIXANA_XO, cmuHfxoCtuneFixCap_Both = _HFXO_XTALCTRL_CTUNEFIXANA_BOTH } |
|
HFXO XI and XO pin fixed capacitor control.
|
|
| enum |
CMU_Precision_TypeDef
{
cmuPrecisionDefault , cmuPrecisionHigh } |
|
Oscillator precision modes.
|
|
Function Documentation
◆ CMU_Calibrate()
| uint32_t CMU_Calibrate | ( | uint32_t |
cycles,
|
| CMU_Select_TypeDef |
ref
|
||
| ) |
Calibrate an oscillator.
Run a calibration of a selectable reference clock againt HCLK. Please refer to the reference manual, CMU chapter, for further details.
- Note
- This function will not return until calibration measurement is completed.
- Parameters
-
[in] cyclesThe number of HCLK cycles to run calibration. Increasing this number increases precision, but the calibration will take more time. [in] refThe reference clock used to compare against HCLK.
- Returns
- The number of ticks the selected reference clock ticked while running cycles ticks of the HCLK clock.
◆ CMU_CalibrateConfig()
| void CMU_CalibrateConfig | ( | uint32_t |
downCycles,
|
| CMU_Select_TypeDef |
downSel,
|
||
| CMU_Select_TypeDef |
upSel
|
||
| ) |
Configure clock calibration.
Configure a calibration for a selectable clock source against another selectable reference clock. Refer to the reference manual, CMU chapter, for further details.
- Note
- After configuration, a call to CMU_CalibrateStart() is required, and the resulting calibration value can be read with the CMU_CalibrateCountGet() function call.
- Parameters
-
[in] downCyclesThe number of downSel clock cycles to run calibration. Increasing this number increases precision, but the calibration will take more time. [in] downSelThe clock which will be counted down downCycles cycles. [in] upSelThe reference clock, the number of cycles generated by this clock will be counted and added up, the result can be given with the CMU_CalibrateCountGet() function call.
◆ CMU_CalibrateCountGet()
| uint32_t CMU_CalibrateCountGet | ( | void |
|
) |
Get calibration count value.
- Note
- If continuous calibration mode is active, calibration busy will almost always be off, and reading the value will be just needed, where the normal case would be that this function call has been triggered by the CALRDY interrupt flag.
- Returns
- Calibration count, the number of UPSEL clocks (see CMU_CalibrateConfig() ) in the period of DOWNSEL oscillator clock cycles configured by a previous write operation to CMU->CALCNT.
◆ CMU_ClkOutPinConfig()
| void CMU_ClkOutPinConfig | ( | uint32_t |
clkNo,
|
| CMU_Select_TypeDef |
sel,
|
||
| CMU_ClkDiv_TypeDef |
clkDiv,
|
||
| GPIO_Port_TypeDef |
port,
|
||
| unsigned int |
pin
|
||
| ) |
Direct a clock to a GPIO pin.
- Parameters
-
[in] clkNoSelects between CLKOUT0, CLKOUT1 or CLKOUT2 outputs. Use values 0,1or 2. [in] selSelect clock source. [in] clkDivSelect a clock divisor (1..32). Only applicable when cmuSelect_EXPCLK is slexted as clock source. [in] portGPIO port. [in] pinGPIO pin.
- Note
- Refer to the reference manual and the datasheet for details on which GPIO port/pins that are available.
◆ CMU_ClockDivGet()
| CMU_ClkDiv_TypeDef CMU_ClockDivGet | ( | CMU_Clock_TypeDef |
clock
|
) |
Get clock divisor.
- Parameters
-
[in] clockClock point to get divisor for. Notice that not all clock points have a divisors. Please refer to CMU overview in reference manual.
- Returns
-
The current clock point divisor. 1 is returned if
clockspecifies a clock point without divisor.
◆ CMU_ClockDivSet()
| void CMU_ClockDivSet | ( | CMU_Clock_TypeDef |
clock,
|
| CMU_ClkDiv_TypeDef |
div
|
||
| ) |
Set clock divisor.
- Parameters
-
[in] clockClock point to set divisor for. Notice that not all clock points have a divisor, please refer to CMU overview in the reference manual. [in] divThe clock divisor to use.
◆ CMU_ClockEnable()
| void CMU_ClockEnable | ( | CMU_Clock_TypeDef |
clock,
|
| bool |
enable
|
||
| ) |
Enable/disable a clock.
Module clocks sre disabled after reset. If a module clock is disabled, the registers of that module are not accessible and accessing such registers will hardfault the Cortex core.
- Parameters
-
[in] clockThe clock to enable/disable. [in] enable- true - enable specified clock.
- false - disable specified clock.
◆ CMU_ClockFreqGet()
| uint32_t CMU_ClockFreqGet | ( | CMU_Clock_TypeDef |
clock
|
) |
Get clock frequency for a clock point.
- Parameters
-
[in] clockClock point to fetch frequency for.
- Returns
- The current frequency in Hz.
◆ CMU_ClockSelectGet()
| CMU_Select_TypeDef CMU_ClockSelectGet | ( | CMU_Clock_TypeDef |
clock
|
) |
Get currently selected reference clock used for a clock branch.
- Parameters
-
[in] clockClock branch to fetch selected ref. clock for.
- Returns
-
Reference clock used for clocking selected branch,
cmuSelect_Error
if invalid
clockprovided.
◆ CMU_ClockSelectSet()
| void CMU_ClockSelectSet | ( | CMU_Clock_TypeDef |
clock,
|
| CMU_Select_TypeDef |
ref
|
||
| ) |
Select reference clock/oscillator used for a clock branch.
- Parameters
-
[in] clockClock branch to select reference clock for. [in] refReference selected for clocking, please refer to reference manual for for details on which reference is available for a specific clock branch.
◆ CMU_LF_ClockPrecisionGet()
| uint16_t CMU_LF_ClockPrecisionGet | ( | CMU_Clock_TypeDef |
clock
|
) |
Gets the precision (in PPM) of the specified low frequency clock branch.
- Parameters
-
[in] clockClock branch.
- Returns
- Precision, in PPM, of the specified clock branch.
- Note
- This function is only for internal usage.
- The current implementation of this function is used to determine if the clock has a precision <= 500 ppm or not (which is the minimum required for BLE). Future version of this function should provide more accurate precision numbers to allow for further optimizations from the stacks.
◆ CMU_HFRCODPLLBandGet()
| CMU_HFRCODPLLFreq_TypeDef CMU_HFRCODPLLBandGet | ( | void |
|
) |
Get HFRCODPLL band in use.
- Returns
- HFRCODPLL band in use.
◆ CMU_HFRCODPLLBandSet()
| void CMU_HFRCODPLLBandSet | ( | CMU_HFRCODPLLFreq_TypeDef |
freq
|
) |
Set HFRCODPLL band and the tuning value based on the value in the calibration table made during production.
- Parameters
-
[in] freqHFRCODPLL frequency band to activate.
◆ CMU_DPLLLock()
| bool CMU_DPLLLock | ( | const CMU_DPLLInit_TypeDef * |
init
|
) |
Lock the DPLL to a given frequency.
The frequency is given by: Fout = Fref * (N+1) / (M+1).
- Note
-
This function does not check if the given N & M values will actually produce the desired target frequency.
N & M limitations:
300 < N <= 4095
0 <= M <= 4095
Any peripheral running off HFRCODPLL should be switched to a lower frequency clock (if possible) prior to calling this function to avoid over-clocking.
- Parameters
-
[in] initDPLL setup parameter struct.
- Returns
- Returns false on invalid target frequency or DPLL locking error.
◆ CMU_HFXOInit()
| void CMU_HFXOInit | ( | const CMU_HFXOInit_TypeDef * |
hfxoInit
|
) |
Initialize all HFXO control registers.
- Note
- HFXO configuration should be obtained from a configuration tool, app note or crystal datasheet. This function returns early if HFXO is already selected as SYSCLK.
- Parameters
-
[in] hfxoInitHFXO setup parameters.
◆ CMU_HFXOCTuneDeltaSet()
| void CMU_HFXOCTuneDeltaSet | ( | int32_t |
delta
|
) |
Set the HFXO crystal tuning delta.
- Parameters
-
[in] deltaChip dependent crystal capacitor bank delta between HFXO XI and XO.
- Note
- The delta between XI and XO is applicable for the series 2 EFR32xG2x devices only.
◆ CMU_HFXOCTuneDeltaGet()
| int32_t CMU_HFXOCTuneDeltaGet | ( | void |
|
) |
Get the HFXO crystal tuning delta.
- Returns
- Chip dependent crystal capacitor bank tuning delta.
◆ CMU_LFXOInit()
| void CMU_LFXOInit | ( | const CMU_LFXOInit_TypeDef * |
lfxoInit
|
) |
Initialize LFXO control registers.
- Note
- LFXO configuration should be obtained from a configuration tool, app note or crystal datasheet. This function disables the LFXO to ensure a valid state before update.
- Parameters
-
[in] lfxoInitLFXO setup parameters
◆ CMU_LFXOPrecisionSet()
| void CMU_LFXOPrecisionSet | ( | uint16_t |
precision
|
) |
Sets LFXO's crystal precision, in PPM.
- Note
- LFXO precision should be obtained from a crystal datasheet.
- Parameters
-
[in] precisionLFXO's crystal precision, in PPM.
◆ CMU_OscillatorTuningGet()
| uint32_t CMU_OscillatorTuningGet | ( | CMU_Osc_TypeDef |
osc
|
) |
Get oscillator frequency tuning setting.
- Parameters
-
[in] oscOscillator to get tuning value for.
- Returns
- The oscillator frequency tuning setting in use.
◆ CMU_OscillatorTuningSet()
| void CMU_OscillatorTuningSet | ( | CMU_Osc_TypeDef |
osc,
|
| uint32_t |
val
|
||
| ) |
Set the oscillator frequency tuning control.
- Note
- Oscillator tuning is done during production, and the tuning value is automatically loaded after a reset. Changing the tuning value from the calibrated value is for more advanced use. Certain oscillators also have build-in tuning optimization.
- Parameters
-
[in] oscOscillator to set tuning value for. [in] valThe oscillator frequency tuning setting to use.
◆ CMU_UpdateWaitStates()
| void CMU_UpdateWaitStates | ( | uint32_t |
freq,
|
| int |
vscale
|
||
| ) |
Configure wait state settings necessary to switch to a given core clock frequency at a certain voltage scale level.
This function will set up the necessary flash wait states. Updating the wait state configuration must be done before increasing the clock frequency and it must be done after decreasing the clock frequency. Updating the wait state configuration must be done before core voltage is decreased and it must be done after a core voltage is increased.
- Parameters
-
[in] freqThe core clock frequency to configure wait-states. [in] vscaleThe voltage scale to configure wait-states. Expected values are 0 or 1, higher number is lower voltage. - 0 = 1.1 V (VSCALE2)
- 1 = 1.0 V (VSCALE1)
◆ CMU_PCNTClockExternalSet()
| void CMU_PCNTClockExternalSet | ( | unsigned int |
instance,
|
| bool |
external
|
||
| ) |
Select the PCNTn clock.
- Parameters
-
[in] instancePCNT instance number to set selected clock source for. [in] externalSet to true to select the external clock, false to select EM23GRPACLK.
◆ CMU_CalibrateCont()
|
inline |
Configure continuous calibration mode.
- Parameters
-
[in] enableIf true, enables continuous calibration, if false disables continuous calibration.
◆ CMU_CalibrateStart()
|
inline |
Start calibration.
- Note
- This call is usually invoked after CMU_CalibrateConfig() and possibly CMU_CalibrateCont() .
◆ CMU_CalibrateStop()
|
inline |
Stop calibration counters.
◆ CMU_DPLLUnlock()
|
inline |
Unlock the DPLL.
- Note
- The HFRCODPLL oscillator is not turned off.
◆ CMU_IntClear()
|
inline |
Clear one or more pending CMU interrupt flags.
- Parameters
-
[in] flagsCMU interrupt sources to clear.
◆ CMU_IntDisable()
|
inline |
Disable one or more CMU interrupt sources.
- Parameters
-
[in] flagsCMU interrupt sources to disable.
◆ CMU_IntEnable()
|
inline |
Enable one or more CMU interrupt sources.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using CMU_IntClear() prior to enabling if such a pending interrupt should be ignored.
- Parameters
-
[in] flagsCMU interrupt sources to enable.
◆ CMU_IntGet()
|
inline |
Get pending CMU interrupt sources.
- Returns
- CMU interrupt sources pending.
◆ CMU_IntGetEnabled()
|
inline |
Get enabled and pending CMU interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- The event bits are not cleared by the use of this function.
- Returns
-
Pending and enabled CMU interrupt sources. The return value is the bitwise AND of
- the enabled interrupt sources in CMU_IEN and
- the pending interrupt flags CMU_IF
◆ CMU_IntSet()
|
inline |
Set one or more pending CMU interrupt sources.
- Parameters
-
[in] flagsCMU interrupt sources to set to pending.
◆ CMU_Lock()
|
inline |
Lock CMU register access in order to protect registers contents against unintended modification.
See the reference manual for CMU registers that will be locked.
- Note
- If locking the CMU registers, they must be unlocked prior to using any CMU API functions modifying CMU registers protected by the lock.
◆ CMU_OscillatorEnable()
|
inline |
Enable/disable oscillator.
- Note
- This is a dummy function to solve backward compatibility issues.
- Parameters
-
[in] oscThe oscillator to enable/disable. [in] enable- true - enable specified oscillator.
- false - disable specified oscillator.
[in] waitOnly used if enableis true.- true - wait for oscillator start-up time to timeout before returning.
- false - do not wait for oscillator start-up time to timeout before returning.
◆ CMU_Unlock()
|
inline |
Unlock CMU register access so that writing to registers is possible.
◆ CMU_WdogLock()
|
inline |
Lock WDOG register access in order to protect registers contents against unintended modification.
- Note
- If locking the WDOG registers, they must be unlocked prior to using any emlib API functions modifying registers protected by the lock.
◆ CMU_WdogUnlock()
|
inline |
Unlock WDOG register access so that writing to registers is possible.
◆ CMU_PrescToLog2()
|
inline |
Convert prescaler dividend to a logarithmic value.
It only works for even numbers equal to 2^n.
- Parameters
-
[in] prescAn unscaled dividend (dividend = presc + 1).
- Returns
- Logarithm of 2, as used by fixed 2^n prescalers.
Macro Definition Documentation
◆ CMU_HFRCODPLL_MIN
| #define CMU_HFRCODPLL_MIN cmuHFRCODPLLFreq_1M0Hz |
HFRCODPLL maximum frequency.
◆ CMU_HFRCODPLL_MAX
| #define CMU_HFRCODPLL_MAX cmuHFRCODPLLFreq_80M0Hz |
HFRCODPLL minimum frequency.
◆ CMU_LFXOINIT_DEFAULT
| #define CMU_LFXOINIT_DEFAULT |
Default LFXO initialization values for XTAL mode.
◆ CMU_LFXOINIT_EXTERNAL_CLOCK
| #define CMU_LFXOINIT_EXTERNAL_CLOCK |
Default LFXO initialization values for external clock mode.
◆ CMU_LFXOINIT_EXTERNAL_SINE
| #define CMU_LFXOINIT_EXTERNAL_SINE |
Default LFXO initialization values for external sine mode.
◆ CMU_HFXOINIT_DEFAULT
| #define CMU_HFXOINIT_DEFAULT |
Default HFXO initialization values for XTAL mode.
◆ CMU_HFXOINIT_EXTERNAL_SINE
| #define CMU_HFXOINIT_EXTERNAL_SINE |
Default HFXO initialization values for external sine mode.
◆ CMU_HFXOINIT_EXTERNAL_SINEPKDET
| #define CMU_HFXOINIT_EXTERNAL_SINEPKDET |
Default HFXO initialization values for external sine mode with peak detector.
◆ CMU_DPLL_LFXO_TO_40MHZ
| #define CMU_DPLL_LFXO_TO_40MHZ |
DPLL initialization values for 39,998,805 Hz using LFXO as reference clock, M=2 and N=3661.
◆ CMU_DPLL_HFXO_TO_76_8MHZ
| #define CMU_DPLL_HFXO_TO_76_8MHZ |
DPLL initialization values for 76,800,000 Hz using HFXO as reference clock, M = 1919, N = 3839.
◆ CMU_DPLL_HFXO_TO_80MHZ
| #define CMU_DPLL_HFXO_TO_80MHZ |
DPLL initialization values for 80,000,000 Hz using HFXO as reference clock, M = 1919, N = 3999.
◆ CMU_DPLLINIT_DEFAULT
| #define CMU_DPLLINIT_DEFAULT |
Default configurations for DPLL initialization.
When using this macro you need to modify the N and M factor and the desired frequency to match the components placed on the board.
Typedef Documentation
◆ CMU_ClkDiv_TypeDef
| typedef uint32_t CMU_ClkDiv_TypeDef |
Clock divider configuration.
Enumeration Type Documentation
◆ CMU_HFRCODPLLFreq_TypeDef
HFRCODPLL frequency bands.
◆ CMU_Clock_TypeDef
| enum CMU_Clock_TypeDef |
Clock points in CMU clock-tree.
◆ CMU_Osc_TypeDef
| enum CMU_Osc_TypeDef |
Oscillator types.
◆ CMU_Select_TypeDef
| enum CMU_Select_TypeDef |
Selectable clock sources.
◆ CMU_DPLLEdgeSel_TypeDef
◆ CMU_DPLLLockMode_TypeDef
◆ CMU_LfxoOscMode_TypeDef
◆ CMU_LfxoStartupDelay_TypeDef
LFXO start-up timeout delay.
◆ CMU_HfxoOscMode_TypeDef
◆ CMU_HfxoCbLsbTimeout_TypeDef
HFXO core bias LSB change timeout.
◆ CMU_HfxoSteadyStateTimeout_TypeDef
HFXO steady state timeout.