EUSART_IrDAInit_TypeDef Struct Reference
IrDA Initialization structure.
#include <em_eusart.h>
Data Fields |
|
| EUSART_UartInit_TypeDef | init |
|
General EUSART initialization structure.
|
|
| bool | irDALowFrequencyEnable |
|
Enable the IrDA low frequency mode. Only RX operation are enabled.
|
|
| EUSART_IrDARxFilterEnable_TypeDef | irDARxFilterEnable |
|
Set to enable filter on IrDA demodulator.
|
|
| EUSART_IrDAPulseWidth_Typedef | irDAPulseWidth |
|
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.
|
|
IrDA Initialization structure.
Field Documentation
◆ init
| EUSART_UartInit_TypeDef EUSART_IrDAInit_TypeDef::init |
General EUSART initialization structure.
◆ irDALowFrequencyEnable
| bool EUSART_IrDAInit_TypeDef::irDALowFrequencyEnable |
Enable the IrDA low frequency mode. Only RX operation are enabled.
◆ irDARxFilterEnable
| EUSART_IrDARxFilterEnable_TypeDef EUSART_IrDAInit_TypeDef::irDARxFilterEnable |
Set to enable filter on IrDA demodulator.
◆ irDAPulseWidth
| EUSART_IrDAPulseWidth_Typedef EUSART_IrDAInit_TypeDef::irDAPulseWidth |
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.