SE - Secure Element
Description
Secure Element peripheral API.
Abstraction of the Secure Element's mailbox interface.
For series 2 devices with a part number that is xG23 or higher, the following step is necessary for basic operation:
Clock enable:
- Note
- The high-level SE API has been moved to the SE manager, and the implementation in em_se should not be used.
- Using the SE's mailbox is not thread-safe in EMLIB, and accessing the SE's mailbox both in regular and IRQ context is not safe. SE operations should be performed using the SE manager if possible.
Modules |
|
Deprecated Functions
|
|
|
Deprecated Functions.
|
|
Data Structures |
|
| struct | SE_DataTransfer_t |
|
SE DMA transfer descriptor.
|
|
| struct | SE_Command_t |
|
SE Command structure to which all commands to the SE must adhere.
|
|
Functions |
|
| void | SE_addDataInput ( SE_Command_t *command, SE_DataTransfer_t *data) |
|
Add input data to a command.
|
|
| void | SE_addDataOutput ( SE_Command_t *command, SE_DataTransfer_t *data) |
|
Add output data to a command.
|
|
| void | SE_addParameter ( SE_Command_t *command, uint32_t parameter) |
|
Add a parameter to a command.
|
|
| void | SE_executeCommand ( SE_Command_t *command) |
|
Execute the passed command.
|
|
| SE_Response_t | SE_getVersion (uint32_t *version) |
|
Get current SE version.
|
|
| SE_Response_t | SE_getConfigStatusBits (uint32_t *cfgStatus) |
|
Get VSE configuration and status bits.
|
|
| SE_Response_t | SE_ackCommand ( SE_Command_t *command) |
|
Acknowledge and get status and output data of a completed command.
|
|
| bool | SE_isCommandCompleted (void) |
|
Check whether the running command has completed.
|
|
| uint32_t | SE_readExecutedCommand (void) |
|
Read the previously executed command.
|
|
| SE_Response_t | SE_readCommandResponse (void) |
|
Read the status of the previously executed command.
|
|
| void | SE_waitCommandCompletion (void) |
|
Wait for completion of the current command.
|
|
| void | SE_disableInterrupt (uint32_t flags) |
|
Disable one or more SE interrupts.
|
|
| void | SE_enableInterrupt (uint32_t flags) |
|
Enable one or more SE interrupts.
|
|
| bool | rootIsOutputMailboxValid (void) |
|
Check whether the VSE Output Mailbox is valid.
|
|
Macros |
|
| #define | SE_RESPONSE_MAILBOX_INVALID 0x00FE0000UL |
|
Root Code Mailbox is invalid.
|
|
| #define | SE_RESPONSE_MAILBOX_VALID 0xE5ECC0DEUL |
|
Root Code Mailbox magic word.
|
|
| #define | SE_RESPONSE_MASK 0x000F0000UL |
|
Response status codes for the Secure Element.
|
|
| #define | SE_RESPONSE_OK 0x00000000UL |
|
Command executed successfully or signature was successfully validated.
|
|
| #define | SE_FIFO_MAX_PARAMETERS 13U |
|
Maximum amount of parameters supported by the hardware FIFO.
|
|
| #define | SE_DATATRANSFER_STOP 0x00000001UL |
|
Stop datatransfer.
|
|
| #define | SE_DATATRANSFER_DISCARD 0x40000000UL |
|
Discard datatransfer.
|
|
| #define | SE_DATATRANSFER_REALIGN 0x20000000UL |
|
Realign datatransfer.
|
|
| #define | SE_DATATRANSFER_CONSTADDRESS 0x10000000UL |
|
Datatransfer Const Address.
|
|
| #define | SE_DATATRANSFER_LENGTH_MASK 0x0FFFFFFFUL |
|
Stop Length Mask.
|
|
| #define | SE_MAX_PARAMETERS 4U |
|
Maximum amount of parameters for largest command in defined command set.
|
|
| #define | SE_DATATRANSFER_DEFAULT (address, length) |
|
Default initialization of data transfer struct.
|
|
| #define | SE_COMMAND_DEFAULT (command) |
|
Default initialization of command struct.
|
|
Typedefs |
|
| typedef uint32_t | SE_Response_t |
|
Possible responses to a command.
|
|
Function Documentation
◆ SE_addDataInput()
| void SE_addDataInput | ( | SE_Command_t * |
command,
|
| SE_DataTransfer_t * |
data
|
||
| ) |
Add input data to a command.
This function adds a buffer of input data to the given SE command structure The buffer gets appended by reference at the end of the list of already added buffers.
- Note
- Note that this function does not copy either the data buffer or the buffer structure, so make sure to keep the data object in scope until the command has been executed by the secure element.
- Parameters
-
[in] commandPointer to an SE command structure. [in] dataPointer to a data transfer structure.
◆ SE_addDataOutput()
| void SE_addDataOutput | ( | SE_Command_t * |
command,
|
| SE_DataTransfer_t * |
data
|
||
| ) |
Add output data to a command.
This function adds a buffer of output data to the given command structure The buffer gets appended by reference at the end of the list of already added buffers.
- Note
- Note that this function does not copy either the data buffer or the buffer structure, so make sure to keep the data object in scope until the command has been executed by the secure element.
- Parameters
-
[in] commandPointer to an SE command structure. [in] dataPointer to a data transfer structure.
◆ SE_addParameter()
| void SE_addParameter | ( | SE_Command_t * |
command,
|
| uint32_t |
parameter
|
||
| ) |
Add a parameter to a command.
This function adds a parameter word to the passed command.
- Note
- Make sure to not exceed SE_MAX_PARAMETERS .
- Parameters
-
[in] commandPointer to a filled-out SE command structure. [in] parameterParameter to add.
◆ SE_executeCommand()
| void SE_executeCommand | ( | SE_Command_t * |
command
|
) |
Execute the passed command.
This function starts the execution of the passed command by the secure element. When started, wait for the RXINT interrupt flag, or call SE_waitCommandCompletion to busy-wait. After completion, you have to call SE_readCommandResponse to get the command's execution status.
- Parameters
-
[in] commandPointer to a filled-out SE command structure.
◆ SE_getVersion()
| SE_Response_t SE_getVersion | ( | uint32_t * |
version
|
) |
Get current SE version.
This function returns the current VSE version
- Parameters
-
[in] versionPointer to location where to copy the version of VSE to.
- Returns
- One of the SE_RESPONSE return codes: SE_RESPONSE_OK when the command was executed successfully SE_RESPONSE_INVALID_PARAMETER when an invalid parameter was passed SE_RESPONSE_MAILBOX_INVALID when the mailbox content is invalid
◆ SE_getConfigStatusBits()
| SE_Response_t SE_getConfigStatusBits | ( | uint32_t * |
cfgStatus
|
) |
Get VSE configuration and status bits.
This function returns the current VSE configuration and status bits. The following list explains what the different bits in cfgStatus indicate. A bit value of 1 means enabled, while 0 means disabled:
- [0]: Secure boot
- [1]: Verify secure boot certificate
- [2]: Anti-rollback
- [3]: Narrow page lock
- [4]: Full page lock The following status bits can be read with VSE versions higher than 1.2.2.
- [10]: Debug port lock
- [11]: Device erase enabled
- [12]: Secure debug enabled
- [15]: Debug port register state, 1 if the debug port is locked.
- Parameters
-
[out] cfgStatusPointer to location to copy Configuration Status bits into.
- Note
- This function will check that the mailbox content is valid before reading the status bits. If the command response has already been read with a call to SE_ackCommand() , the validity check will fail, and the config status bits cannot be read before a reset has occurred.
- Returns
- One of the SE_RESPONSE return codes: SE_RESPONSE_OK when the command was executed successfully SE_RESPONSE_INVALID_PARAMETER when an invalid parameter was passed SE_RESPONSE_MAILBOX_INVALID when the mailbox content is invalid
◆ SE_ackCommand()
| SE_Response_t SE_ackCommand | ( | SE_Command_t * |
command
|
) |
Acknowledge and get status and output data of a completed command.
This function acknowledges and gets the status and output data of a completed mailbox command. The mailbox command is acknowledged by inverting all bits in the checksum (XOR with 0xFFFFFFFF). The output data is copied into the linked list of output buffers pointed to in the given command data structure.
- Parameters
-
[in] commandPointer to an SE command structure.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully or a signature was successfully verified, SE_RESPONSE_INVALID_COMMANDwhen the command ID was not recognized, SE_RESPONSE_AUTHORIZATION_ERRORwhen the command is not authorized, SE_RESPONSE_INVALID_SIGNATUREwhen signature verification failed, SE_RESPONSE_BUS_ERRORwhen a bus error was thrown during the command, e.g. because of conflicting Secure/Non-Secure memory accesses, SE_RESPONSE_CRYPTO_ERRORon an internal SE failure, or SE_RESPONSE_INVALID_PARAMETERwhen an invalid parameter was passed SE_RESPONSE_MAILBOX_INVALIDwhen mailbox command not done or invalid
◆ SE_isCommandCompleted()
| bool SE_isCommandCompleted | ( | void |
|
) |
Check whether the running command has completed.
This function polls the SE-to-host mailbox interrupt flag.
- Returns
- True if a command has completed and the result is available
◆ SE_readExecutedCommand()
| uint32_t SE_readExecutedCommand | ( | void |
|
) |
Read the previously executed command.
This function reads the previously executed command.
- Returns
- One of the SE command words. SE_RESPONSE_MAILBOX_INVALID when the mailbox content is invalid.
◆ SE_readCommandResponse()
| SE_Response_t SE_readCommandResponse | ( | void |
|
) |
Read the status of the previously executed command.
This function reads the status of the previously executed command.
- Returns
- One of the SE_RESPONSE return codes: SE_RESPONSE_OK when the command was executed successfully or a signature was successfully verified, SE_RESPONSE_INVALID_COMMAND when the command ID was not recognized, SE_RESPONSE_AUTHORIZATION_ERROR when the command is not authorized, SE_RESPONSE_INVALID_SIGNATURE when signature verification failed, SE_RESPONSE_BUS_ERROR when a bus error was thrown during the command, e.g. because of conflicting Secure/Non-Secure memory accesses, SE_RESPONSE_CRYPTO_ERROR on an internal SE failure, or SE_RESPONSE_INVALID_PARAMETER when an invalid parameter was passed SE_RESPONSE_MAILBOX_INVALID when the mailbox content is invalid
◆ SE_waitCommandCompletion()
|
inline |
Wait for completion of the current command.
This function "busy"-waits until the execution of the ongoing instruction has completed.
◆ SE_disableInterrupt()
|
inline |
Disable one or more SE interrupts.
- Parameters
-
[in] flagsSE interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the Secure Element module (SE_CONFIGURATION_(TX/RX)INTEN).
◆ SE_enableInterrupt()
|
inline |
Enable one or more SE interrupts.
- Parameters
-
[in] flagsSE interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the Secure Element module (SEMAILBOX_CONFIGURATION_TXINTEN or SEMAILBOX_CONFIGURATION_RXINTEN).
◆ rootIsOutputMailboxValid()
| bool rootIsOutputMailboxValid | ( | void |
|
) |
Check whether the VSE Output Mailbox is valid.
- Returns
- True if the VSE Output Mailbox is valid (magic and checksum OK)
Macro Definition Documentation
◆ SE_RESPONSE_MAILBOX_INVALID
| #define SE_RESPONSE_MAILBOX_INVALID 0x00FE0000UL |
Root Code Mailbox is invalid.
◆ SE_RESPONSE_MAILBOX_VALID
| #define SE_RESPONSE_MAILBOX_VALID 0xE5ECC0DEUL |
Root Code Mailbox magic word.
◆ SE_RESPONSE_MASK
| #define SE_RESPONSE_MASK 0x000F0000UL |
Response status codes for the Secure Element.
◆ SE_RESPONSE_OK
| #define SE_RESPONSE_OK 0x00000000UL |
Command executed successfully or signature was successfully validated.
◆ SE_FIFO_MAX_PARAMETERS
| #define SE_FIFO_MAX_PARAMETERS 13U |
Maximum amount of parameters supported by the hardware FIFO.
◆ SE_DATATRANSFER_STOP
| #define SE_DATATRANSFER_STOP 0x00000001UL |
Stop datatransfer.
◆ SE_DATATRANSFER_DISCARD
| #define SE_DATATRANSFER_DISCARD 0x40000000UL |
Discard datatransfer.
◆ SE_DATATRANSFER_REALIGN
| #define SE_DATATRANSFER_REALIGN 0x20000000UL |
Realign datatransfer.
◆ SE_DATATRANSFER_CONSTADDRESS
| #define SE_DATATRANSFER_CONSTADDRESS 0x10000000UL |
Datatransfer Const Address.
◆ SE_DATATRANSFER_LENGTH_MASK
| #define SE_DATATRANSFER_LENGTH_MASK 0x0FFFFFFFUL |
Stop Length Mask.
◆ SE_MAX_PARAMETERS
| #define SE_MAX_PARAMETERS 4U |
Maximum amount of parameters for largest command in defined command set.
◆ SE_DATATRANSFER_DEFAULT
| #define SE_DATATRANSFER_DEFAULT | ( |
address,
|
|
length
|
|||
| ) |
Default initialization of data transfer struct.
◆ SE_COMMAND_DEFAULT
| #define SE_COMMAND_DEFAULT | ( |
command
|
) |
Default initialization of command struct.
Typedef Documentation
◆ SE_Response_t
| typedef uint32_t SE_Response_t |
Possible responses to a command.