BURTC - Backup RTC
Description
Backup Real Time Counter (BURTC) Peripheral API.
This module contains functions to control the BURTC peripheral of Silicon Labs 32-bit MCUs. The Backup Real Time Counter allows timekeeping in all energy modes. The Backup RTC is also available when the system is in backup mode.
| Data Structures | |
| struct | BURTC_Init_TypeDef | 
| BURTC initialization structure for Series 0 devices. | |
| Functions | |
| void | BURTC_IntClear (uint32_t flags) | 
| Clear one or more pending BURTC interrupts. | |
| void | BURTC_IntDisable (uint32_t flags) | 
| Disable one or more BURTC interrupts. | |
| void | BURTC_IntEnable (uint32_t flags) | 
| Enable one or more BURTC interrupts. | |
| uint32_t | BURTC_IntGet (void) | 
| Get pending BURTC interrupt flags. | |
| uint32_t | BURTC_IntGetEnabled (void) | 
| Get enabled and pending BURTC interrupt flags. | |
| void | BURTC_IntSet (uint32_t flags) | 
| Set one or more pending BURTC interrupts from SW. | |
| uint32_t | BURTC_Status (void) | 
| Status of BURTC RAM, timestamp and LP Mode. | |
| void | BURTC_StatusClear (void) | 
| Clear and reset BURTC status register. | |
| void | BURTC_SyncWait (void) | 
| Wait for the BURTC to complete all synchronization of register changes and commands. | |
| uint32_t | BURTC_CounterGet (void) | 
| Get BURTC counter. | |
| uint32_t | BURTC_TimestampGet (void) | 
| Get BURTC timestamp for entering BU. | |
| void | BURTC_FreezeEnable (bool enable) | 
| Freeze register updates until enabled. | |
| void | BURTC_Powerdown (bool enable) | 
| Shut down power to retention register bank. | |
| void | BURTC_RetRegSet (uint32_t num, uint32_t data) | 
| Set a value in one of the retention registers. | |
| uint32_t | BURTC_RetRegGet (uint32_t num) | 
| Read a value from one of the retention registers. | |
| void | BURTC_Lock (void) | 
| Lock BURTC registers, which will protect from writing new config settings. | |
| void | BURTC_Unlock (void) | 
| Unlock BURTC registers, which will enable write access to change configuration. | |
| void | BURTC_Reset (void) | 
| Restore BURTC to reset state. | |
| void | BURTC_Init (const BURTC_Init_TypeDef *burtcInit) | 
| Initialize BURTC. | |
| void | BURTC_Enable (bool enable) | 
| Enable or Disable BURTC peripheral reset and start counter. | |
| void | BURTC_CounterReset (void) | 
| Reset counter. | |
| void | BURTC_CompareSet (unsigned int comp, uint32_t value) | 
| Set BURTC compare channel. | |
| uint32_t | BURTC_CompareGet (unsigned int comp) | 
| Get the BURTC compare value. | |
| uint32_t | BURTC_ClockFreqGet (void) | 
| Get the clock frequency of the BURTC. | |
| Macros | |
| #define | burtcClkDiv_1 1 | 
| BURTC clock divisors. | |
| #define | burtcClkDiv_2 2 | 
| Divide clock by 2. | |
| #define | burtcClkDiv_4 4 | 
| Divide clock by 4. | |
| #define | burtcClkDiv_8 8 | 
| Divide clock by 8. | |
| #define | burtcClkDiv_16 16 | 
| Divide clock by 16. | |
| #define | burtcClkDiv_32 32 | 
| Divide clock by 32. | |
| #define | burtcClkDiv_64 64 | 
| Divide clock by 64. | |
| #define | burtcClkDiv_128 128 | 
| Divide clock by 128. | |
| #define | BURTC_INIT_DEFAULT | 
| Default configuration for BURTC initialization structure. | |
| Enumerations | |
| enum | BURTC_ClkSel_TypeDef
         
         { burtcClkSelULFRCO = BURTC_CTRL_CLKSEL_ULFRCO, burtcClkSelLFRCO = BURTC_CTRL_CLKSEL_LFRCO, burtcClkSelLFXO = BURTC_CTRL_CLKSEL_LFXO } | 
| BURTC clock selection. | |
| enum | BURTC_Mode_TypeDef
         
         { burtcModeDisable = BURTC_CTRL_MODE_DISABLE, burtcModeEM2 = BURTC_CTRL_MODE_EM2EN, burtcModeEM3 = BURTC_CTRL_MODE_EM3EN, burtcModeEM4 = BURTC_CTRL_MODE_EM4EN } | 
| BURTC mode of operation. | |
| enum | BURTC_LP_TypeDef
         
         { burtcLPDisable = BURTC_LPMODE_LPMODE_DISABLE, burtcLPEnable = BURTC_LPMODE_LPMODE_ENABLE, burtcLPBU = BURTC_LPMODE_LPMODE_BUEN } | 
| BURTC low power mode. | |
Function Documentation
◆ BURTC_IntClear()
| 
 | inline | 
Clear one or more pending BURTC interrupts.
- Parameters
- 
         [in] flagsBURTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). 
◆ BURTC_IntDisable()
| 
 | inline | 
Disable one or more BURTC interrupts.
- Parameters
- 
         [in] flagsBURTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). 
◆ BURTC_IntEnable()
| 
 | inline | 
Enable one or more BURTC interrupts.
- Note
- Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using BURTC_IntClear() prior to enabling if a pending interrupt should be ignored.
- Parameters
- 
         [in] flagsBURTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). 
◆ BURTC_IntGet()
| 
 | inline | 
Get pending BURTC interrupt flags.
- Note
- This function does not clear the event bits.
- Returns
- Pending BURTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
◆ BURTC_IntGetEnabled()
| 
 | inline | 
Get enabled and pending BURTC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending BURTC interrupt sources that is also enabled. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
◆ BURTC_IntSet()
| 
 | inline | 
Set one or more pending BURTC interrupts from SW.
- Parameters
- 
         [in] flagsBURTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). 
◆ BURTC_Status()
| 
 | inline | 
Status of BURTC RAM, timestamp and LP Mode.
- Returns
- A mask logically OR-ed status bits
◆ BURTC_StatusClear()
| 
 | inline | 
Clear and reset BURTC status register.
◆ BURTC_SyncWait()
| 
 | inline | 
Wait for the BURTC to complete all synchronization of register changes and commands.
◆ BURTC_CounterGet()
| 
 | inline | 
Get BURTC counter.
- Returns
- BURTC counter value
◆ BURTC_TimestampGet()
| 
 | inline | 
Get BURTC timestamp for entering BU.
- Returns
- BURTC Time Stamp value
◆ BURTC_FreezeEnable()
| 
 | inline | 
Freeze register updates until enabled.
- Parameters
- 
         [in] enableIf true, registers are not updated until enabled again. 
◆ BURTC_Powerdown()
| 
 | inline | 
Shut down power to retention register bank.
- Parameters
- 
         [in] enableIf true, shuts off power to retention registers. 
- Note
- When power retention is disabled, it can't be enabled again (until reset).
◆ BURTC_RetRegSet()
| 
 | inline | 
Set a value in one of the retention registers.
- Parameters
- 
         [in] numRegister to set [in] dataValue to put into register 
◆ BURTC_RetRegGet()
| 
 | inline | 
Read a value from one of the retention registers.
- Parameters
- 
         [in] numRetention Register to read 
- Returns
- Value of the retention register
◆ BURTC_Lock()
| 
 | inline | 
Lock BURTC registers, which will protect from writing new config settings.
◆ BURTC_Unlock()
| 
 | inline | 
Unlock BURTC registers, which will enable write access to change configuration.
◆ BURTC_Reset()
| void BURTC_Reset | ( | void | 
            | ) | 
Restore BURTC to reset state.
- Note
- Before accessing the BURTC, BURSTEN in RMU->CTRL must be cleared. LOCK will not be reset to default value, as this will disable access to core BURTC registers.
◆ BURTC_Init()
| void BURTC_Init | ( | const BURTC_Init_TypeDef * | 
            burtcInit
            | ) | 
Initialize BURTC.
Configures the BURTC peripheral.
- Note
- 
         Before initialization, BURTC module must first be enabled by clearing the reset bit in the RMU, i.e.,
         * RMU_ResetControl(rmuResetBU, rmuResetModeClear); * Compare channel 0 must be configured outside this function, before initialization if enable is set to true. The counter will always be reset.
- Parameters
- 
         [in] burtcInitA pointer to the BURTC initialization structure. 
◆ BURTC_Enable()
| void BURTC_Enable | ( | bool | 
            enable
            | ) | 
Enable or Disable BURTC peripheral reset and start counter.
- Parameters
- 
         [in] enableIf true; asserts reset to BURTC, halts counter, if false; deassert reset 
◆ BURTC_CounterReset()
| void BURTC_CounterReset | ( | void | 
            | ) | 
Reset counter.
◆ BURTC_CompareSet()
| void BURTC_CompareSet | ( | unsigned int | 
            comp,
            | 
| uint32_t | 
            value
            | ||
| ) | 
Set BURTC compare channel.
- Parameters
- 
         [in] compCompare the channel index, must be 0 for current devices. [in] valueNew compare value. 
◆ BURTC_CompareGet()
| uint32_t BURTC_CompareGet | ( | unsigned int | 
            comp
            | ) | 
Get the BURTC compare value.
- Parameters
- 
         [in] compCompare the channel index value, must be 0 for Giant/Leopard Gecko. 
- Returns
- The currently configured value for this compare channel.
◆ BURTC_ClockFreqGet()
| uint32_t BURTC_ClockFreqGet | ( | void | 
            | ) | 
Get the clock frequency of the BURTC.
- Returns
- The current frequency in Hz.
Ultra-low frequency (1 kHz) clock.
Low-frequency RC oscillator.
Low-frequency crystal oscillator.
Macro Definition Documentation
◆ burtcClkDiv_1
| #define burtcClkDiv_1 1 | 
BURTC clock divisors.
These values are valid for the BURTC prescaler. Divide clock by 1.
◆ burtcClkDiv_2
| #define burtcClkDiv_2 2 | 
Divide clock by 2.
◆ burtcClkDiv_4
| #define burtcClkDiv_4 4 | 
Divide clock by 4.
◆ burtcClkDiv_8
| #define burtcClkDiv_8 8 | 
Divide clock by 8.
◆ burtcClkDiv_16
| #define burtcClkDiv_16 16 | 
Divide clock by 16.
◆ burtcClkDiv_32
| #define burtcClkDiv_32 32 | 
Divide clock by 32.
◆ burtcClkDiv_64
| #define burtcClkDiv_64 64 | 
Divide clock by 64.
◆ burtcClkDiv_128
| #define burtcClkDiv_128 128 | 
Divide clock by 128.
◆ BURTC_INIT_DEFAULT
| #define BURTC_INIT_DEFAULT | 
Default configuration for BURTC initialization structure.
Enumeration Type Documentation
◆ BURTC_ClkSel_TypeDef
| enum BURTC_ClkSel_TypeDef | 
◆ BURTC_Mode_TypeDef
| enum BURTC_Mode_TypeDef | 
◆ BURTC_LP_TypeDef
| enum BURTC_LP_TypeDef |