Bootload
Description
Methods to verify and bootload application images.
Function Documentation
| bool bootload_checkApplicationPropertiesMagic | ( | void * |
appProperties
|
) |
Check application properties magic.
- Parameters
-
appPropertiesPointer to ApplicationProperties_t
- Returns
- True if the application properties magic is valid.
| bool bootload_checkApplicationPropertiesVersion | ( | void * |
appProperties
|
) |
Check application properties struct version.
- Parameters
-
appPropertiesPointer to ApplicationProperties_t
- Returns
- True if the application properties struct version is compatible with the bootloader.
| bool bootload_verifyApplication | ( | uint32_t |
startAddress
|
) |
Verify the application image stored in the Flash memory starting at the address startAddress.
If secure boot is enforced, the function will only return true if the cryptographic signature of the application is valid. Else, the application is verified according to the signature type defined in the ApplicationProperties_t structure embedded in the application. Silicon Labs wireless stacks declare this structure. Applications, which are not using a full wireless stack may need to instantiate the structure.
Examples of results when secure boot is not enforced:
- App has no signature: Valid if initial stack pointer and program counter have reasonable values
- App has CRC checksum: Valid if checksum is valid
- App has ECDSA signature: Valid if ECDSA signature is valid.
When secure boot is enforced, only ECDSA-signed applications with a valid signature are considered valid.
- Parameters
-
[in] startAddressStarting address of the application
- Returns
- True if the image is deemed valid
| void bootload_bootloaderCallback | ( | uint32_t |
offset,
|
| uint8_t |
data[],
|
||
| size_t |
length,
|
||
| void * |
context
|
||
| ) |
Bootloader upgrade callback implementation.
- Parameters
-
offsetOffset of bootloader data (byte counter incrementing from 0) dataRaw bootloader data lengthSize in bytes of raw bootloader data. contextA context variable defined by the implementation that is implementing this callback.
| void bootload_applicationCallback | ( | uint32_t |
address,
|
| uint8_t |
data[],
|
||
| size_t |
length,
|
||
| void * |
context
|
||
| ) |
Image data callback implementation.
- Parameters
-
addressAddress (inside the raw image) the data starts at dataRaw image data lengthSize in bytes of raw image data. Always constrained to a multiple of four. contextA context variable defined by the implementation that is implementing this callback.
| bool bootloader_enforceSecureBoot | ( | void |
|
) |
Indicates whether the bootloader should enforce a secure boot.
- Returns
- True if secure boot is to be enforced.
| bool bootload_commitBootloaderUpgrade | ( | uint32_t |
upgradeAddress,
|
| uint32_t |
size
|
||
| ) |
Perform a bootloader upgrade using the upgrade image present at upgradeAddress with length size.
If the bootloader upgrade process starts successfully, this function does not return and execution will resume from the reset handler of the upgraded bootloader.
- Parameters
-
[in] upgradeAddressThe starting address of the upgrade image [in] sizeThe length of the upgrade image in bytes
- Returns
- False if the bootloader upgrade process didn't start
| bool bootload_verifyApplicationVersion | ( | uint32_t |
appVersion,
|
| bool |
checkRemainingAppUpgrades
|
||
| ) |
Verify the application version for rollback protection.
- Parameters
-
[in] appVersionApplication version to be checked. [in] checkRemainingAppUpgradesCheck remaining application upgrades.
- Returns
-
True if the application version is higher or equal than the application versions seen. False if the application version is lower than the application versions seen. False if no remaining application upgrades are left when
checkRemainingAppUpgradesis true.
| bool bootload_storeApplicationVersion | ( | uint32_t |
startAddress
|
) |
Store the application version.
- Note
- Only the version of the verified application should be stored.
- Parameters
-
startAddressStart address of application.
- Returns
- True if application version is successfully stored.
| uint32_t bootload_remainingApplicationUpgrades | ( | void |
|
) |
Count the total remaining number of application upgrades.
- Returns
- remaining number of application upgrades.
| void bootload_storeApplicationVersionResetMagic | ( | void |
|
) |
Store application version reset magic.
- Note
- Store application version reset magic to ensure that application versions are cleaned after a bootloader upgrade.
| void bootload_removeStoredApplicationVersions | ( | void |
|
) |
Clean the application versions seen.
- Note
- The application versions are cleaned only if this is requested with a magic and the application version storage is not already empty.
| uint32_t bootload_getApplicationVersionStorageCapacity | ( | void |
|
) |
Get application version storage capacity.
- Returns
- Application version storage capacity.
| uint32_t* bootload_getApplicationVersionStoragePtr | ( | uint32_t |
index
|
) |
Get address of the application version storage buffer.
- Parameters
-
indexIndex of the application version storage buffer.
- Returns
- Address of the application version storage buffer with the given index.
| bool bootload_gotCertificate | ( | void * |
appProp
|
) |
Check if application contains a certificate.
- Parameters
-
appPropPointer to ApplicationProperties_t of application.
- Returns
- True if application contains a certificate.
| bool bootload_verifyCertificate | ( | void * |
cert
|
) |
Verify a certificate with bootloader certificate.
- Parameters
-
certPointer to ApplicationCertificate_t .
- Returns
- True if certificate is verified.
| bool bootload_verifyApplicationCertificate | ( | void * |
appProp,
|
| void * |
gotCert
|
||
| ) |
Verify application certificate.
- Note
-
This function will always return true if certificate support is not enabled. Also true if
appPropdoes not contain any certificate and direct signed applications can be accepted.
- Parameters
-
appPropPointer to ApplicationProperties_t of application. gotCertBoolean to store application certificate presence.
- Returns
- True if application certificate is verified.
| bool bootload_checkSeUpgradeVersion | ( | uint32_t |
upgradeVersion
|
) |
Check that an SE upgrade with a given version number is allowed to be installed.
This will only be true if the upgrade version is higher than the running version.
- Parameters
-
[in] upgradeVersionThe version of the SE upgrade image
- Returns
- True if the SE upgrade image should be installed
| bool bootload_commitSeUpgrade | ( | uint32_t |
upgradeAddress
|
) |
Perform an SE upgrade using the upgrade image present at upgradeAddress.
If the SE upgrade process starts successfully, this function does not return and execution will resume from the reset handler after the SE upgrade is complete.
- Parameters
-
[in] upgradeAddressThe starting address of the upgrade image.
- Returns
- False if the SE upgrade process didn't start.