Communication
Description
Host communication interface.
The Communication plugin provides an interface for implementing communication with a host device, such as a computer or a microcontroller.
Communication Protocol Implementations
Several plugins implement the communication interface, using different transports and protocols.
BGAPI UART DFU
EZSP-SPI
ezsp-spi-bootloader
that was previously released with the EmberZnet and SL-Thread wireless stacks.
UART XMODEM
serial-uart-bootloader
that was previously released with the EmberZnet and SL-Thread wireless stacks.
Modules |
|
| Utils | |
Functions |
|
| void | communication_init (void) |
| int32_t | communication_start (void) |
| int32_t | communication_main (void) |
| void | communication_shutdown (void) |
Function Documentation
| void communication_init | ( | void |
|
) |
Initialize hardware for the communication plugin.
| int32_t communication_start | ( | void |
|
) |
Initialize communication between the bootloader and external host. E.g. indicate to the external host that we're alive and kicking.
- Returns
- Error code indicating success or failure
- Return values
-
BOOTLOADER_OKon success BOOTLOADER_ERROR_COMMUNICATION_STARTon failure
| int32_t communication_main | ( | void |
|
) |
This function is not supposed to return until the host signals the end of the current session, or a new image has been flashed and verified.
- Returns
- Error code indicating sucess or failure
- Return values
-
BOOTLOADER_OKwhen a new image was flashed BOOTLOADER_ERROR_COMMUNICATION_ERRORon communication error BOOTLOADER_ERROR_COMMUNICATION_DONEwhen no image was received BOOTLOADER_ERROR_COMMUNICATION_IMAGE_ERRORwhen received image is invalid
| void communication_shutdown | ( | void |
|
) |
Stop communication between the bootloader and external host.