Image parser plugin.
Generic image parser interface for Silicon Labs bootloader.
|
|
|
int32_t
|
parser_init
(void *context, void *decryptContext, void *authContext, uint8_t flags)
|
|
|
|
int32_t
|
parser_parse
(void *context,
ImageProperties_t
*imageProperties, uint8_t buffer[], size_t length, const
BootloaderParserCallbacks_t
*callbacks)
|
|
|
|
bool
|
parser_requireAuthenticity
(void)
|
|
|
|
bool
|
parser_requireConfidentiality
(void)
|
|
|
|
bool
|
parser_requireCertificateAuthenticity
(void)
|
|
|
|
bool
|
parser_requireCertificateSignedImage
(void)
|
|
|
|
bool
|
parser_requireAntiRollbackProtection
(void)
|
|
|
|
uint32_t
|
parser_applicationMinimumVersionValid
(void)
|
|
|
|
bool
|
parser_applicationUpgradeVersionValid
(
ApplicationData_t
*app, bool checkRemainingAppUpgrades)
|
|
|
|
uint32_t
|
parser_getApplicationAddress
(void)
|
|
|
|
uint32_t
|
parser_getFirstStageBootloaderTable
(void)
|
|
|
|
uint32_t
|
parser_getMainBootloaderTable
(void)
|
|
|
|
uint32_t
|
parser_getBootloaderUpgradeAddress
(void)
|
|
|
|
bool
|
parser_applicationUpgradeValidCallback
(
ApplicationData_t
*app)
|
|
|
|
int32_t
|
parser_verifyCertificate
(void *context, void *input, void *blProperties, void *shaState)
|
|
|
|
int32_t parser_init
|
(
|
void *
|
context,
|
|
|
|
void *
|
decryptContext,
|
|
|
|
void *
|
authContext,
|
|
|
|
uint8_t
|
flags
|
|
|
)
|
|
|
Initialize the parser's context.
-
Parameters
-
context
|
Pointer to context for the parser implementation
|
decryptContext
|
Pointer to context for decryption of parsed file
|
authContext
|
Pointer to context for authentication of parsed file
|
flags
|
Flags for parser support
|
-
Returns
-
BOOTLOADER_OK
if OK, error code otherwise.
Parse an image file to extract the binary and some metadata.
Pushes data into the image file parser to be parsed.
-
Parameters
-
context
|
Pointer to the specific parser's context variable
|
imageProperties
|
Pointer to the image file state variable
|
buffer
|
Pointer to byte array containing data to parse
|
length
|
Size in bytes of the data in buffer
|
callbacks
|
Struct containing function pointers to be called by the parser to pass the extracted binary data back to BTL.
|
-
Returns
-
BOOTLOADER_OK
if OK, error code otherwise.
|
bool parser_requireAuthenticity
|
(
|
void
|
|
)
|
|
Check whether the parser requires images to be signed.
-
Returns
-
True if authenticity is required, else false
|
bool parser_requireConfidentiality
|
(
|
void
|
|
)
|
|
Check whether the parser requires images to be encrypted.
-
Returns
-
True if confidentiality is required, else false
|
bool parser_requireCertificateAuthenticity
|
(
|
void
|
|
)
|
|
Check whether the parser requires images to be authenticated by the bootloader certificate.
-
Returns
-
True if certificate based authenticity is required, else false
|
bool parser_requireCertificateSignedImage
|
(
|
void
|
|
)
|
|
Check whether the parser requires images to be signed by a certificate.
-
Returns
-
True if certificate signed image is required, else false
|
bool parser_requireAntiRollbackProtection
|
(
|
void
|
|
)
|
|
Check whether the parser requires rollback protection of applications.
-
Returns
-
True if rollback protection of application is required, else false
|
uint32_t parser_applicationMinimumVersionValid
|
(
|
void
|
|
)
|
|
Check the minimum version of the applications that can be accepted.
-
Returns
-
Minimum version of the applications that can be accepted.
|
bool parser_applicationUpgradeVersionValid
|
(
|
ApplicationData_t
*
|
app,
|
|
|
|
bool
|
checkRemainingAppUpgrades
|
|
|
)
|
|
|
Check whether the application version is valid and the application can be accepted.
-
Note
-
This function will always return true if BOOTLOADER_ROLLBACK_PROTECTION is not enabled from the core plugin option.
-
Parameters
-
|
[in]
|
app
|
Pointer to the application data structure contained in the upgrade image.
|
|
[in]
|
checkRemainingAppUpgrades
|
Check remaining application upgrades.
|
-
Returns
-
True if the application version is higher or equal than the application versions seen. False if the application version is lower than the application versions seen. False if no remaining application upgrades are left when
checkRemainingAppUpgrades
is true.
|
uint32_t parser_getApplicationAddress
|
(
|
void
|
|
)
|
|
Return the start address of the application.
-
Returns
-
start address of the application.
|
uint32_t parser_getFirstStageBootloaderTable
|
(
|
void
|
|
)
|
|
Return the address of the first stage bootloader table.
-
Returns
-
address of the first stage bootloader table.
|
uint32_t parser_getMainBootloaderTable
|
(
|
void
|
|
)
|
|
Return the address of the main bootloader table.
-
Returns
-
address of the main bootloader table.
|
uint32_t parser_getBootloaderUpgradeAddress
|
(
|
void
|
|
)
|
|
Return the start address of the bootloader upgrade location.
-
Returns
-
start address of the bootloader upgrade location if upgrading is supported, otherwise 0.
Callback to tell the parser whether to accept the application upgrade present in the upgrade image.
-
Parameters
-
|
[in]
|
app
|
Pointer to the application data structure contained in the upgrade image.
|
-
Returns
-
True if the application is accepted, and the parser should continue. False if the application is rejected. If rejected, the parser will abort parsing the image file and return
BOOTLOADER_ERROR_PARSER_REJECTED
.
|
int32_t parser_verifyCertificate
|
(
|
void *
|
context,
|
|
|
|
void *
|
input,
|
|
|
|
void *
|
blProperties,
|
|
|
|
void *
|
shaState
|
|
|
)
|
|
|