Description

ECDSA signing functionality for the bootloader.

Modules

ECC Library
Elliptic Curve Cryptography Library.

Macros

#define BTL_SECURITY_ECDSA_SHA256_LENGTH 32
Number of bytes of data to verify the signature against.
#define BTL_SECURITY_ECDSA_POINT_LENGTH 32
Number of bytes in the EC points that the signature consists of.

Functions

int32_t btl_verifyEcdsaP256r1 (const uint8_t *sha256, const uint8_t *signatureR, const uint8_t *signatureS, const uint8_t *keyX, const uint8_t *keyY)

Function Documentation

int32_t btl_verifyEcdsaP256r1 ( const uint8_t * sha256,
const uint8_t * signatureR,
const uint8_t * signatureS,
const uint8_t * keyX,
const uint8_t * keyY
)

Verify an ECDSA signature of a SHA256-hash using secp256r1.

Verifies the authenticity of data by checking the ECDSA signature of the data's SHA256-hash. This function is only for use with the secp256r1 curve. The public key which the signature is validated against will be retrieved from the respective tokens in the lockbits-page.

Parameters
sha256 The hash of the data which is authenticated
signatureR Byte array (MSB first) of R-point of the ECDSA signature
signatureS Byte array (MSB first) of S-point of the ECDSA signature
keyX Pointer to the X coordinate of the ECDSA public key
keyY Pointer to the Y coordinate of the ECDSA public key
Returns
BOOTLOADER_OK if signature is valid, else error code in BOOTLOADER_ERROR_SECURITY_BASE range.