ParserContext_t Struct Reference
Description
Image parser context definition.
Definition at line
101
of file
btl_ebl_parser.h
.
#include <
btl_ebl_parser.h
>
Data Fields |
|
| uint8_t | internalBuffer [64] |
|
Buffer contents.
|
|
| uint8_t | bytesInInternalBuffer |
|
Amount of bytes present in buffer.
|
|
| uint8_t | internalBufferOffset |
|
Current reading offset into the buffer (circular)
|
|
| uint8_t | flags |
|
Parser flags.
|
|
| bool | inEncryptedContainer |
|
Parser is currently inside an encrypted tag.
|
|
| bool | gotSignature |
|
Parser has received and verified signature.
|
|
| uint8_t | receivedFlags |
|
Parser has received bootloader upgrade tag.
|
|
| EblParserState_t | internalState |
|
State of the EBL parser state machine.
|
|
| void * | aesContext |
|
AES-CCM decryption (= AES-CTR) context.
|
|
| void * | shaContext |
|
SHA256 hashing context.
|
|
| size_t | lengthOfTag |
|
Total length of the tag currently being parsed.
|
|
| size_t | offsetInTag |
|
Current offset into tag being parsed.
|
|
| size_t | lengthOfEncryptedTag |
|
Total length of current encrypted data block.
|
|
| size_t | offsetInEncryptedTag |
|
Offset into current encrypted data block.
|
|
| uint32_t | programmingAddress |
|
Current address the image needs to be written to.
|
|
| uint32_t | tagAddress |
|
Current offset of metadata/bootloader being handled (starts at 0)
|
|
| uint8_t | withheldApplicationVectors [24] |
|
Withheld application data.
|
|
| uint8_t | withheldUpgradeVectors [4] |
|
Withheld bootloader upgrade data during app parsing.
|
|
| uint8_t | withheldBootloaderVectors [4] |
|
Withheld bootloader upgrade data during bootloader parsing.
|
|
| uint32_t | fileCrc |
|
Running CRC-32 over the incoming EBL file.
|
|
| uint32_t | customTagId |
|
Context for custom tag.
|
|
The documentation for this struct was generated from the following file:
-
btl_ebl_parser.h