ImageProperties_t Struct Reference
Description
Structure containing state of the image file processed.
Definition at line
41
of file
btl_image_parser.h
.
#include <
btl_image_parser.h
>
Data Fields |
|
| uint8_t | contents |
|
Image contents.
|
|
| uint8_t | instructions |
|
Parser instructions.
|
|
| bool | imageCompleted |
|
Flag to indicate parsing has completed.
|
|
| bool | imageVerified |
|
Flag to indicate the image file has been validated.
|
|
| uint32_t | bootloaderVersion |
|
Version number of main bootloader extracted from image file.
|
|
| ApplicationData_t | application |
|
Information about the application.
|
|
| uint32_t | bootloaderUpgradeSize |
|
Size of the bootloader upgrade contained in the image file.
|
|
| uint32_t | seUpgradeVersion |
|
Version number of SE upgrade extracted from image file.
|
|
The documentation for this struct was generated from the following file:
-
btl_image_parser.h