XMODEM Parser
Description
Parser for XMODEM packets.
XMODEM packet parser supporting XMODEM-CRC.
Modules |
|
| Commands | |
Data Structures |
|
| struct | XmodemPacket_t |
|
XMODEM packet.
|
|
Macros |
|
| #define | XMODEM_DATA_SIZE 128 |
|
Size of an XMODEM packet.
|
|
Functions |
|
| void | xmodem_reset (void) |
| int32_t | xmodem_parsePacket ( XmodemPacket_t *packet, uint8_t *response) |
| uint8_t | xmodem_getLastPacketNumber (void) |
Function Documentation
| void xmodem_reset | ( | void |
|
) |
Reset the XMODEM parser to start a new transfer
| int32_t xmodem_parsePacket | ( | XmodemPacket_t * |
packet,
|
| uint8_t * |
response
|
||
| ) |
Parse an XMODEM packet.
- Parameters
-
[in] packetThe XMODEM packet to parse. [out] responseThe XMODEM response to the parsed frame
- Returns
- BOOTLOADER_OK on success, else error code
| uint8_t xmodem_getLastPacketNumber | ( | void |
|
) |
Return the packet number of the last packet that was successfully parsed.
- Returns
- Last packet number received. Defaults to 0 if nothing has been received yet.