Description
Elliptic Curve Cryptography Library.
The ECC (Elliptic Curve Cryptography) API includes ECDSA verification on one of the elliptic curves recommended by NIST in csrc.nist.gov/groups/ST/toolkit/documents/dss/NISTReCur.pdf :
- secp256r1: NIST/SECG X9.62 curve over a 256 bit prime field
Data Structures |
|
| struct | ECC_Point_t |
| struct | ECC_EcdsaSignature_t |
Macros |
|
| #define | ECC_BIGINT_SIZE_IN_BITS (256) |
| #define | ECC_BIGINT_SIZE_IN_BYTES ( ECC_BIGINT_SIZE_IN_BITS / 8) |
| #define | ECC_BIGINT_SIZE_IN_32BIT_WORDS |
Typedefs |
|
| typedef uint32_t | ECC_BigInt_t [ ECC_BIGINT_SIZE_IN_32BIT_WORDS ] |
Functions |
|
| int32_t | ECC_ECDSA_VerifySignatureP256 (CRYPTO_TypeDef *crypto, const uint8_t *msgDigest, int msgDigestLen, const ECC_Point_t *publicKey, ECC_EcdsaSignature_t *signature) |
|
Verify an ECDSA signature.
|
|
| void | ECC_HexToBigInt ( ECC_BigInt_t bigint, const char *hex) |
|
Convert a large integer from a hexadecimal string to the ECC_BigInt_t format.
|
|
| void | ECC_BigIntToHex (char *hex, ECC_BigInt_t bigint) |
|
Convert a large integer from the ECC_BigInt_t to a hexadecimal string format.
|
|
| void | ECC_ByteArrayToBigInt ( ECC_BigInt_t bigint, const uint8_t *bytearray) |
|
Convert a big integer from a byte array to the ECC_BigInt_t format.
|
|
| void | ECC_BigIntToByteArray (uint8_t *bytearray, ECC_BigInt_t bigint) |
|
Convert a large integer from the ECC_BigInt_t to the byte array format.
|
|
| void | ECC_UnsignedIntToBigInt ( ECC_BigInt_t bigint, const uint32_t value) |
|
Convert an integer from uint32_t to ECC_BigInt_t format.
|
|
Macro Definition Documentation
| #define ECC_BIGINT_SIZE_IN_BITS (256) |
ECC big integer size in bits.
Definition at line
49
of file
ecc.h
.
| #define ECC_BIGINT_SIZE_IN_BYTES ( ECC_BIGINT_SIZE_IN_BITS / 8) |
ECC big integer size in bytes.
Definition at line
52
of file
ecc.h
.
| #define ECC_BIGINT_SIZE_IN_32BIT_WORDS |
ECC big integer size in words.
Definition at line
55
of file
ecc.h
.
Typedef Documentation
| typedef uint32_t ECC_BigInt_t[ ECC_BIGINT_SIZE_IN_32BIT_WORDS ] |
ECC big integer type
Definition at line
59
of file
ecc.h
.
Function Documentation
| int32_t ECC_ECDSA_VerifySignatureP256 | ( | CRYPTO_TypeDef * |
crypto,
|
| const uint8_t * |
msgDigest,
|
||
| int |
msgDigestLen,
|
||
| const ECC_Point_t * |
publicKey,
|
||
| ECC_EcdsaSignature_t * |
signature
|
||
| ) |
Verify an ECDSA signature.
TBW
- Parameters
-
[in] cryptoPointer to CRYPTO peripheral instance [in] msgDigestThe message digest associated with the signature. [in] msgDigestLenThe length of the message digest. [in] publicKeyPublic key of entity that generated signature. [out] signatureThe signature to verify.
- Returns
- Error code.
| void ECC_HexToBigInt | ( | ECC_BigInt_t |
bigint,
|
| const char * |
hex
|
||
| ) |
Convert a large integer from a hexadecimal string to the ECC_BigInt_t format.
Convert a large integer from a hexadecimal string representation to a ECC_BigInt_t representation.
- Parameters
-
[out] bigintPointer to the location where to store the result. [in] hexThe hex representation of the large integer to convert.
| void ECC_BigIntToHex | ( | char * |
hex,
|
| ECC_BigInt_t |
bigint
|
||
| ) |
Convert a large integer from the ECC_BigInt_t to a hexadecimal string format.
Convert a large integer from a ECC_BigInt_t representation to a hexadecimal string representation.
- Parameters
-
[out] hexBuffer where to store the hexadecimal result. [in] bigintThe ECC_BigInt_t representation of the large integer to convert.
| void ECC_ByteArrayToBigInt | ( | ECC_BigInt_t |
bigint,
|
| const uint8_t * |
bytearray
|
||
| ) |
Convert a big integer from a byte array to the ECC_BigInt_t format.
Convert a large integer from a byte array representation to a ECC_BigInt_t representation.
- Parameters
-
[out] bigintPointer to the location where to store the result. [in] bytearrayThe byte array representation of the large integer to convert.
| void ECC_BigIntToByteArray | ( | uint8_t * |
bytearray,
|
| ECC_BigInt_t |
bigint
|
||
| ) |
Convert a large integer from the ECC_BigInt_t to the byte array format.
Convert a large integer from a ECC_BigInt_t representation to a byte array representation. Caution: byte array must be big enough to contain the result.
- Parameters
-
[out] bytearrayBuffer to store the resulting byte array. [in] bigintThe ECC_BigInt_t representation of the large integer to convert.
| void ECC_UnsignedIntToBigInt | ( | ECC_BigInt_t |
bigint,
|
| const uint32_t |
value
|
||
| ) |
Convert an integer from uint32_t to ECC_BigInt_t format.
Convert a integer from an uint32_t representation to a ECC_BigInt_t representation.
- Parameters
-
[out] bigintPointer to the location to store the result. [in] valueThe value to convert.