spidrv.h File Reference

SPIDRV API definition.

Version
5.4.0

License

(C) Copyright 2014 Silicon Labs, www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file spidrv.h.

#include "em_device.h"
#include "em_cmu.h"
#include "ecode.h"
#include "spidrv_config.h"
#include "rtcdriver.h"
#include "dmadrv.h"

Data Structures

struct  SPIDRV_HandleData
 
struct  SPIDRV_Init
 

Macros

#define ECODE_EMDRV_SPIDRV_ABORTED   (ECODE_EMDRV_SPIDRV_BASE | 0x00000007)
 An SPI transfer has been aborted.
 
#define ECODE_EMDRV_SPIDRV_BUSY   (ECODE_EMDRV_SPIDRV_BASE | 0x00000003)
 The SPI port is busy.
 
#define ECODE_EMDRV_SPIDRV_DMA_ALLOC_ERROR   (ECODE_EMDRV_SPIDRV_BASE | 0x00000009)
 Unable to allocate DMA channels.
 
#define ECODE_EMDRV_SPIDRV_IDLE   (ECODE_EMDRV_SPIDRV_BASE | 0x00000006)
 No SPI transfer in progress.
 
#define ECODE_EMDRV_SPIDRV_ILLEGAL_HANDLE   (ECODE_EMDRV_SPIDRV_BASE | 0x00000001)
 An illegal SPI handle.
 
#define ECODE_EMDRV_SPIDRV_MODE_ERROR   (ECODE_EMDRV_SPIDRV_BASE | 0x00000008)
 SPI master used slave API or vica versa.
 
#define ECODE_EMDRV_SPIDRV_OK   (ECODE_OK)
 A successful return value.
 
#define ECODE_EMDRV_SPIDRV_PARAM_ERROR   (ECODE_EMDRV_SPIDRV_BASE | 0x00000002)
 An illegal input parameter.
 
#define ECODE_EMDRV_SPIDRV_TIMEOUT   (ECODE_EMDRV_SPIDRV_BASE | 0x00000005)
 An SPI transfer timeout.
 
#define ECODE_EMDRV_SPIDRV_TIMER_ALLOC_ERROR   (ECODE_EMDRV_SPIDRV_BASE | 0x00000004)
 Unable to allocate timeout timer.
 
#define SPIDRV_MASTER_USART0
 Configuration data for SPI master using USART0.
 
#define SPIDRV_MASTER_USART1
 Configuration data for SPI master using USART1.
 
#define SPIDRV_MASTER_USART2
 Configuration data for SPI master using USART2.
 
#define SPIDRV_MASTER_USART3
 Configuration data for SPI master using USART3.
 
#define SPIDRV_SLAVE_USART0
 Configuration data for SPI slave using USART0.
 
#define SPIDRV_SLAVE_USART1
 Configuration data for SPI slave using USART1.
 
#define SPIDRV_SLAVE_USART2
 Configuration data for SPI slave using USART2.
 
#define SPIDRV_SLAVE_USART3
 Configuration data for SPI slave using USART3.
 

Typedefs

typedef enum SPIDRV_BitOrder SPIDRV_BitOrder_t
 SPI bus bit order.
 
typedef void(* SPIDRV_Callback_t) (struct SPIDRV_HandleData *handle, Ecode_t transferStatus, int itemsTransferred)
 SPIDRV transfer completion callback function.
 
typedef enum SPIDRV_ClockMode SPIDRV_ClockMode_t
 SPI clock mode (clock polarity and phase).
 
typedef enum SPIDRV_CsControl SPIDRV_CsControl_t
 SPI master chip select (CS) control scheme.
 
typedef SPIDRV_HandleData_tSPIDRV_Handle_t
 An SPI driver instance handle.
 
typedef struct SPIDRV_HandleData SPIDRV_HandleData_t
 
typedef struct SPIDRV_Init SPIDRV_Init_t
 
typedef enum SPIDRV_SlaveStart SPIDRV_SlaveStart_t
 SPI slave transfer start scheme.
 
typedef enum SPIDRV_Type SPIDRV_Type_t
 SPI driver instance type.
 

Enumerations

enum  SPIDRV_BitOrder {
  spidrvBitOrderLsbFirst = 0,
  spidrvBitOrderMsbFirst = 1
}
 SPI bus bit order.
 
enum  SPIDRV_ClockMode {
  spidrvClockMode0 = 0,
  spidrvClockMode1 = 1,
  spidrvClockMode2 = 2,
  spidrvClockMode3 = 3
}
 SPI clock mode (clock polarity and phase).
 
enum  SPIDRV_CsControl {
  spidrvCsControlAuto = 0,
  spidrvCsControlApplication = 1
}
 SPI master chip select (CS) control scheme.
 
enum  SPIDRV_SlaveStart {
  spidrvSlaveStartImmediate = 0,
  spidrvSlaveStartDelayed = 1
}
 SPI slave transfer start scheme.
 
enum  SPIDRV_Type {
  spidrvMaster = 0,
  spidrvSlave = 1
}
 SPI driver instance type.
 

Functions

Ecode_t SPIDRV_AbortTransfer (SPIDRV_Handle_t handle)
 Abort an ongoing SPI transfer.
 
Ecode_t SPIDRV_DeInit (SPIDRV_Handle_t handle)
 Deinitialize an SPI driver instance.
 
Ecode_t SPIDRV_GetBitrate (SPIDRV_Handle_t handle, uint32_t *bitRate)
 Get current SPI bus bitrate.
 
Ecode_t SPIDRV_GetFramelength (SPIDRV_Handle_t handle, uint32_t *frameLength)
 Get current SPI framelength.
 
Ecode_t SPIDRV_GetTransferStatus (SPIDRV_Handle_t handle, int *itemsTransferred, int *itemsRemaining)
 Get the status of an SPI transfer.
 
Ecode_t SPIDRV_Init (SPIDRV_Handle_t handle, SPIDRV_Init_t *initData)
 Initialize an SPI driver instance.
 
Ecode_t SPIDRV_MReceive (SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback)
 Start an SPI master receive transfer.
 
Ecode_t SPIDRV_MReceiveB (SPIDRV_Handle_t handle, void *buffer, int count)
 Start an SPI master blocking receive transfer.
 
Ecode_t SPIDRV_MTransfer (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count, SPIDRV_Callback_t callback)
 Start an SPI master transfer.
 
Ecode_t SPIDRV_MTransferB (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count)
 Start an SPI master blocking transfer.
 
Ecode_t SPIDRV_MTransferSingleItemB (SPIDRV_Handle_t handle, uint32_t txValue, void *rxValue)
 Start an SPI master blocking single item (frame) transfer.
 
Ecode_t SPIDRV_MTransmit (SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback)
 Start an SPI master transmit transfer.
 
Ecode_t SPIDRV_MTransmitB (SPIDRV_Handle_t handle, const void *buffer, int count)
 Start an SPI master blocking transmit transfer.
 
Ecode_t SPIDRV_SetBitrate (SPIDRV_Handle_t handle, uint32_t bitRate)
 Set SPI bus bitrate.
 
Ecode_t SPIDRV_SetFramelength (SPIDRV_Handle_t handle, uint32_t frameLength)
 Set SPI framelength.
 
Ecode_t SPIDRV_SReceive (SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs)
 Start an SPI slave receive transfer.
 
Ecode_t SPIDRV_SReceiveB (SPIDRV_Handle_t handle, void *buffer, int count, int timeoutMs)
 Start an SPI slave blocking receive transfer.
 
Ecode_t SPIDRV_STransfer (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count, SPIDRV_Callback_t callback, int timeoutMs)
 Start an SPI slave transfer.
 
Ecode_t SPIDRV_STransferB (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count, int timeoutMs)
 Start an SPI slave blocking transfer.
 
Ecode_t SPIDRV_STransmit (SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs)
 Start an SPI slave transmit transfer.
 
Ecode_t SPIDRV_STransmitB (SPIDRV_Handle_t handle, const void *buffer, int count, int timeoutMs)
 Start an SPI slave blocking transmit transfer.