LDMA_TransferCfg_t Struct ReferenceEMLIB > LDMA
DMA transfer configuration structure.
This struct configures all aspects of a DMA transfer.
Definition at line 709
of file em_ldma.h
.
#include <
em_ldma.h
>
Data Fields | |
uint8_t | ldmaCfgArbSlots |
uint8_t | ldmaCfgDstIncSign |
uint8_t | ldmaCfgSrcIncSign |
uint8_t | ldmaCtrlSyncPrsClrOff |
uint8_t | ldmaCtrlSyncPrsClrOn |
uint8_t | ldmaCtrlSyncPrsSetOff |
uint8_t | ldmaCtrlSyncPrsSetOn |
bool | ldmaDbgHalt |
uint8_t | ldmaLoopCnt |
bool | ldmaReqDis |
uint32_t | ldmaReqSel |
Field Documentation
uint8_t LDMA_TransferCfg_t::ldmaCfgArbSlots |
Arbitration slot number.
Definition at line 717
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
uint8_t LDMA_TransferCfg_t::ldmaCfgDstIncSign |
Dest. addr. increment sign.
Definition at line 719
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
uint8_t LDMA_TransferCfg_t::ldmaCfgSrcIncSign |
Source addr. increment sign.
Definition at line 718
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
uint8_t LDMA_TransferCfg_t::ldmaCtrlSyncPrsClrOff |
PRS Synctrig clear enables to clear.
Definition at line 711
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
uint8_t LDMA_TransferCfg_t::ldmaCtrlSyncPrsClrOn |
PRS Synctrig clear enables to set.
Definition at line 712
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
uint8_t LDMA_TransferCfg_t::ldmaCtrlSyncPrsSetOff |
PRS Synctrig set enables to clear.
Definition at line 713
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
uint8_t LDMA_TransferCfg_t::ldmaCtrlSyncPrsSetOn |
PRS Synctrig set enables to set.
Definition at line 714
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
bool LDMA_TransferCfg_t::ldmaDbgHalt |
Dis. DMA trig when cpu is halted.
Definition at line 716
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
uint8_t LDMA_TransferCfg_t::ldmaLoopCnt |
Counter for looped transfers.
Definition at line 720
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
bool LDMA_TransferCfg_t::ldmaReqDis |
Mask the PRS trigger input.
Definition at line 715
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
uint32_t LDMA_TransferCfg_t::ldmaReqSel |
Selects DMA trigger source.
Definition at line 710
of file em_ldma.h
.
Referenced by LDMA_StartTransfer().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_ldma.h