IDAC_TypeDef Struct ReferenceDevices > IDAC

IDAC Register Declaration

Definition at line 49 of file efm32jg12b_idac.h .

#include < efm32jg12b_idac.h >

Data Fields

__IM uint32_t APORTCONFLICT
__IM uint32_t APORTREQ
__IOM uint32_t CTRL
__IOM uint32_t CURPROG
__IOM uint32_t DUTYCONFIG
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
uint32_t RESERVED0 [1]
uint32_t RESERVED1 [2]
uint32_t RESERVED2 [1]
uint32_t RESERVED3 [1]
__IM uint32_t STATUS

Field Documentation

__IM uint32_t IDAC_TypeDef::APORTCONFLICT

APORT Request Status Register

Definition at line 64 of file efm32jg12b_idac.h .

__IM uint32_t IDAC_TypeDef::APORTREQ

APORT Request Status Register

Definition at line 63 of file efm32jg12b_idac.h .

__IOM uint32_t IDAC_TypeDef::CTRL

Control Register

Definition at line 50 of file efm32jg12b_idac.h .

Referenced by IDAC_Enable() , IDAC_Init() , IDAC_MinimalOutputTransitionMode() , IDAC_OutEnable() , IDAC_RangeSet() , and IDAC_Reset() .

__IOM uint32_t IDAC_TypeDef::CURPROG

Current Programming Register

Definition at line 51 of file efm32jg12b_idac.h .

Referenced by IDAC_RangeSet() , IDAC_Reset() , and IDAC_StepSet() .

__IOM uint32_t IDAC_TypeDef::DUTYCONFIG

Duty Cycle Configuration Register

Definition at line 53 of file efm32jg12b_idac.h .

Referenced by IDAC_Reset() .

__IOM uint32_t IDAC_TypeDef::IEN

Interrupt Enable Register

Definition at line 61 of file efm32jg12b_idac.h .

Referenced by IDAC_IntDisable() , IDAC_IntEnable() , and IDAC_IntGetEnabled() .

__IM uint32_t IDAC_TypeDef::IF

Interrupt Flag Register

Definition at line 58 of file efm32jg12b_idac.h .

Referenced by IDAC_IntGet() , and IDAC_IntGetEnabled() .

__IOM uint32_t IDAC_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 60 of file efm32jg12b_idac.h .

Referenced by IDAC_IntClear() .

__IOM uint32_t IDAC_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 59 of file efm32jg12b_idac.h .

Referenced by IDAC_IntSet() .

uint32_t IDAC_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 52 of file efm32jg12b_idac.h .

uint32_t IDAC_TypeDef::RESERVED1[2]

Reserved for future use

Definition at line 55 of file efm32jg12b_idac.h .

uint32_t IDAC_TypeDef::RESERVED2[1]

Reserved for future use

Definition at line 57 of file efm32jg12b_idac.h .

uint32_t IDAC_TypeDef::RESERVED3[1]

Reserved for future use

Definition at line 62 of file efm32jg12b_idac.h .

__IM uint32_t IDAC_TypeDef::STATUS

Status Register

Definition at line 56 of file efm32jg12b_idac.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG12B/Include/ efm32jg12b_idac.h