SensorStruct_t Struct ReferencePlatform Middleware > Capacitive Sensing Firmware Library
Stores all runtime values for an enabled capacitive sensor.
Definition at line 61
of file cslib.h
.
#include <
cslib.h
>
Data Fields | |
uint8_t | activeIndicator |
Bit array showing whether touch is qualified on sensor, uses DEBOUNCE_ACTIVE_MASK. | |
signed char | baselineAccumulator |
Tracks trend of CS values to determine whether baseline rises or falls. | |
uint32_t | currentBaseline |
Runtime estimate of untouched or inactive state of CS sensor input. | |
uint8_t | debounceCounts |
Stores consecutive CS values above or below active or inactive threshold. | |
SI_UU32_t | expValue |
Filtered CS value with 16 bits of LSBs. | |
uint32_t | rawBuffer [DEF_SENSOR_BUFFER_SIZE] |
Newest sample taken from CS hardware, without any processing. | |
uint8_t | touchDeltaDiv16 |
Describes the expected difference between untouched and touched CS value. | |
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/middleware/cslib/inc/
cslib.h