SMU_TypeDef Struct ReferenceDevices > SMU
SMU Register Declaration
Definition at line 49
of file efm32jg12b_smu.h
.
#include <
efm32jg12b_smu.h
>
Data Fields | |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | PPUCTRL |
__IM uint32_t | PPUFS |
__IOM uint32_t | PPUPATD0 |
__IOM uint32_t | PPUPATD1 |
uint32_t | RESERVED0 [3] |
uint32_t | RESERVED1 [9] |
uint32_t | RESERVED2 [3] |
uint32_t | RESERVED3 [14] |
Field Documentation
__IOM uint32_t SMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line 54
of file efm32jg12b_smu.h
.
__IM uint32_t SMU_TypeDef::IF |
Interrupt Flag Register
Definition at line 51
of file efm32jg12b_smu.h
.
__IOM uint32_t SMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 53
of file efm32jg12b_smu.h
.
__IOM uint32_t SMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 52
of file efm32jg12b_smu.h
.
__IOM uint32_t SMU_TypeDef::PPUCTRL |
PPU Control Register
Definition at line 57
of file efm32jg12b_smu.h
.
__IM uint32_t SMU_TypeDef::PPUFS |
PPU Fault Status
Definition at line 63
of file efm32jg12b_smu.h
.
__IOM uint32_t SMU_TypeDef::PPUPATD0 |
PPU Privilege Access Type Descriptor 0
Definition at line 59
of file efm32jg12b_smu.h
.
__IOM uint32_t SMU_TypeDef::PPUPATD1 |
PPU Privilege Access Type Descriptor 1
Definition at line 60
of file efm32jg12b_smu.h
.
uint32_t SMU_TypeDef::RESERVED0[3] |
Reserved for future use
Definition at line 50
of file efm32jg12b_smu.h
.
uint32_t SMU_TypeDef::RESERVED1[9] |
Reserved for future use
Definition at line 56
of file efm32jg12b_smu.h
.
uint32_t SMU_TypeDef::RESERVED2[3] |
Reserved for future use
Definition at line 58
of file efm32jg12b_smu.h
.
uint32_t SMU_TypeDef::RESERVED3[14] |
Reserved for future use
Definition at line 62
of file efm32jg12b_smu.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG12B/Include/
efm32jg12b_smu.h