CapSenseKit Drivers
Functions |
|
uint32_t | CAPLESENSE_getNormalizedVal (uint8_t channel) |
Get the current normalized channelValue for a channel.
|
|
uint8_t | CAPLESENSE_getSegmentChannel (uint8_t capSegment) |
Get the channelValue for a sensor segment.
|
|
int32_t | CAPLESENSE_getSliderPosition (void) |
Get the position of the slider.
|
|
uint32_t | CAPLESENSE_getVal (uint8_t channel) |
Get the current channelValue for a channel.
|
|
void | CAPLESENSE_Init (bool sleep) |
Initializes the capacative sense system without LESENSE.
|
|
void | CAPLESENSE_setupCallbacks (void(*scanCb)(void), void(*chCb)(void)) |
LESENSE callback setup.
|
|
void | CAPLESENSE_setupLESENSE (bool sleep) |
Setup the LESENSE for capavitive sensing.
|
|
void | CAPLESENSE_Sleep (void) |
Send the capacative sense system to sleep mode.
|
|
uint32_t | CAPSENSE_getNormalizedVal (uint8_t channel) |
Get the current normalized channelValue for a channel.
|
|
bool | CAPSENSE_getPressed (uint8_t channel) |
Get the state of the Gecko Button.
|
|
int32_t | CAPSENSE_getSliderPosition (void) |
Get the position of the slider.
|
|
uint32_t | CAPSENSE_getVal (uint8_t channel) |
Get the current channelValue for a channel.
|
|
void | CAPSENSE_Init (void) |
Initializes the capacitive sense system.
|
|
void | CAPSENSE_Sense (void) |
This function iterates through all the capsensors and reads and initiates a reading. Uses EM1 while waiting for the result from each sensor.
|
|
Function Documentation
uint32_t CAPLESENSE_getNormalizedVal | ( | uint8_t |
channel
|
) |
Get the current normalized channelValue for a channel.
- Parameters
-
channel
The channel.
- Returns
- The channel value in range (0-256).
Definition at line
425
of file
caplesense.c
.
References channelMaxValues , and channelValues .
uint8_t CAPLESENSE_getSegmentChannel | ( | uint8_t |
capSegment
|
) |
Get the channelValue for a sensor segment.
- Parameters
-
capSegment
- Returns
- channel
Definition at line
389
of file
caplesense.c
.
int32_t CAPLESENSE_getSliderPosition | ( | void |
|
) |
Get the position of the slider.
- Returns
- The position of the slider if it can be determined, -1 otherwise.
Definition at line
436
of file
caplesense.c
.
References channelMaxValues , and channelValues .
uint32_t CAPLESENSE_getVal | ( | uint8_t |
channel
|
) |
Get the current channelValue for a channel.
- Parameters
-
channel
The channel.
- Returns
- The channelValue.
Definition at line
415
of file
caplesense.c
.
References channelValues .
void CAPLESENSE_Init | ( | bool |
sleep
|
) |
Initializes the capacative sense system without LESENSE.
- Parameters
-
sleep
If true, go into sleep mode.
Definition at line
501
of file
caplesense.c
.
References CAPLESENSE_setupACMP() , CAPLESENSE_setupCMU() , CAPLESENSE_setupGPIO() , CAPLESENSE_setupLESENSE() , CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , and CORE_EXIT_ATOMIC .
void CAPLESENSE_setupCallbacks | ( | void(*)(void) |
scanCb,
|
void(*)(void) |
chCb
|
||
) |
LESENSE callback setup.
- Parameters
-
scanCb
Scan callback chCb
Channel callback
Definition at line
330
of file
caplesense.c
.
References lesenseChCb , and lesenseScanCb .
void CAPLESENSE_setupLESENSE | ( | bool |
sleep
|
) |
Setup the LESENSE for capavitive sensing.
- Parameters
-
sleep
If true, go into sleep mode.
Definition at line
163
of file
caplesense.c
.
References channelsInUse .
Referenced by CAPLESENSE_Init() .
uint32_t CAPSENSE_getNormalizedVal | ( | uint8_t |
channel
|
) |
Get the current normalized channelValue for a channel.
- Parameters
-
channel
The channel.
- Returns
- The channel value in range (0-256).
Definition at line
132
of file
capsense.c
.
References channelMaxValues , and channelValues .
bool CAPSENSE_getPressed | ( | uint8_t |
channel
|
) |
Get the state of the Gecko Button.
- Parameters
-
channel
The channel.
- Returns
- true if the button is "pressed" false otherwise.
Definition at line
144
of file
capsense.c
.
References channelMaxValues , and channelValues .
int32_t CAPSENSE_getSliderPosition | ( | void |
|
) |
Get the position of the slider.
- Returns
- The position of the slider if it can be determined, -1 otherwise.
Definition at line
164
of file
capsense.c
.
References channelMaxValues , and channelValues .
uint32_t CAPSENSE_getVal | ( | uint8_t |
channel
|
) |
Get the current channelValue for a channel.
- Parameters
-
channel
The channel.
- Returns
- The channelValue.
Definition at line
122
of file
capsense.c
.
References channelValues .
void CAPSENSE_Init | ( | void |
|
) |
Initializes the capacitive sense system.
Capacitive sensing uses two timers: TIMER0 and TIMER1 as well as ACMP. ACMP is set up in cap-sense (oscillator mode). TIMER1 counts the number of pulses generated by ACMP_CAPSENSE. When TIMER0 expires it generates an interrupt. The number of pulses counted by TIMER1 is then stored in channelValues
Definition at line
284
of file
capsense.c
.
References ACMP_CAPSENSE_INIT_DEFAULT , ACMP_CapsenseInit() , CMU , CMU_ClockEnable() , cmuClock_HFPER , cmuClock_PRS , cmuClock_TIMER0 , cmuClock_TIMER1 , PRS , PRS_CH_CTRL_EDSEL_POSEDGE , TIMER0 , TIMER0_IRQn , TIMER1 , TIMER_CC_CTRL_ICEDGE_BOTH , TIMER_CC_CTRL_ICEVCTRL_RISING , TIMER_CC_CTRL_INSEL_PRS , TIMER_CC_CTRL_MODE_INPUTCAPTURE , TIMER_CC_CTRL_PRSSEL_PRSCH0 , TIMER_CTRL_CLKSEL_CC1 , TIMER_CTRL_PRESC_DIV1024 , TIMER_CTRL_PRESC_DIV512 , and TIMER_IEN_OF .