LEUART_Init_TypeDef Struct ReferenceEMLIB > LEUART
Initialization structure.
Definition at line 99
of file em_leuart.h
.
#include <
em_leuart.h
>
Data Fields | |
uint32_t | baudrate |
LEUART_Databits_TypeDef | databits |
LEUART_Enable_TypeDef | enable |
LEUART_Parity_TypeDef | parity |
uint32_t | refFreq |
LEUART_Stopbits_TypeDef | stopbits |
Field Documentation
uint32_t LEUART_Init_TypeDef::baudrate |
Desired baud rate.
Definition at line 110
of file em_leuart.h
.
Referenced by BSP_BccInit(), LEUART_Init(), RETARGET_SerialInit(), and UARTDRV_InitLeuart().
LEUART_Databits_TypeDef LEUART_Init_TypeDef::databits |
Number of data bits in frame.
Definition at line 113
of file em_leuart.h
.
Referenced by LEUART_Init(), and UARTDRV_InitLeuart().
LEUART_Enable_TypeDef LEUART_Init_TypeDef::enable |
Specifies whether TX and/or RX will be enabled when initialization completes.
Definition at line 101
of file em_leuart.h
.
Referenced by LEUART_Init(), RETARGET_SerialInit(), and UARTDRV_InitLeuart().
LEUART_Parity_TypeDef LEUART_Init_TypeDef::parity |
Parity mode to use.
Definition at line 116
of file em_leuart.h
.
Referenced by LEUART_Init(), and UARTDRV_InitLeuart().
uint32_t LEUART_Init_TypeDef::refFreq |
LEUART reference clock assumed when configuring baud rate setup. Set to 0 if using currently configured reference clock.
Definition at line 107
of file em_leuart.h
.
Referenced by LEUART_Init().
LEUART_Stopbits_TypeDef LEUART_Init_TypeDef::stopbits |
Number of stop bits to use.
Definition at line 119
of file em_leuart.h
.
Referenced by LEUART_Init(), and UARTDRV_InitLeuart().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_leuart.h