EBI_TypeDef Struct ReferenceDevices > EFM32G_EBI

Definition at line 48 of file efm32g_ebi.h .

Data Fields

__IOM uint32_t ADDRTIMING
__IOM uint32_t CTRL
__IOM uint32_t POLARITY
__IOM uint32_t RDTIMING
__IOM uint32_t ROUTE
__IOM uint32_t WRTIMING

Field Documentation

__IOM uint32_t EBI_TypeDef::ADDRTIMING

Address Timing Register

Definition at line 50 of file efm32g_ebi.h .

__IOM uint32_t EBI_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32g_ebi.h .

__IOM uint32_t EBI_TypeDef::POLARITY

Polarity Register

Definition at line 53 of file efm32g_ebi.h .

__IOM uint32_t EBI_TypeDef::RDTIMING

Read Timing Register

Definition at line 51 of file efm32g_ebi.h .

__IOM uint32_t EBI_TypeDef::ROUTE

I/O Routing Register

Definition at line 54 of file efm32g_ebi.h .

__IOM uint32_t EBI_TypeDef::WRTIMING

Write Timing Register

Definition at line 52 of file efm32g_ebi.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32G/Include/ efm32g_ebi.h