GPIO_P_TypeDef Struct ReferenceDevices
GPIO_P EFM32G GPIO P.
Definition at line
46
of file
efm32g_gpio_p.h
.
#include <
efm32g_gpio_p.h
>
Data Fields |
|
| __IOM uint32_t | CTRL |
| __IM uint32_t | DIN |
| __IOM uint32_t | DOUT |
| __OM uint32_t | DOUTCLR |
| __OM uint32_t | DOUTSET |
| __OM uint32_t | DOUTTGL |
| __IOM uint32_t | MODEH |
| __IOM uint32_t | MODEL |
| __IOM uint32_t | PINLOCKN |
Field Documentation
| __IOM uint32_t GPIO_P_TypeDef::CTRL |
Port Control Register
Definition at line
47
of file
efm32g_gpio_p.h
.
| __IM uint32_t GPIO_P_TypeDef::DIN |
Port Data In Register
Definition at line
54
of file
efm32g_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::DOUT |
Port Data Out Register
Definition at line
50
of file
efm32g_gpio_p.h
.
| __OM uint32_t GPIO_P_TypeDef::DOUTCLR |
Port Data Out Clear Register
Definition at line
52
of file
efm32g_gpio_p.h
.
| __OM uint32_t GPIO_P_TypeDef::DOUTSET |
Port Data Out Set Register
Definition at line
51
of file
efm32g_gpio_p.h
.
| __OM uint32_t GPIO_P_TypeDef::DOUTTGL |
Port Data Out Toggle Register
Definition at line
53
of file
efm32g_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::MODEH |
Port Pin Mode High Register
Definition at line
49
of file
efm32g_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::MODEL |
Port Pin Mode Low Register
Definition at line
48
of file
efm32g_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::PINLOCKN |
Port Unlocked Pins Register
Definition at line
55
of file
efm32g_gpio_p.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32G/Include/
efm32g_gpio_p.h