RTC_TypeDef Struct ReferenceDevices > EFM32G_RTC

Definition at line 48 of file efm32g_rtc.h .

Data Fields

__IM uint32_t CNT
__IOM uint32_t COMP0
__IOM uint32_t COMP1
__IOM uint32_t CTRL
__IOM uint32_t FREEZE
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IM uint32_t SYNCBUSY

Field Documentation

__IM uint32_t RTC_TypeDef::CNT

Counter Value Register

Definition at line 50 of file efm32g_rtc.h .

__IOM uint32_t RTC_TypeDef::COMP0

Compare Value Register 0

Definition at line 51 of file efm32g_rtc.h .

__IOM uint32_t RTC_TypeDef::COMP1

Compare Value Register 1

Definition at line 52 of file efm32g_rtc.h .

__IOM uint32_t RTC_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32g_rtc.h .

__IOM uint32_t RTC_TypeDef::FREEZE

Freeze Register

Definition at line 58 of file efm32g_rtc.h .

__IOM uint32_t RTC_TypeDef::IEN

Interrupt Enable Register

Definition at line 56 of file efm32g_rtc.h .

__IM uint32_t RTC_TypeDef::IF

Interrupt Flag Register

Definition at line 53 of file efm32g_rtc.h .

__IOM uint32_t RTC_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 55 of file efm32g_rtc.h .

__IOM uint32_t RTC_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 54 of file efm32g_rtc.h .

__IM uint32_t RTC_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 59 of file efm32g_rtc.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32G/Include/ efm32g_rtc.h