Utility FunctionsBSP > Thunderboard Sense BSP
Detailed Description
Utility functions.
Macros |
|
| #define | UTIL_SUPPLY_TYPE_AA 2 |
| #define | UTIL_SUPPLY_TYPE_AAA 3 |
| #define | UTIL_SUPPLY_TYPE_CR2032 4 |
| #define | UTIL_SUPPLY_TYPE_UNKNOWN 0 |
| #define | UTIL_SUPPLY_TYPE_USB 1 |
Functions |
|
| static void | adcDeInit (void) |
|
De-initializes the A/D converter.
|
|
| static void | adcInit (void) |
|
Initializes the A/D converter.
|
|
| static uint16_t | getAdcSample (void) |
|
Initiates an A/D conversion and reads the sample when done.
|
|
| static float | measureSupplyIR (uint8_t loadSetting) |
|
Measures the unladed and loaded supply voltage and calculates the intermal resistance of the connected supply. The load is provided by the heater element built in the Si7021.
|
|
| static float | measureSupplyVoltage (unsigned int avg) |
|
Measures the supply voltage by averaging multiple readings.
|
|
| static void | rtcCb ( RTCDRV_TimerID_t id, void *user) |
|
RTC callback function, called when the timer expired.
|
|
| void | SysTick_Handler (void) |
|
Interrupt Service Routine for system tick counter.
|
|
| void | UTIL_delay (uint32_t ms) |
|
Delays number of msTick Systicks (1 ms)
|
|
| uint32_t | UTIL_init (void) |
|
Sets up the SysTick timer for 1ms interrupts and initializes and starts the RTC timer.
|
|
| bool | UTIL_isLowPower (void) |
|
Checks if the current power supply has low power capability.
|
|
| void | UTIL_shutdown (void) |
|
Enter lowest power shutdown mode, EM4S.
|
|
| void | UTIL_sleep (uint32_t ms) |
|
Delays number of milliseconds in sleep mode (EM2) using the RTC.
|
|
| uint32_t | UTIL_sleepInit (void) |
|
Sets up the RTC timer used for sleep functions.
|
|
| void | UTIL_supplyGetCharacteristics (uint8_t *type, float *voltage, float *ir) |
|
Retrieves the supply characteristic variables.
|
|
| uint8_t | UTIL_supplyGetType (void) |
|
Returns the type of the power supply.
|
|
| void | UTIL_supplyProbe (void) |
|
Probes the connected supply and determines its type. The results are stored in global variables.
|
|
| uint32_t | UTIL_waitForEvent (uint32_t timeout) |
|
Delays number of milliseconds in sleep mode (EM2) using the RTC but but returns if an event wakes up the MCU.
|
|
Macro Definition Documentation
| #define UTIL_SUPPLY_TYPE_AA 2 |
The board powered from AA batteries
Definition at line
34
of file
util.h
.
| #define UTIL_SUPPLY_TYPE_AAA 3 |
The board powered from AAA batteries
Definition at line
35
of file
util.h
.
Referenced by UTIL_supplyProbe() .
| #define UTIL_SUPPLY_TYPE_CR2032 4 |
The board powered from a CR2032 battery
Definition at line
36
of file
util.h
.
Referenced by UTIL_isLowPower() , and UTIL_supplyProbe() .
| #define UTIL_SUPPLY_TYPE_UNKNOWN 0 |
Unknown power supply type
Definition at line
32
of file
util.h
.
Referenced by UTIL_isLowPower() , and UTIL_supplyProbe() .
| #define UTIL_SUPPLY_TYPE_USB 1 |
The board powered from the USB connector
Definition at line
33
of file
util.h
.
Referenced by UTIL_supplyProbe() .
Function Documentation
|
static |
De-initializes the A/D converter.
- Returns
- None
Definition at line
91
of file
util_supply.c
.
References _CMU_CTRL_CLKOUTSEL1_MASK , and CMU .
Referenced by measureSupplyVoltage() .
|
static |
Initializes the A/D converter.
- Returns
- None
Definition at line
57
of file
util_supply.c
.
References _ADC_CTRL_RESETVALUE , ADC_InitSingle_TypeDef::acqTime , ADC0 , ADC_Init() , ADC_INIT_DEFAULT , ADC_InitSingle() , ADC_INITSINGLE_DEFAULT , ADC_PrescaleCalc() , ADC_TimebaseCalc() , adcAcqTime16 , adcPRSSELCh4 , adcRef5VDIFF , CMU_ClockEnable() , cmuClock_ADC0 , cmuClock_PRS , ADC_Init_TypeDef::prescale , ADC_InitSingle_TypeDef::prsEnable , ADC_InitSingle_TypeDef::prsSel , ADC_InitSingle_TypeDef::reference , and ADC_Init_TypeDef::timebase .
Referenced by measureSupplyVoltage() , and MIC_init() .
|
static |
Initiates an A/D conversion and reads the sample when done.
- Returns
- The output of the A/D conversion
Definition at line
106
of file
util_supply.c
.
References ADC0 , ADC_DataSingleGet() , ADC_IF_SINGLE , ADC_IntGet() , ADC_Start() , and adcStartSingle .
Referenced by measureSupplyVoltage() .
|
static |
Measures the unladed and loaded supply voltage and calculates the intermal resistance of the connected supply. The load is provided by the heater element built in the Si7021.
- Parameters
-
[in] loadSettingHeater current setting of the Si7021
- Returns
- The measured internal resistance of the connected supply
Definition at line
159
of file
util_supply.c
.
References measureSupplyVoltage() , SI7021_CMD_WRITE_HEATER_CTRL , SI7021_CMD_WRITE_USER_REG1 , SI7021_cmdWrite() , and UTIL_delay() .
Referenced by UTIL_supplyProbe() .
|
static |
Measures the supply voltage by averaging multiple readings.
- Parameters
-
[in] avgNumber of measurements to average
- Returns
- The measured voltage
Definition at line
125
of file
util_supply.c
.
References adcDeInit() , adcInit() , and getAdcSample() .
Referenced by measureSupplyIR() , and UTIL_supplyProbe() .
|
static |
RTC callback function, called when the timer expired.
- Parameters
-
[in] idThe id of the timer [in] userExtra parameter for user application (not used)
- Returns
- None
Definition at line
127
of file
util_sleep.c
.
Referenced by UTIL_sleep() , and UTIL_waitForEvent() .
| void SysTick_Handler | ( | void |
|
) |
Interrupt Service Routine for system tick counter.
- Returns
- None
Definition at line
67
of file
util.c
.
| void UTIL_delay | ( | uint32_t |
ms
|
) |
Delays number of msTick Systicks (1 ms)
- Parameters
-
[in] msNumber of ticks (ms) to delay
- Returns
- None
Definition at line
84
of file
util.c
.
References EMU_EnterEM1() .
Referenced by BAP_init() , BOARD_flashDeepPowerDown() , BOARD_gasSensorWake() , BOARD_init() , CCS811_init() , HALL_init() , ICM20648_accelGyroCalibrate() , ICM20648_gyroCalibrate() , ICM20648_init() , ICM20648_lowPowerModeEnter() , ICM20648_reset() , ICM20648_wakeOnMotionITEnable() , IMU_config() , measureSupplyIR() , SI1133_init() , SI1133_measureLuxUvi() , SI1133_reset() , SI7021_init() , and SI7021_measure() .
| uint32_t UTIL_init | ( | void |
|
) |
Sets up the SysTick timer for 1ms interrupts and initializes and starts the RTC timer.
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line
48
of file
util.c
.
References CMU_ClockFreqGet() , and cmuClock_CORE .
| bool UTIL_isLowPower | ( | void |
|
) |
Checks if the current power supply has low power capability.
- Returns
- True if the supply is low power type, false otherwise
Definition at line
279
of file
util_supply.c
.
References UTIL_SUPPLY_TYPE_CR2032 , and UTIL_SUPPLY_TYPE_UNKNOWN .
| void UTIL_shutdown | ( | void |
|
) |
Enter lowest power shutdown mode, EM4S.
- Returns
- None
Definition at line
103
of file
util.c
.
References EMU_EnterEM4() , GPIO_PinModeSet() , and gpioModeInputPullFilter .
| void UTIL_sleep | ( | uint32_t |
ms
|
) |
Delays number of milliseconds in sleep mode (EM2) using the RTC.
- Parameters
-
msNumber of milliseconds to sleep
- Returns
- None
Definition at line
74
of file
util_sleep.c
.
References EMU_EnterEM2() , rtcCb() , RTCDRV_StartTimer() , and rtcdrvTimerTypeOneshot .
| uint32_t UTIL_sleepInit | ( | void |
|
) |
Sets up the RTC timer used for sleep functions.
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line
49
of file
util_sleep.c
.
References ECODE_EMDRV_RTCDRV_OK , RTCDRV_AllocateTimer() , and RTCDRV_Init() .
| void UTIL_supplyGetCharacteristics | ( | uint8_t * |
type,
|
| float * |
voltage,
|
||
| float * |
ir
|
||
| ) |
Retrieves the supply characteristic variables.
- Parameters
-
[in] typeSupply type [in] voltageLoaded supply voltage [in] irInternal resistance of the supply
- Returns
- None
Definition at line
251
of file
util_supply.c
.
| uint8_t UTIL_supplyGetType | ( | void |
|
) |
Returns the type of the power supply.
- Returns
- The type of the supply
Definition at line
267
of file
util_supply.c
.
| void UTIL_supplyProbe | ( | void |
|
) |
Probes the connected supply and determines its type. The results are stored in global variables.
- Returns
- None
Definition at line
206
of file
util_supply.c
.
References measureSupplyIR() , measureSupplyVoltage() , SI7021_deInit() , SI7021_init() , UTIL_SUPPLY_TYPE_AAA , UTIL_SUPPLY_TYPE_CR2032 , UTIL_SUPPLY_TYPE_UNKNOWN , and UTIL_SUPPLY_TYPE_USB .
| uint32_t UTIL_waitForEvent | ( | uint32_t |
timeout
|
) |
Delays number of milliseconds in sleep mode (EM2) using the RTC but but returns if an event wakes up the MCU.
- Parameters
-
timeoutTimeout, the maximum number of milliseconds to sleep
- Returns
- The number of milliseconds remained from the timeout
Definition at line
96
of file
util_sleep.c
.
References EMU_EnterEM2() , rtcCb() , RTCDRV_StartTimer() , RTCDRV_TimeRemaining() , and rtcdrvTimerTypeOneshot .