display.h File Reference
Display device interface.
- Version
- 5.5.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
display.h
.
#include <stdbool.h>
#include <stdint.h>
#include "
emstatus.h
"
#include "
displayconfigall.h
"
Data Structures |
|
| struct | DISPLAY_Device_t |
| struct | DISPLAY_Geometry_t |
Macros |
|
| #define | DISPLAY_EMSTATUS_INVALID_PARAMETER ( DISPLAY_EMSTATUS_BASE | 3) |
| #define | DISPLAY_EMSTATUS_NOT_ENOUGH_MEMORY ( DISPLAY_EMSTATUS_BASE | 1) |
| #define | DISPLAY_EMSTATUS_NOT_INITIALIZED ( DISPLAY_EMSTATUS_BASE | 5) |
| #define | DISPLAY_EMSTATUS_NOT_SUPPORTED ( DISPLAY_EMSTATUS_BASE | 4) |
| #define | DISPLAY_EMSTATUS_OK (0) |
| #define | DISPLAY_EMSTATUS_OUT_OF_RANGE ( DISPLAY_EMSTATUS_BASE | 2) |
Typedefs |
|
| typedef enum DISPLAY_AddressMode_t | DISPLAY_AddressMode_t |
| typedef enum DISPLAY_ColourMode_t | DISPLAY_ColourMode_t |
| typedef struct DISPLAY_Device_t | DISPLAY_Device_t |
| typedef struct DISPLAY_Geometry_t | DISPLAY_Geometry_t |
| typedef void * | DISPLAY_PixelMatrix_t |
| typedef EMSTATUS(* | pDisplayDeviceDriverInitFunction_t ) (void) |
Functions |
|
| EMSTATUS | DISPLAY_DeviceGet (int displayDeviceNo, DISPLAY_Device_t *device) |
|
Get the display device data structure corresponding to the device number.
|
|
| EMSTATUS | DISPLAY_DriverRefresh (void) |
|
Refresh all DISPLAY devices.
|
|
| EMSTATUS | DISPLAY_Init (void) |
|
Initialize the DISPLAY module.
|
|